Functions | |
| SDL_VTM_adc_code | SDL_VTM_getAdcCode (SDL_VTM_InstTs instance) |
| read Temperature sensor ADC code More... | |
| int32_t | SDL_VTM_tsGetCtrl (SDL_VTM_InstTs instance, uint32_t *pTsCtrlCfg) |
| Read VTM Temperature Sensor Control. More... | |
| int32_t | SDL_VTM_tsConvADCToTemp (SDL_VTM_adc_code adcCode, int32_t *pMilliDegreeTempVal) |
| VTM Temperature ADC code to Temperature conversion. More... | |
| int32_t | SDL_VTM_tsConvTempToAdc (int32_t milliDegreeTempVal, SDL_VTM_adc_code *pAdcCode) |
| VTM Temperature to ADC code conversion. More... | |
| SDL_VTM_adc_code SDL_VTM_getAdcCode | ( | SDL_VTM_InstTs | instance | ) |
read Temperature sensor ADC code
| instance | [IN] sensor for which ADC code is needed |
| int32_t SDL_VTM_tsGetCtrl | ( | SDL_VTM_InstTs | instance, |
| uint32_t * | pTsCtrlCfg | ||
| ) |
Read VTM Temperature Sensor Control.
| instance | [IN] VTM Temperature sensor instance |
| pTsCtrlCfg | [IN] Pointer to temperature sensor control configuration |
| int32_t SDL_VTM_tsConvADCToTemp | ( | SDL_VTM_adc_code | adcCode, |
| int32_t * | pMilliDegreeTempVal | ||
| ) |
VTM Temperature ADC code to Temperature conversion.
| adcCode | [IN] 7 Bit ADC code |
| pMilliDegreeTempVal | [OUT] Pointer to Temperature in milli degree celcius |
| int32_t SDL_VTM_tsConvTempToAdc | ( | int32_t | milliDegreeTempVal, |
| SDL_VTM_adc_code * | pAdcCode | ||
| ) |
VTM Temperature to ADC code conversion.
| milliDegreeTempVal | [IN] Temperature in milli degree celcius |
| pAdcCode | [OUT] Pointer to 7 Bit ADC code |