This module contains APIs to program and use the UART.
Sub Modules | |
| APIs for UART DMA mode | |
Files | |
| file | uart_lld.h |
| This file contains the prototype of UART driver APIs. | |
Data Structures | |
| struct | UART_ExtendedParams |
| struct | UART_Transaction |
| Data structure used with UART_read() and UART_write() More... | |
| struct | UARTLLD_InitObject |
| UART driver initialization object. More... | |
| struct | UARTLLD_Handle |
| UART driver object. More... | |
Functions | |
| uint32_t | UART_operatingModeSelect (uint32_t baseAddr, uint32_t modeFlag) |
| uint32_t | UART_spaceAvail (uint32_t baseAddr) |
| uint32_t | UART_IsTxRxFifoEmpty (uint32_t baseAddr) |
| int32_t | UART_writeCancelNoCB (UARTLLD_Handle hUart) |
| int32_t | UART_readCancelNoCB (UARTLLD_Handle hUart) |
| uint32_t | UART_getBaseAddr_lld (UARTLLD_Handle handle) |
| Function to get base address of UART instance of a particular handle. More... | |
| void | UART_enableLoopbackMode (uint32_t baseAddr) |
| Function to enable loopback mode. This function is for internal use. Not recommended for customers to use. More... | |
| void | UART_disableLoopbackMode (uint32_t baseAddr) |
| Function to disable loopback mode. This function is for internal use. Not recommended for customers to use. More... | |
| int32_t | UART_lld_init (UARTLLD_Handle hUart) |
| This API Initializes the UART instance. More... | |
| int32_t | UART_lld_initDma (UARTLLD_Handle hUart) |
| This API Initializes the UART instance in DMA mode. More... | |
| int32_t | UART_lld_deInit (UARTLLD_Handle hUart) |
| This API De-Initializes the UART instance. More... | |
| int32_t | UART_lld_deInitDma (UARTLLD_Handle hUart) |
| This API De-Initializes the UART instance in DMA mode. More... | |
| int32_t | UART_lld_write (UARTLLD_Handle hUart, void *txBuf, uint32_t size, uint32_t timeout, const UART_ExtendedParams *extendedParams) |
| This API writes data to the UART instance in Polling mode. More... | |
| int32_t | UART_lld_writeIntr (UARTLLD_Handle hUart, void *txBuf, uint32_t size, const UART_ExtendedParams *extendedParams) |
| This API writes data to the UART instance in Interrupt mode. More... | |
| int32_t | UART_lld_writeDma (UARTLLD_Handle hUart, void *txBuf, uint32_t size, const UART_ExtendedParams *extendedParams) |
| This API writes data to the UART instance in DMA mode. More... | |
| int32_t | UART_lld_read (UARTLLD_Handle hUart, void *rxBuf, uint32_t size, uint32_t timeout, const UART_ExtendedParams *extendedParams) |
| This API reads data from the UART instance in Polling mode. More... | |
| int32_t | UART_lld_readWithCounter (UARTLLD_Handle hUart, void *rxBuf, uint32_t size, uint32_t timeout, const UART_ExtendedParams *extendedParams) |
| This API reads data with counter. More... | |
| int32_t | UART_lld_readIntr (UARTLLD_Handle hUart, void *rxBuf, uint32_t size, const UART_ExtendedParams *extendedParams) |
| This API reads data from the UART instance in Interrupt mode. More... | |
| int32_t | UART_lld_readDma (UARTLLD_Handle hUart, void *rxBuf, uint32_t size, const UART_ExtendedParams *extendedParams) |
| This API reads data from the UART instance in DMA mode. More... | |
| int32_t | UART_lld_writeCancel (UARTLLD_Handle hUart, UART_Transaction *trans) |
| This API cancels current UART Write. More... | |
| int32_t | UART_lld_readCancel (UARTLLD_Handle hUart, UART_Transaction *trans) |
| This API cancels current UART Read. More... | |
| int32_t | UART_lld_flushTxFifo (UARTLLD_Handle hUart) |
| Function to flush a TX FIFO of peripheral specified by the UART handle. More... | |
| int32_t | UART_procLineStatusErr (UARTLLD_Handle hUart) |
| Function to check various error conditions in uart. More... | |
| int32_t | UART_lld_setRxState (UARTLLD_Handle hUart, uint32_t state) |
| Function to enable/disable UART RX State. More... | |
| void | UART_lld_controllerIsr (void *args) |
| This is the UART ISR and can be used as IRQ handler. More... | |
| void | UART_intrDisable (uint32_t baseAddr, uint32_t intrFlag) |
| This API disables the specified interrupts in the UART mode of operation. More... | |
| void | UART_intr2Disable (uint32_t baseAddr, uint32_t intrFlag) |
| This API disables the specified interrupts in the UART mode of operation for IER2. More... | |
| uint32_t | UART_checkCharsAvailInFifo (uint32_t baseAddr) |
| This API checks if the RX FIFO (or RHR in non-FIFO mode) has atleast one byte of data to be read. More... | |
| uint32_t | UART_readLineStatus (uint32_t baseAddr) |
| This API reads the line status register value. More... | |
| uint8_t | UART_getCharFifo (uint32_t baseAddr, uint8_t *readBuf) |
| This API reads the data present at the top of the RX FIFO, that is, the data in the Receive Holding Register(RHR). However before reading the data from RHR, it checks for RX error. More... | |
| void | UART_putChar (uint32_t baseAddr, uint8_t byteTx) |
| This API writes a byte to the Transmitter FIFO without checking for the emptiness of the Transmitter FIFO or the Transmitter Shift Register(TSR). More... | |
| void | UART_intrEnable (uint32_t baseAddr, uint32_t intrFlag) |
| This API enables the specified interrupts in the UART mode of operation. More... | |
| uint32_t | UART_getChar (uint32_t baseAddr, uint8_t *pChar) |
| This API reads a byte from the Receiver Buffer Register (RBR). It checks once if any character is ready to be read. More... | |
| uint32_t | UART_getIntr2Status (uint32_t baseAddr) |
| This API determines the UART Interrupt Status 2. More... | |
| uint32_t | UART_getIntrIdentityStatus (uint32_t baseAddr) |
| This API determines the UART Interrupt Status. More... | |
| void | UART_intr2Enable (uint32_t baseAddr, uint32_t intrFlag) |
| This API enables the specified interrupts in the UART mode of operation for IER2. More... | |
| void | UART_lld_Transaction_init (UART_Transaction *trans) |
| Function to initialize the UART_Transaction struct to its defaults. More... | |
| void | UART_lld_Transaction_deInit (UART_Transaction *trans) |
| Function to de-initialize the UART_Transaction struct to its defaults. More... | |
Typedefs | |
| typedef uint32_t(* | UART_clockGet) (void) |
| typedef uint32_t(* | UART_clockUsecToTick) (uint64_t usecs) |
| typedef void(* | UART_readCompCallbackFxn) (struct UARTLLD_Object_s *args) |
| The definition of a read complete callback function used by the UART driver when used in UART_TRANSFER_MODE_CALLBACK. More... | |
| typedef void(* | UART_writeCompCallbackFxn) (struct UARTLLD_Object_s *args) |
| The definition of a write complete callback function used by the UART driver when used in UART_TRANSFER_MODE_CALLBACK. More... | |
| typedef struct UARTLLD_InitObject * | UARTLLD_InitHandle |
Macros | |
| #define | UART_FIFO_SIZE (64U) |
| Uart FIFO Size. More... | |
| #define | UART_TRANSMITEMPTY_TRIALCOUNT (3000U) |
| Timeout in ms used for TX FIFO empty at the time of delete. Three seconds is more than sufficient to transfer 64 bytes (FIFO size) at the lowest baud rate of 2400. More... | |
| #define | UART_ERROR_COUNT (0x00FFFFFFU) |
| Count Value to check error in the recieved byte More... | |
| #define | UART_NOT_IN_USE(x) (void) 0 |
| NOT_IN_USE macro to highlight unused parameters. More... | |
| #define | UART_STATE_RX_DISABLED (0x0U) |
| #define | UART_STATE_RX_ENABLED (0x1U) |
Transfer Status Code | |
|
Status codes that are set by the UART driver | |
| #define | UART_STATUS_SUCCESS ((int32_t)0) |
| Transaction success. More... | |
| #define | UART_STATUS_FAILURE ((int32_t)-1) |
| Transaction failure. More... | |
| #define | UART_TRANSFER_STATUS_SUCCESS ((int32_t)0) |
| Transaction success. More... | |
| #define | UART_TRANSFER_STATUS_FAILURE ((int32_t)-1) |
| Transaction failure. More... | |
| #define | UART_WAIT_FOREVER ((int32_t)-1) |
| Value to use when needing a timeout of infinity or wait forver until resource is available. More... | |
| #define | UART_INVALID_PARAM ((int32_t)-3) |
| Return status when the API execution failed due invalid parameters. More... | |
| #define | UART_TRANSFER_BUSY ((int32_t)-4) |
| Return status when the API execution failed due to driver busy. More... | |
| #define | UART_TRANSFER_TIMEOUT ((int32_t)-2) |
| Return status when the API execution was not successful due to a time out. More... | |
| #define | UART_TRANSFER_INVALID_STATE ((int32_t)-5) |
| Return status when the API execution failed due to invalid LLD state. More... | |
| #define | UART_TRANSFER_STATUS_TIMEOUT (1U) |
| Time out error. More... | |
| #define | UART_TRANSFER_STATUS_ERROR_BI (2U) |
| Break condition error. More... | |
| #define | UART_TRANSFER_STATUS_ERROR_FE (3U) |
| Framing error. More... | |
| #define | UART_TRANSFER_STATUS_ERROR_PE (4U) |
| Parity error. More... | |
| #define | UART_TRANSFER_STATUS_ERROR_OE (5U) |
| Overrun error. More... | |
| #define | UART_TRANSFER_STATUS_CANCELLED (6U) |
| Cancelled. More... | |
| #define | UART_TRANSFER_STATUS_STARTED (7U) |
| Transaction started. More... | |
| #define | UART_TRANSFER_STATUS_READ_TIMEOUT (8U) |
| Read timeout error. More... | |
| #define | UART_TRANSFER_STATUS_ERROR_INUSE (9U) |
| UART is currently in use. More... | |
| #define | UART_TRANSFER_STATUS_ERROR_OTH (10U) |
| Other errors. More... | |
| #define | UART_STATE_RESET (0U) |
| #define | UART_STATE_READY (1U) |
| #define | UART_STATE_BUSY (2U) |
| #define | UART_STATE_ERROR (3U) |
UART Read length | |
|
This enumeration defines the return modes for UART_read(). UART_READ_RETURN_MODE_FULL unblocks or performs a callback when the read buffer has been filled with the number of bytes passed to UART_read(). UART_READ_RETURN_MODE_PARTIAL unblocks or performs a callback whenever a read timeout error occurs on the UART peripheral. The read timeout occurs if the read FIFO is non-empty and no new data has been received for a specific device/baudrate dependent number of clock cycles. This mode can be used when the exact number of bytes to be read is not known. | |
| #define | UART_READ_RETURN_MODE_FULL (0U) |
| Unblock/callback when buffer is full. More... | |
| #define | UART_READ_RETURN_MODE_PARTIAL (1U) |
| Unblock/callback when no new data comes in. More... | |
UART data length | |
|
Note: The values should not be changed since it represents the actual register configuration values used to configure the UART | |
| #define | UART_LEN_5 (0U) |
| #define | UART_LEN_6 (1U) |
| #define | UART_LEN_7 (2U) |
| #define | UART_LEN_8 (3U) |
UART stop bits | |
|
Note: The values should not be changed since it represents the actual register configuration values used to configure the UART | |
| #define | UART_STOPBITS_1 (0U) |
| #define | UART_STOPBITS_2 (1U) |
| #define | UART_STOPBITS_1P5 (UART_STOPBITS_1) |
UART Parity | |
|
Note: The values should not be changed since it represents the actual register configuration values used to configure the UART | |
| #define | UART_PARITY_NONE (0x00U) |
| #define | UART_PARITY_ODD (0x01U) |
| #define | UART_PARITY_EVEN (0x03U) |
| #define | UART_PARITY_FORCED0 (0x07U) |
| #define | UART_PARITY_FORCED1 (0x05U) |
UART Flow Control Type | |
|
Note: The values should not be changed since it represents the actual register configuration values used to configure the UART | |
| #define | UART_FCTYPE_NONE (0x00U) |
| #define | UART_FCTYPE_HW (0x02U) |
UART Flow Control Params for RX | |
|
Note: The values should not be changed since it represents the actual register configuration values used to configure the UART | |
| #define | UART_FCPARAM_RXNONE (0x00U) |
| #define | UART_FCPARAM_RXXONXOFF_2 (0x01U) |
| #define | UART_FCPARAM_RXXONXOFF_1 (0x02U) |
| #define | UART_FCPARAM_RXXONXOFF_12 (0x03U) |
| #define | UART_FCPARAM_AUTO_RTS (0x40U) |
UART Flow Control Params for TX | |
|
Note: The values should not be changed since it represents the actual register configuration values used to configure the UART | |
| #define | UART_FCPARAM_TXNONE (0x00U) |
| #define | UART_FCPARAM_TXXONXOFF_2 (0x04U) |
| #define | UART_FCPARAM_TXXONXOFF_1 (0x08U) |
| #define | UART_FCPARAM_TXXONXOFF_12 (0x0CU) |
| #define | UART_FCPARAM_AUTO_CTS (0x80U) |
UART RX trigger level | |
|
Note: The values should not be changed since it represents the actual register configuration values used to configure the UART | |
| #define | UART_RXTRIGLVL_1 (1U) |
| #define | UART_RXTRIGLVL_8 (8U) |
| #define | UART_RXTRIGLVL_16 (16U) |
| #define | UART_RXTRIGLVL_56 (56U) |
| #define | UART_RXTRIGLVL_60 (60U) |
UART TX trigger level | |
|
Note: The values should not be changed since it represents the actual register configuration values used to configure the UART | |
| #define | UART_TXTRIGLVL_1 (1U) |
| #define | UART_TXTRIGLVL_8 (8U) |
| #define | UART_TXTRIGLVL_16 (16U) |
| #define | UART_TXTRIGLVL_32 (32U) |
| #define | UART_TXTRIGLVL_56 (56U) |
UART Operational Mode | |
|
Note: The values should not be changed since it represents the actual register configuration values used to configure the UART | |
| #define | UART_OPER_MODE_16X (0U) |
| #define | UART_OPER_MODE_SIR (1U) |
| #define | UART_OPER_MODE_16X_AUTO_BAUD (2U) |
| #define | UART_OPER_MODE_13X (3U) |
| #define | UART_OPER_MODE_MIR (4U) |
| #define | UART_OPER_MODE_FIR (5U) |
| #define | UART_OPER_MODE_CIR (6U) |
| #define | UART_OPER_MODE_DISABLED (7U) |
Values indicating the filled status of TX FIFO | |
|
Note: The values should not be changed since it represents the actual register configuration values used to configure the UART | |
| #define | UART_TX_FIFO_NOT_FULL |
| #define | UART_TX_FIFO_FULL |
Values related to status of Interrupt souces. | |
| #define | UART_INTID_MODEM_STAT |
| Values pertaining to status of UART Interrupt sources. More... | |
| #define | UART_INTID_TX_THRES_REACH |
| #define | UART_INTID_RX_THRES_REACH |
| #define | UART_INTID_RX_LINE_STAT_ERROR |
| #define | UART_INTID_CHAR_TIMEOUT |
| #define | UART_INTID_XOFF_SPEC_CHAR_DETECT |
| #define | UART_INTID_MODEM_SIG_STATE_CHANGE |
| #define | UART_INTR_PENDING (0U) |
| Values indicating the UART Interrupt pending status. More... | |
| #define | UART_N0_INTR_PENDING (1U) |
Values related to enabling/disabling of Interrupts. | |
| #define | UART_INTR_CTS (UART_IER_CTS_IT_MASK) |
| Values for enabling/disabling the interrupts of UART. More... | |
| #define | UART_INTR_RTS (UART_IER_RTS_IT_MASK) |
| #define | UART_INTR_XOFF (UART_IER_XOFF_IT_MASK) |
| #define | UART_INTR_SLEEPMODE (UART_IER_SLEEP_MODE_MASK) |
| #define | UART_INTR_MODEM_STAT (UART_IER_MODEM_STS_IT_MASK) |
| #define | UART_INTR_LINE_STAT (UART_IER_LINE_STS_IT_MASK) |
| #define | UART_INTR_THR (UART_IER_THR_IT_MASK) |
| #define | UART_INTR_RHR_CTI (UART_IER_RHR_IT_MASK) |
| #define | UART_INTR2_RX_EMPTY (UART_IER2_EN_RXFIFO_EMPTY_MASK) |
| #define | UART_INTR2_TX_EMPTY (UART_IER2_EN_TXFIFO_EMPTY_MASK) |
Values related to Line Status information. | |
| #define | UART_FIFO_PE_FE_BI_DETECTED (UART_LSR_RX_FIFO_STS_MASK) |
| Values pertaining to UART Line Status information. More... | |
| #define | UART_BREAK_DETECTED_ERROR (UART_LSR_RX_BI_MASK) |
| #define | UART_FRAMING_ERROR (UART_LSR_RX_FE_MASK) |
| #define | UART_PARITY_ERROR (UART_LSR_RX_PE_MASK) |
| #define | UART_OVERRUN_ERROR (UART_LSR_RX_OE_MASK) |
Values related to Register Mode Configuration. | |
| #define | UART_REG_CONFIG_MODE_A ((uint32_t) 0x0080) |
| Values to be used while switching between register configuration modes. More... | |
| #define | UART_REG_CONFIG_MODE_B ((uint32_t) 0x00BF) |
| #define | UART_REG_OPERATIONAL_MODE ((uint32_t) 0x007F) |
UART Configration Mode | |
|
This determines whether the driver configuration mode like Polled, Interrupt, Dma used for the transfer function | |
| #define | UART_CONFIG_MODE_POLLED (0x00U) |
| #define | UART_CONFIG_MODE_INTERRUPT (0x01U) |
| #define | UART_CONFIG_MODE_USER_INTR (0x02U) |
| #define | UART_CONFIG_MODE_DMA (0x03U) |
| #define | UART_CONFIG_MODE_POLLED_WITH_COUNTER (0x04U) |
| #define UART_FIFO_SIZE (64U) |
Uart FIFO Size.
| #define UART_TRANSMITEMPTY_TRIALCOUNT (3000U) |
Timeout in ms used for TX FIFO empty at the time of delete. Three seconds is more than sufficient to transfer 64 bytes (FIFO size) at the lowest baud rate of 2400.
| #define UART_ERROR_COUNT (0x00FFFFFFU) |
Count Value to check error in the recieved byte
| #define UART_STATUS_SUCCESS ((int32_t)0) |
Transaction success.
| #define UART_STATUS_FAILURE ((int32_t)-1) |
Transaction failure.
| #define UART_TRANSFER_STATUS_SUCCESS ((int32_t)0) |
Transaction success.
| #define UART_TRANSFER_STATUS_FAILURE ((int32_t)-1) |
Transaction failure.
| #define UART_WAIT_FOREVER ((int32_t)-1) |
Value to use when needing a timeout of infinity or wait forver until resource is available.
| #define UART_INVALID_PARAM ((int32_t)-3) |
Return status when the API execution failed due invalid parameters.
| #define UART_TRANSFER_BUSY ((int32_t)-4) |
Return status when the API execution failed due to driver busy.
| #define UART_TRANSFER_TIMEOUT ((int32_t)-2) |
Return status when the API execution was not successful due to a time out.
| #define UART_TRANSFER_INVALID_STATE ((int32_t)-5) |
Return status when the API execution failed due to invalid LLD state.
| #define UART_TRANSFER_STATUS_TIMEOUT (1U) |
Time out error.
| #define UART_TRANSFER_STATUS_ERROR_BI (2U) |
Break condition error.
| #define UART_TRANSFER_STATUS_ERROR_FE (3U) |
Framing error.
| #define UART_TRANSFER_STATUS_ERROR_PE (4U) |
Parity error.
| #define UART_TRANSFER_STATUS_ERROR_OE (5U) |
Overrun error.
| #define UART_TRANSFER_STATUS_CANCELLED (6U) |
Cancelled.
| #define UART_TRANSFER_STATUS_STARTED (7U) |
Transaction started.
| #define UART_TRANSFER_STATUS_READ_TIMEOUT (8U) |
Read timeout error.
| #define UART_TRANSFER_STATUS_ERROR_INUSE (9U) |
UART is currently in use.
| #define UART_TRANSFER_STATUS_ERROR_OTH (10U) |
Other errors.
| #define UART_READ_RETURN_MODE_FULL (0U) |
Unblock/callback when buffer is full.
| #define UART_READ_RETURN_MODE_PARTIAL (1U) |
Unblock/callback when no new data comes in.
| #define UART_LEN_5 (0U) |
| #define UART_LEN_6 (1U) |
| #define UART_LEN_7 (2U) |
| #define UART_LEN_8 (3U) |
| #define UART_STATE_RESET (0U) |
| #define UART_STATE_READY (1U) |
| #define UART_STATE_BUSY (2U) |
| #define UART_STATE_ERROR (3U) |
| #define UART_NOT_IN_USE | ( | x | ) | (void) 0 |
NOT_IN_USE macro to highlight unused parameters.
| #define UART_STOPBITS_1 (0U) |
| #define UART_STOPBITS_2 (1U) |
| #define UART_STOPBITS_1P5 (UART_STOPBITS_1) |
| #define UART_PARITY_NONE (0x00U) |
| #define UART_PARITY_ODD (0x01U) |
| #define UART_PARITY_EVEN (0x03U) |
| #define UART_PARITY_FORCED0 (0x07U) |
| #define UART_PARITY_FORCED1 (0x05U) |
| #define UART_FCTYPE_NONE (0x00U) |
| #define UART_FCTYPE_HW (0x02U) |
| #define UART_FCPARAM_RXNONE (0x00U) |
| #define UART_FCPARAM_RXXONXOFF_2 (0x01U) |
| #define UART_FCPARAM_RXXONXOFF_1 (0x02U) |
| #define UART_FCPARAM_RXXONXOFF_12 (0x03U) |
| #define UART_FCPARAM_AUTO_RTS (0x40U) |
| #define UART_FCPARAM_TXNONE (0x00U) |
| #define UART_FCPARAM_TXXONXOFF_2 (0x04U) |
| #define UART_FCPARAM_TXXONXOFF_1 (0x08U) |
| #define UART_FCPARAM_TXXONXOFF_12 (0x0CU) |
| #define UART_FCPARAM_AUTO_CTS (0x80U) |
| #define UART_RXTRIGLVL_1 (1U) |
| #define UART_RXTRIGLVL_8 (8U) |
| #define UART_RXTRIGLVL_16 (16U) |
| #define UART_RXTRIGLVL_56 (56U) |
| #define UART_RXTRIGLVL_60 (60U) |
| #define UART_TXTRIGLVL_1 (1U) |
| #define UART_TXTRIGLVL_8 (8U) |
| #define UART_TXTRIGLVL_16 (16U) |
| #define UART_TXTRIGLVL_32 (32U) |
| #define UART_TXTRIGLVL_56 (56U) |
| #define UART_OPER_MODE_16X (0U) |
| #define UART_OPER_MODE_SIR (1U) |
| #define UART_OPER_MODE_16X_AUTO_BAUD (2U) |
| #define UART_OPER_MODE_13X (3U) |
| #define UART_OPER_MODE_MIR (4U) |
| #define UART_OPER_MODE_FIR (5U) |
| #define UART_OPER_MODE_CIR (6U) |
| #define UART_OPER_MODE_DISABLED (7U) |
| #define UART_TX_FIFO_NOT_FULL |
| #define UART_TX_FIFO_FULL |
| #define UART_INTID_MODEM_STAT |
Values pertaining to status of UART Interrupt sources.
| #define UART_INTID_TX_THRES_REACH |
| #define UART_INTID_RX_THRES_REACH |
| #define UART_INTID_RX_LINE_STAT_ERROR |
| #define UART_INTID_CHAR_TIMEOUT |
| #define UART_INTID_XOFF_SPEC_CHAR_DETECT |
| #define UART_INTID_MODEM_SIG_STATE_CHANGE |
| #define UART_INTR_PENDING (0U) |
Values indicating the UART Interrupt pending status.
| #define UART_N0_INTR_PENDING (1U) |
| #define UART_INTR_CTS (UART_IER_CTS_IT_MASK) |
Values for enabling/disabling the interrupts of UART.
| #define UART_INTR_RTS (UART_IER_RTS_IT_MASK) |
| #define UART_INTR_XOFF (UART_IER_XOFF_IT_MASK) |
| #define UART_INTR_SLEEPMODE (UART_IER_SLEEP_MODE_MASK) |
| #define UART_INTR_MODEM_STAT (UART_IER_MODEM_STS_IT_MASK) |
| #define UART_INTR_LINE_STAT (UART_IER_LINE_STS_IT_MASK) |
| #define UART_INTR_THR (UART_IER_THR_IT_MASK) |
| #define UART_INTR_RHR_CTI (UART_IER_RHR_IT_MASK) |
| #define UART_INTR2_RX_EMPTY (UART_IER2_EN_RXFIFO_EMPTY_MASK) |
| #define UART_INTR2_TX_EMPTY (UART_IER2_EN_TXFIFO_EMPTY_MASK) |
| #define UART_FIFO_PE_FE_BI_DETECTED (UART_LSR_RX_FIFO_STS_MASK) |
Values pertaining to UART Line Status information.
| #define UART_BREAK_DETECTED_ERROR (UART_LSR_RX_BI_MASK) |
| #define UART_FRAMING_ERROR (UART_LSR_RX_FE_MASK) |
| #define UART_PARITY_ERROR (UART_LSR_RX_PE_MASK) |
| #define UART_OVERRUN_ERROR (UART_LSR_RX_OE_MASK) |
| #define UART_REG_CONFIG_MODE_A ((uint32_t) 0x0080) |
Values to be used while switching between register configuration modes.
| #define UART_REG_CONFIG_MODE_B ((uint32_t) 0x00BF) |
| #define UART_REG_OPERATIONAL_MODE ((uint32_t) 0x007F) |
| #define UART_CONFIG_MODE_POLLED (0x00U) |
| #define UART_CONFIG_MODE_INTERRUPT (0x01U) |
| #define UART_CONFIG_MODE_USER_INTR (0x02U) |
| #define UART_CONFIG_MODE_DMA (0x03U) |
| #define UART_CONFIG_MODE_POLLED_WITH_COUNTER (0x04U) |
| #define UART_STATE_RX_DISABLED (0x0U) |
| #define UART_STATE_RX_ENABLED (0x1U) |
| typedef uint32_t(* UART_clockGet) (void) |
| typedef uint32_t(* UART_clockUsecToTick) (uint64_t usecs) |
| typedef void(* UART_readCompCallbackFxn) (struct UARTLLD_Object_s *args) |
The definition of a read complete callback function used by the UART driver when used in UART_TRANSFER_MODE_CALLBACK.
| hUart | Handle to the UART instance used |
| typedef void(* UART_writeCompCallbackFxn) (struct UARTLLD_Object_s *args) |
The definition of a write complete callback function used by the UART driver when used in UART_TRANSFER_MODE_CALLBACK.
| hUart | Handle to the UART instance used |
| typedef struct UARTLLD_InitObject * UARTLLD_InitHandle |
| uint32_t UART_operatingModeSelect | ( | uint32_t | baseAddr, |
| uint32_t | modeFlag | ||
| ) |
| uint32_t UART_spaceAvail | ( | uint32_t | baseAddr | ) |
| uint32_t UART_IsTxRxFifoEmpty | ( | uint32_t | baseAddr | ) |
| int32_t UART_writeCancelNoCB | ( | UARTLLD_Handle | hUart | ) |
| int32_t UART_readCancelNoCB | ( | UARTLLD_Handle | hUart | ) |
| uint32_t UART_getBaseAddr_lld | ( | UARTLLD_Handle | handle | ) |
Function to get base address of UART instance of a particular handle.
| handle | UARTLLD_Handle returned from UART_open() |
| void UART_enableLoopbackMode | ( | uint32_t | baseAddr | ) |
Function to enable loopback mode. This function is for internal use. Not recommended for customers to use.
| baseAddr | Memory address of the UART instance being used. |
| void UART_disableLoopbackMode | ( | uint32_t | baseAddr | ) |
Function to disable loopback mode. This function is for internal use. Not recommended for customers to use.
| baseAddr | Memory address of the UART instance being used. |
| int32_t UART_lld_init | ( | UARTLLD_Handle | hUart | ) |
This API Initializes the UART instance.
| hUart | Handle to the UART instance used |
| int32_t UART_lld_initDma | ( | UARTLLD_Handle | hUart | ) |
This API Initializes the UART instance in DMA mode.
| hUart | Handle to the UART instance used |
| int32_t UART_lld_deInit | ( | UARTLLD_Handle | hUart | ) |
This API De-Initializes the UART instance.
| hUart | Handle to the UART instance used |
| int32_t UART_lld_deInitDma | ( | UARTLLD_Handle | hUart | ) |
This API De-Initializes the UART instance in DMA mode.
| hUart | Handle to the UART instance used |
| int32_t UART_lld_write | ( | UARTLLD_Handle | hUart, |
| void * | txBuf, | ||
| uint32_t | size, | ||
| uint32_t | timeout, | ||
| const UART_ExtendedParams * | extendedParams | ||
| ) |
This API writes data to the UART instance in Polling mode.
| hUart | Handle to the UART instance used |
| txBuf | Pointer to write data buffer |
| size | Data size to be transferred |
| timeout | Write timeout value |
| extendedParams | Structure to hold the extended parameters |
| int32_t UART_lld_writeIntr | ( | UARTLLD_Handle | hUart, |
| void * | txBuf, | ||
| uint32_t | size, | ||
| const UART_ExtendedParams * | extendedParams | ||
| ) |
This API writes data to the UART instance in Interrupt mode.
| hUart | Handle to the UART instance used |
| txBuf | Pointer to write data buffer |
| size | Data size to be transferred |
| extendedParams | Structure to hold the extended parameters |
| int32_t UART_lld_writeDma | ( | UARTLLD_Handle | hUart, |
| void * | txBuf, | ||
| uint32_t | size, | ||
| const UART_ExtendedParams * | extendedParams | ||
| ) |
This API writes data to the UART instance in DMA mode.
| hUart | Handle to the UART instance used |
| txBuf | Pointer to write data buffer |
| size | Data size to be transferred |
| extendedParams | Structure to hold the extended parameters |
| int32_t UART_lld_read | ( | UARTLLD_Handle | hUart, |
| void * | rxBuf, | ||
| uint32_t | size, | ||
| uint32_t | timeout, | ||
| const UART_ExtendedParams * | extendedParams | ||
| ) |
This API reads data from the UART instance in Polling mode.
| hUart | Handle to the UART instance used |
| rxBuf | Pointer to read data buffer |
| size | Data size to be transferred |
| timeout | Write timeout value |
| extendedParams | Structure to hold the extended parameters |
| int32_t UART_lld_readWithCounter | ( | UARTLLD_Handle | hUart, |
| void * | rxBuf, | ||
| uint32_t | size, | ||
| uint32_t | timeout, | ||
| const UART_ExtendedParams * | extendedParams | ||
| ) |
This API reads data with counter.
| hUart | Handle to the UART instance used |
| rxBuf | Pointer to read data buffer |
| size | Data size to be transferred |
| timeout | Write timeout value |
| extendedParams | Structure to hold the extended parameters |
| int32_t UART_lld_readIntr | ( | UARTLLD_Handle | hUart, |
| void * | rxBuf, | ||
| uint32_t | size, | ||
| const UART_ExtendedParams * | extendedParams | ||
| ) |
This API reads data from the UART instance in Interrupt mode.
| hUart | Handle to the UART instance used |
| rxBuf | Pointer to read data buffer |
| size | Data size to be transferred |
| extendedParams | Structure to hold the extended parameters |
| int32_t UART_lld_readDma | ( | UARTLLD_Handle | hUart, |
| void * | rxBuf, | ||
| uint32_t | size, | ||
| const UART_ExtendedParams * | extendedParams | ||
| ) |
This API reads data from the UART instance in DMA mode.
| hUart | Handle to the UART instance used |
| rxBuf | Pointer to read data buffer |
| size | Data size to be transferred |
| extendedParams | Structure to hold the extended parameters |
| int32_t UART_lld_writeCancel | ( | UARTLLD_Handle | hUart, |
| UART_Transaction * | trans | ||
| ) |
This API cancels current UART Write.
| hUart | Handle to the UART instance used |
| trans | Pointer to UART_Transaction structure |
| int32_t UART_lld_readCancel | ( | UARTLLD_Handle | hUart, |
| UART_Transaction * | trans | ||
| ) |
This API cancels current UART Read.
| hUart | Handle to the UART instance used |
| trans | Pointer to UART_Transaction structure |
| int32_t UART_lld_flushTxFifo | ( | UARTLLD_Handle | hUart | ) |
Function to flush a TX FIFO of peripheral specified by the UART handle.
| hUart | Handle to the UART instance used |
| int32_t UART_procLineStatusErr | ( | UARTLLD_Handle | hUart | ) |
Function to check various error conditions in uart.
| hUart | Handle to the UART instance used |
| int32_t UART_lld_setRxState | ( | UARTLLD_Handle | hUart, |
| uint32_t | state | ||
| ) |
Function to enable/disable UART RX State.
| hUart | Handle to the UART instance used |
| state | Enable/Disable UART interrupt |
| void UART_lld_controllerIsr | ( | void * | args | ) |
This is the UART ISR and can be used as IRQ handler.
| args | Argument to the ISR. |
| void UART_intrDisable | ( | uint32_t | baseAddr, |
| uint32_t | intrFlag | ||
| ) |
This API disables the specified interrupts in the UART mode of operation.
| baseAddr | Memory address of the UART instance being used. |
| intrFlag | Bit mask value of the bits corresponding to Interrupt Enable Register(IER). This specifies the UART interrupts to be disabled. |
'intrFlag' can take one or a combination of the following macros:
| void UART_intr2Disable | ( | uint32_t | baseAddr, |
| uint32_t | intrFlag | ||
| ) |
This API disables the specified interrupts in the UART mode of operation for IER2.
| baseAddr | Memory address of the UART instance being used. |
| intrFlag | Bit mask value of the bits corresponding to Interrupt Enable Register(IER2). This specifies the UART interrupts to be disabled. |
'intrFlag' can take one or a combination of the following macros:
| uint32_t UART_checkCharsAvailInFifo | ( | uint32_t | baseAddr | ) |
This API checks if the RX FIFO (or RHR in non-FIFO mode) has atleast one byte of data to be read.
| baseAddr | Memory address of the UART instance being used. |
| uint32_t UART_readLineStatus | ( | uint32_t | baseAddr | ) |
This API reads the line status register value.
| baseAddr | Memory address of the UART instance being used. |
| uint8_t UART_getCharFifo | ( | uint32_t | baseAddr, |
| uint8_t * | readBuf | ||
| ) |
This API reads the data present at the top of the RX FIFO, that is, the data in the Receive Holding Register(RHR). However before reading the data from RHR, it checks for RX error.
| baseAddr | Memory address of the UART instance being used. |
| readBuf | Pointer to the byte buffer to be read from RHR register. |
| void UART_putChar | ( | uint32_t | baseAddr, |
| uint8_t | byteTx | ||
| ) |
This API writes a byte to the Transmitter FIFO without checking for the emptiness of the Transmitter FIFO or the Transmitter Shift Register(TSR).
| baseAddr | Memory address of the UART instance being used. |
| byteTx | The byte to be transmitted by the UART. |
| void UART_intrEnable | ( | uint32_t | baseAddr, |
| uint32_t | intrFlag | ||
| ) |
This API enables the specified interrupts in the UART mode of operation.
| baseAddr | Memory address of the UART instance being used. |
| intrFlag | Bit mask value of the bits corresponding to Interrupt Enable Register(IER). This specifies the UART interrupts to be enabled. |
'intrFlag' can take one or a combination of the following macros:
| uint32_t UART_getChar | ( | uint32_t | baseAddr, |
| uint8_t * | pChar | ||
| ) |
This API reads a byte from the Receiver Buffer Register (RBR). It checks once if any character is ready to be read.
| baseAddr | Memory address of the UART instance being used. |
| pChar | Pointer to the byte variable which saves the byte read from RBR if there is any char ready to be read |
| uint32_t UART_getIntr2Status | ( | uint32_t | baseAddr | ) |
This API determines the UART Interrupt Status 2.
| baseAddr | Memory address of the UART instance being used. |
| uint32_t UART_getIntrIdentityStatus | ( | uint32_t | baseAddr | ) |
This API determines the UART Interrupt Status.
| baseAddr | Memory address of the UART instance being used. |
| void UART_intr2Enable | ( | uint32_t | baseAddr, |
| uint32_t | intrFlag | ||
| ) |
This API enables the specified interrupts in the UART mode of operation for IER2.
| baseAddr | Memory address of the UART instance being used. |
| intrFlag | Bit mask value of the bits corresponding to Interrupt Enable Register(IER2). This specifies the UART interrupts to be enabled. |
'intrFlag' can take one or a combination of the following macros:
| void UART_lld_Transaction_init | ( | UART_Transaction * | trans | ) |
Function to initialize the UART_Transaction struct to its defaults.
| trans | Pointer to UART_Transaction structure for initialization |
| void UART_lld_Transaction_deInit | ( | UART_Transaction * | trans | ) |
Function to de-initialize the UART_Transaction struct to its defaults.
| trans | Pointer to UART_Transaction structure for initialization |