AM263Px MCU+ SDK  11.00.00

Introduction

These APIs try are used for the phy tuning

Functions

int32_t OSPI_lld_phyTuneDDR (OSPILLD_Handle handle, uint32_t flashOffset)
 This function tunes the OSPI PHY for DDR mode to set optimal PHY parameters. More...
 
int32_t OSPI_lld_phyTuneSDR (OSPILLD_Handle handle, uint32_t flashOffset)
 This function tunes the OSPI PHY for SDR mode to set optimal PHY parameters. More...
 
int32_t OSPI_lld_phyTuneGrapher (OSPILLD_Handle handle, uint32_t flashOffset, uint8_t arrays[4][128][128])
 This function takes a 4x128x128 array and fills it with TX RX DLL data for graphing purpose. More...
 
void OSPI_lld_phyGetTuningData (uint32_t *tuningData, uint32_t *tuningDataSize)
 This function returns the address to the attack vector buf required for tuning the PHY. More...
 
int32_t OSPI_lld_phyReadAttackVector (OSPILLD_Handle handle, uint32_t offset)
 This function checks if the attack vector, or the data used for tuning the PHY is present at an offset in the flash. More...
 
int32_t OSPI_lld_enablePhy (OSPILLD_Handle handle)
 This function enables the PHY. More...
 
int32_t OSPI_lld_disablePhy (OSPILLD_Handle handle)
 This function disables the PHY. More...
 
int32_t OSPI_lld_enablePhyPipeline (OSPILLD_Handle handle)
 This function enables the PHY Pipeline. More...
 
int32_t OSPI_lld_disablePhyPipeline (OSPILLD_Handle handle)
 This function disables the PHY Pipeline. More...
 

Function Documentation

◆ OSPI_lld_phyTuneDDR()

int32_t OSPI_lld_phyTuneDDR ( OSPILLD_Handle  handle,
uint32_t  flashOffset 
)

This function tunes the OSPI PHY for DDR mode to set optimal PHY parameters.

Precondition
OSPI controller has been opened using OSPI_open()
Parameters
handleAn OSPILLD_Handle returned from an OSPI_open()
flashOffsetOffset of the flash at which the PHY tuning data is present
Returns
OSPI_SYSTEM_SUCCESS on success, OSPI_SYSTEM_FAILURE otherwise

◆ OSPI_lld_phyTuneSDR()

int32_t OSPI_lld_phyTuneSDR ( OSPILLD_Handle  handle,
uint32_t  flashOffset 
)

This function tunes the OSPI PHY for SDR mode to set optimal PHY parameters.

Precondition
OSPI controller has been opened using OSPI_open()
Parameters
handleAn OSPILLD_Handle returned from an OSPI_open()
flashOffsetOffset of the flash at which the PHY tuning data is present
Returns
OSPI_SYSTEM_SUCCESS on success, OSPI_SYSTEM_FAILURE otherwise

◆ OSPI_lld_phyTuneGrapher()

int32_t OSPI_lld_phyTuneGrapher ( OSPILLD_Handle  handle,
uint32_t  flashOffset,
uint8_t  arrays[4][128][128] 
)

This function takes a 4x128x128 array and fills it with TX RX DLL data for graphing purpose.

Precondition
OSPI controller has been opened using OSPI_open()
Parameters
handleAn OSPILLD_Handle returned from an OSPI_open()
flashOffsetOffset of the flash at which the PHY tuning data is present
arraysA 4x128x128 array. In this, the tx rx dll data for 4 different read delay values will be stored. This can be later used for graphing
Returns
OSPI_SYSTEM_SUCCESS on success, OSPI_SYSTEM_FAILURE otherwise

◆ OSPI_lld_phyGetTuningData()

void OSPI_lld_phyGetTuningData ( uint32_t *  tuningData,
uint32_t *  tuningDataSize 
)

This function returns the address to the attack vector buf required for tuning the PHY.

Parameters
tuningDataAddress of the tuningData array
tuningDataSizeSize of the tuningData array

◆ OSPI_lld_phyReadAttackVector()

int32_t OSPI_lld_phyReadAttackVector ( OSPILLD_Handle  handle,
uint32_t  offset 
)

This function checks if the attack vector, or the data used for tuning the PHY is present at an offset in the flash.

Parameters
handleAn OSPILLD_Handle returned from an OSPI_open()
offsetOffset in flash to check for tuningData
Returns
OSPI_SYSTEM_SUCCESS on success, OSPI_SYSTEM_FAILURE otherwise

◆ OSPI_lld_enablePhy()

int32_t OSPI_lld_enablePhy ( OSPILLD_Handle  handle)

This function enables the PHY.

Precondition
OSPI controller has been opened using OSPI_open()
Parameters
handleAn OSPILLD_Handle returned from an OSPI_open()
Returns
OSPI_SYSTEM_SUCCESS on success, OSPI_SYSTEM_FAILURE otherwise

◆ OSPI_lld_disablePhy()

int32_t OSPI_lld_disablePhy ( OSPILLD_Handle  handle)

This function disables the PHY.

Precondition
OSPI controller has been opened using OSPI_open()
Parameters
handleAn OSPILLD_Handle returned from an OSPI_open()
Returns
OSPI_SYSTEM_SUCCESS on success, OSPI_SYSTEM_FAILURE otherwise

◆ OSPI_lld_enablePhyPipeline()

int32_t OSPI_lld_enablePhyPipeline ( OSPILLD_Handle  handle)

This function enables the PHY Pipeline.

Precondition
OSPI controller has been opened using OSPI_open()
Parameters
handleAn OSPILLD_Handle returned from an OSPI_open()
Returns
OSPI_SYSTEM_SUCCESS on success, OSPI_SYSTEM_FAILURE otherwise

◆ OSPI_lld_disablePhyPipeline()

int32_t OSPI_lld_disablePhyPipeline ( OSPILLD_Handle  handle)

This function disables the PHY Pipeline.

Precondition
OSPI controller has been opened using OSPI_open()
Parameters
handleAn OSPILLD_Handle returned from an OSPI_open()
Returns
OSPI_SYSTEM_SUCCESS on success, OSPI_SYSTEM_FAILURE otherwise