This module contains APIs to program the MPU Firewall module.
◆ Fwl_Return_t
Firewall Driver Error code.
The enumeration describes all the possible return and error codes which the Firewall Driver can return
| Enumerator |
|---|
| FWL_DRV_RETURN_SUCCESS | Success/pass return code
|
| FWL_DRV_RETURN_FAILURE | General or unspecified failure/error
|
◆ MPU_FIREWALL_getRegion()
Retrieves the start and end addresses and the permission attributes of a given region in a given firewall.
- Parameters
-
| mpuParams | Structure containing all region configuration parameters. |
- Returns
- FWL_DRV_RETURN_SUCCESS if the region configuration is successfully fetched; else FWL_DRV_RETURN_FAILURE
◆ MPU_FIREWALL_getFirewallConfig()
Function to get parameters associated to a MPU firewall.
- Parameters
-
| firewallId | Firewall ID. |
| firewallConfig | Structure to save mpu firewall configuration. |
- Returns
- FWL_DRV_RETURN_SUCCESS on successful config read; else FWL_DRV_RETURN_FAILURE
◆ MPU_FIREWALL_readFaultAddress()
| Fwl_Return_t MPU_FIREWALL_readFaultAddress |
( |
uint32_t |
firewallId, |
|
|
uint32_t * |
faultAddress |
|
) |
| |
Function to read the fault address that created the firewall violation.
- Parameters
-
| firewallId | MPU Firewall Id |
| faultAddress | pointer to the faultAddress to be populated |
- Returns
- FWL_DRV_RETURN_SUCCESS on successful fault address read; else FWL_DRV_RETURN_FAILURE
◆ MPU_FIREWALL_readFaultStatus()
| Fwl_Return_t MPU_FIREWALL_readFaultStatus |
( |
uint32_t |
firewallId, |
|
|
uint32_t * |
faultStatus |
|
) |
| |
Function to read the fault status register. It contains information on the kind of firewall violation that had occurred.
- Parameters
-
| firewallId | MPU Firewall Id |
| faultStatus | pointer to the faultStatus to be populated |
- Returns
- FWL_DRV_RETURN_SUCCESS on successful fault status read; else FWL_DRV_RETURN_FAILURE
◆ MPU_FIREWALL_getInterruptStatus()
| Fwl_Return_t MPU_FIREWALL_getInterruptStatus |
( |
uint32_t |
firewallId, |
|
|
uint32_t * |
interruptStatus |
|
) |
| |
Function to read interrupt status.
- Parameters
-
| firewallId | MPU Firewall Id |
| interruptStatus | pointer to the interruptStatus to be populated |
- Returns
- FWL_DRV_RETURN_SUCCESS on successful interrupt status read; else FWL_DRV_RETURN_FAILURE