This example is a application which demonstrates the LIN message communication. Instance LIN1 is set to Transmit as well as Recieve.
The LIN1 instance initiates the transmission by sending LINID followed by message. It receives the same message.
| Parameter | Value |
|---|---|
| CPU + OS | r5fss0-0 freertos |
| r5fss0-0 nortos | |
| Toolchain | ti-arm-clang |
| Boards | am263px-cc, am263px-lp |
| Example folder | examples/drivers/lin/lin_loopback_interrupt |
Shown below is a sample output when the application is run,