This example demonstrates setting of multiple LED at the same time connected to the same I2C controller. It makes use of the I2C LLD Driver and it's interrupt transfer API.
The application will blink all the I2C controlled LED in the EVM.
Application exits after 10 iterations.
| Parameter | Value |
|---|---|
| CPU + OS | r5fss0-0 nortos |
| Toolchain | ti-arm-clang |
| Boards | am263px-cc, am263px-lp |
| Example folder | examples/drivers/i2c/i2c_led_blink_interrupt_lld |
Shown below is a sample output when the application is run,