AM263Px MCU+ SDK  11.00.00
EPWM valley switching

Introduction

EPWM Valley Switching

This example configures ePWMx as follows

  • ePWMx with DCAEVT1 forcing the ePWM output LOW
  • GPIO_A is used as the input to the INPUT XBAR INPUT1
  • INPUT1 (from INPUT XBAR) is used as the source for DCAEVT1
  • GPIO_B is set to output and toggled in the main loop to trip the PWM
  • ePWMx with DCBEVT1 forcing the ePWM output LOW
  • GPIO_A is used as the input to the INPUT XBAR INPUT1
  • INPUT1 (from INPUT XBAR) is used as the source for DCBEVT1
  • GPIO_B is set to output and toggled in the main loop to trip the PWM
  • DCBEVT1 uses the filtered version of DCBEVT1
  • The DCFILT signal uses the valley switching module to delay the
  • DCFILT signal by a software defined DELAY value.

Block Diagram for EPWM Valley Switching example

External Connections

  • For AM263x-CC or AM263Px-CC or AM261x-SOM
    • GPIO48 is connected to GPIO122.
    • EPWM0_A and EPWM0_B pin can be connected to an oscilloscope to view the waveform.
  • For AM263x-LP or AM263Px-LP
    • GPIO11 is connected to GPIO12.
    • EPWM1_A and EPWM1_B pin can be connected to an oscilloscope to view the waveform.
  • For AM261x-LP
    • GPIO5 is connected to GPIO6.
    • EPWM1_A and EPWM1_B pin can be connected to an oscilloscope to view the waveform.

AM263X-CC or AM263PX-CC or AM261X-SOM

When using AM263x-CC, AM263Px-CC or AM261x-SOM with TMDSHSECDOCK (HSEC180 controlCARD Baseboard Docking Station)

  • Connect HSEC Pin 52 to HSEC Pin 72
  • Capture waveform on HSEC Pin 49 for epwm0_A
  • Capture waveform on HSEC Pin 51 for epwm0_B

AM263X-LP or AM263PX-LP

  • Connect boosterpack header J1/J3 pin 7 to J2/J4 pin 18
  • Capture waveform on boosterpack header J2/J4 Pin 37 for epwm1_A
  • Capture waveform on boosterpack header J2/J4 Pin 38 for epwm1_B

AM261X-LP

  • Connect boosterpack header J6/J8 pin 52 to J6/J8 53
  • Capture waveform on boosterpack header J5/J7 Pin 69 for epwm1_A
  • Capture waveform on boosterpack header J5/J7 Pin 63 for epwm1_B

Supported Combinations

Parameter Value
CPU + OS r5fss0-0 nortos
Toolchain ti-arm-clang
Board am263px-cc, am263px-lp
Example folder examples/drivers/epwm/epwm_valley_switching

Steps to Run the Example

  • When using CCS projects to build, import the CCS project for the required combination and build it using the CCS project menu (see Using SDK with CCS Projects).
  • When using makefiles to build, note the required combination and build using make command (see Using SDK with Makefiles)
  • Establish connections as mentioned in External Connections section
  • Launch a CCS debug session and run the executable, see CCS Launch, Load and Run

See Also

EPWM

Sample Output

Shown below is a sample output when the application is run,

EPWM Valley Switching Test Started ...
EPWM Valley Switching Test Passed!!
All tests have passed!!

EPWM Valley Switching waveform