AM263Px MCU+ SDK  11.00.00
EPWM Hr Updown

Introduction

EPWM HR UpDown

This example modifies the MEP control registers to show edge displacement for high-resolution period with ePWM in Up-Down count mode due to the HRPWM control extension of the respective ePWM module.

Block Diagram for EPWM HR UpDown example

External Connections

  • Pin can be connected to high resolution oscilloscope (1 GHz) to observe the edge displacement.

AM263X-CC or AM263PX-CC or AM261X-SOM

When using with TMDSHSECDOCK (HSEC180 controlCARD Baseboard Docking Station)

  • Capture waveform on HSEC Pin 49, 51 for epwm0
  • Capture waveform on HSEC Pin 53, 55 for epwm1
  • Capture waveform on HSEC Pin 50, 52 for epwm2
  • Capture waveform on HSEC Pin 54, 56 for epwm3
  • Capture waveform on HSEC Pin 57, 59 for epwm4

AM263X-LP or AM263PX-LP

When using AM263X-LP or AM263PX-LP

  • Capture waveform on J2.11 / J6.59 for epwm0
  • Capture waveform on J4.37 / J4.38 for epwm1
  • Capture waveform on J4.39 / J4.40 for epwm2
  • Capture waveform on J8.77 / J8.78 for epwm3
  • Capture waveform on J8.75 / J8.76 for epwm9

AM261X-LP

When using AM261X-LP

  • Capture waveform on J7.69 / J7.63 for epwm1
  • Capture waveform on J4.40 / J4.39 for epwm2
  • Capture waveform on J4.38 / J4.37 for epwm3
  • Capture waveform on J4.36 / J4.35 for epwm4
  • Capture waveform on J8.78 / J8.77 for epwm6

Supported Combinations

Parameter Value
CPU + OS r5fss0-0 nortos
Toolchain ti-arm-clang
Board am263px-cc
Example folder examples/drivers/epwm/epwm_hr_updown

Steps to Run the Example

  • When using CCS projects to build, import the CCS project for the required combination and build it using the CCS project menu (see Using SDK with CCS Projects).
  • When using makefiles to build, note the required combination and build using make command (see Using SDK with Makefiles)
  • Establish connections as mentioned in External Connections section
  • Launch a CCS debug session and run the executable, see CCS Launch, Load and Run

See Also

EPWM

Sample Output

Shown below is a sample output when the application is run,

EPWM High Resolution Up Down Test Started ...
Please wait for 60 secs
EPWM High Resolution Up Down Test Passed!!
All tests have passed!!

EPWM HR UpDown waveform