Introduction
This example demostrates how the RTI and ADC to be configured so that the ADC SOC can be triggered from the RTI Events.
Configurations
- RTI is configured to generate trigger every 5uS. Refer to the syscfg of the RTI for the configurational details
- ADC SOC0 is configured for RTI trigger and generate interrupt at EOC0
ISRs
App_adcISR
- ISR to read ADC SOC0 result and service the interrupt generated at EOC0. App_rtiISR
- ISR callback to service RTI interrupt.
Both ISR have a counter to increment on each call. these counters are compared for the validation of the ADC triggers from RTI.
External Connections
Feed Analog voltages on ADC0_AIN2
AM263x-CC E2 or AM263Px-CC E2 or AM261X-SOM E1
- ADC0_AIN2, i.e., HSEC PIN 15
AM263x-LP or AM263Px-LP
- ADC0_AIN2, i.e., J5/7 PIN 66
AM261x-LP
- ADC0_AIN2, i.e., J5/7 PIN 64, this needs IO Expander Configurations, Check Syscfg and/or schematics
Watch Variables
The below watch variables can be used to view ADC conversion results.
- gAdcResults[] : Digital representation of the voltage sample on pin AIN2 of ADC0, triggered by RTI
- gAdcIsrCount : counter for the ADC ISR
- gRtiIsrCount : counter for the RTI ISR
Supported Combinations
| Parameter | Value |
| CPU + OS | r5fss0-0 nortos |
| Toolchain | ti-arm-clang |
| Board | am263px-cc, am263px-lp |
| Example folder | examples/drivers/adc/adc_soc_rti/ |
Steps to Run the Example
- When using CCS projects to build, import the CCS project for the required combination and build it using the CCS project menu (see Using SDK with CCS Projects).
- When using makefiles to build, note the required combination and build using make command (see Using SDK with Makefiles)
- Establish connections as mentioned in External Connections section
- Launch a CCS debug session and run the executable, see CCS Launch, Load and Run
- Using watch variables, view the ADC conversion results.
- View the ADC conversion results in UART console logs
See Also
ADC
Sample Output
Shown below is a sample output when the application is run,
ADC Triggered by RTI Test Started ...
ADC Triggered by RTI Test Passed
All tests have passed!!