Introduction
Example Description
This example demonstrates the PPB offset features of Post Processing Blocks of ADC. The PPB offset features are the following,
- PPB Calibration Offset
- This is used for correcting the calibration offset of the selected SOC result.
- For example, when set the ADC result corresponding to the set SOC ADC_result = ADC_result - PPB Calibration value.
- If more than one PPB are set for the given SOC, then the result with higher value after calculation will be implemented.
- PPB Reference Offset
- This can be used to calculate an offset from a given reference.
- The result will be specific to the PPB registers and is stored seperately from the SOC result.
- For example, when set, the PPB result corresponding to the set SOC ADC_result, PPB_result = ADC_result - PPB Reference value.
- If "Twos complement mode" is selected, then, PPB_result = PPB Reference value - ADC_result
SOC Configurations
ADC SOC0 and SOC1 are set for Channel 0, with sample window 17 each and are triggered by only software.
PPB Configurations
- PPB1
- Set to SOC1
- Calibration Offset Value is set to -100
- Reference Offset Value is set to 0
- Twos Complement mode is disabled
- PPB2
- Set to SOC1
- Calibration Offset Value is set to 50
- Reference Offset Value is set to 50
- Twos Complement mode is disabled
- PPB3
- Set to SOC1
- Calibration Offset Value is set to 100
- Reference Offset Value is set to 50
- Twos Complement mode is enabled
Interrupt Configurations
- ADC1_INT1 is set to EOC/SOC1.
External Connections
AM263PX-CC E2 or AM263X-CC E2 or AM261X-SOM E1
- Feed Analog Input to ADC1_AIN0, HSEC Pin 12
AM263X-CC E1
- Feed Analog Input to ADC1_AIN0, HSEC Pin 18
AM263PX-LP or AM263X-LP or AM261X-LP
- Feed Analog Input to ADC1_AIN0, J1/3 Pin 24
Watch Variables
- gAdc1Soc0Result[] holds the digital representation of the Analog signal on ADC1_AIN0
- gAdc1Soc1Result[] holds the digital representation of the Analog signal on ADC1_AIN0 with Calibration offset
- gAdc1PPB1Result[] holds the digital representation of the Analog signal on ADC1_AIN0 with Calibration offset with Reference Offset of 0
- gAdc1PPB2Result[] holds the digital representation of the Analog signal on ADC1_AIN0 with Calibration offset with Reference Offset of 50
- gAdc1PPB3Result[] holds the digital representation of the Analog signal on ADC1_AIN0 with Calibration offset with Reference Offset of 50 and Twos complement enabled.
Supported Combinations
| Parameter | Value |
| CPU + OS | r5fss0-0 nortos |
| Toolchain | ti-arm-clang |
| Board | am263px-cc, am263px-lp |
| Example folder | examples/drivers/adc/adc_ppb_offset/ |
Steps to Run the Example
- When using CCS projects to build, import the CCS project for the required combination and build it using the CCS project menu (see Using SDK with CCS Projects).
- When using makefiles to build, note the required combination and build using make command (see Using SDK with Makefiles)
- Establish connections as mentioned in External Connections section
- Launch a CCS debug session and run the executable, see CCS Launch, Load and Run
- Using the watch variables, view the ADC conversion results.
- Observe 6 EPWM waveforms. After ADC input voltage exceeds the PPB limit, PWMs get tripped.
See Also
ADC
Sample Output
Shown below is a sample output when the application is run,
ADC PPB Offset Test Started
SOC0 SOC1(SOC0 result + calibration offset) PPB1(SOC1 result) PPB2(SOC1 result + ref offset) PPB3(PPB2 result in 2's complement)
777 675 675 625 -625
776 675 675 625 -625
772 674 674 624 -624
776 676 676 626 -626
776 676 676 626 -626
775 675 675 625 -625
775 674 674 624 -624
777 675 675 625 -625
ADC PPB Offset Test Passed
All tests have passed!!