Introduction
This example sets up ePWM0 to periodically trigger a set of conversions (SOC0,1,12,13,14,15) on ADC1 for conversion of inputs on ADC_AIN0, ADC_AIN1 and burst mode conversion on ADC_AIN3. This demonstrates a batch of conversion on ADC1 (inputs on ADC_AIN0 and ADC_AIN1) and burst mode conversion on ADC1 (input ADC_AIN3). ADC1 Interrupt ISR is used to read results of ADC1 (i.e. digital representations of inputs ADC_AIN0, ADC_AIN1 and average of oversampled ADC_AIN3)
Module Block diagram
The example does the below
- Configures SOC0,1,2 of ADC1, as high priority SOCs, to be triggered by EPWM0.
- Configures ADC interrupt 0 to be generated at end of conversion of SOC12.
- ADC1 Interrupt ISR is used to read results of ADC1 from SOC0,SOC1 and average of SOC12 through SOC15.
Watch Variables
- The watch variables gAdc1Result0, gAdc1Result1, gAdc1Result2 storing ADC conversion outputs can be used to view the results.
External Connections
- ADC1_AIN0, ADC1_AIN1, ADC1_AIN3 pins should be connected to signals to be converted.
AM263PX-CC E2 or AM263X-CC E2 or AM261X-SOM
When using with TMDSHSECDOCK (HSEC180 controlCARD Baseboard Docking Station)
- Feed analog inputs
- ADC1_AIN0 - HSEC 12
- ADC1_AIN1 - HSEC 14
- ADC1_AIN3 - HSEC 20
AM263X-CC E1
When using E1 with TMDSHSECDOCK (HSEC180 controlCARD Baseboard Docking Station)
- Feed analog inputs
- ADC1_AIN0 - HSEC 18
- ADC1_AIN1 - HSEC 20
- ADC1_AIN3 - HSEC 23
AM263PX-LP or AM263X-LP
When using LP
- Feed analog inputs (non-zero volatage) to Boosterpack header Pin 24, Pin 29 and Pin 6.
AM261X-LP
When using AM261x-LP
- Feed Analog Inputs to the Boosterpack Headers at the following
- ADC1_AIN0 - J5 pin 24
- ADC1_AIN1 - J5 pin 42
- ADC1_AIN3 - J5 pin 46
Supported Combinations
| Parameter | Value |
| CPU + OS | r5fss0-0 nortos |
| Toolchain | ti-arm-clang |
| Board | am263px-cc, am263px-lp |
| Example folder | examples/drivers/adc/adc_burst_mode_oversampling/ |
Steps to Run the Example
- When using CCS projects to build, import the CCS project for the required combination and build it using the CCS project menu (see Using SDK with CCS Projects).
- When using makefiles to build, note the required combination and build using make command (see Using SDK with Makefiles)
- Establish connections as mentioned in External Connections section.
- Launch a CCS debug session and run the executable, see CCS Launch, Load and Run
- Using the watch variables, view the ADC conversion results.
- View the ADC conversion results in UART console logs
See Also
ADC
Sample Output
Shown below is a sample output when the application is run,
ADC EPWM Triggered Burst Mode Conversions Test Started ...
ADC1 SOC0 : SOC1 : SOC2 : Result register value :
3379 : 2364 : 1524
1158 : 2314 : 1519
1158 : 2314 : 1522
1157 : 2314 : 1524
1158 : 2313 : 1520
1158 : 2313 : 1523
1158 : 2314 : 1522
1158 : 2313 : 1520
1157 : 2313 : 1527
1158 : 2314 : 1522
1158 : 2314 : 1518
ADC Burst Mode Oversampling Test Passed
All tests have passed!!