|
AM263Px MCU+ SDK
09.02.00
|
|
Go to the documentation of this file.
33 #ifndef UART_DMA_EDMA_H_
34 #define UART_DMA_EDMA_H_
43 typedef struct UART_EdmaChConfig_s
uint32_t edmaTxParam
Definition: uart_dma_edma.h:59
uint32_t edmaTxChId
Definition: uart_dma_edma.h:55
EDMA interrupt configuration object. The object is passed to the EDMA_registerIntr() function....
Definition: edma/v0/edma.h:479
uint32_t edmaTccTx
Definition: uart_dma_edma.h:49
uint32_t edmaRxParam
Definition: uart_dma_edma.h:57
uint32_t edmaDummyParam
Definition: uart_dma_edma.h:61
uint32_t edmaRxChId
Definition: uart_dma_edma.h:53
uint32_t edmaBaseAddr
Definition: uart_dma_edma.h:65
uint32_t edmaTccDummy
Definition: uart_dma_edma.h:51
This file contains the prototype of EDMA driver APIs.
Edma_IntrObject edmaIntrObjDummy
Definition: uart_dma_edma.h:71
void * drvHandle
Definition: uart_dma_edma.h:45
uint32_t isOpen
Definition: uart_dma_edma.h:73
Edma_IntrObject edmaIntrObjRx
Definition: uart_dma_edma.h:67
uint32_t edmaRegionId
Definition: uart_dma_edma.h:63
uint32_t edmaTccRx
Definition: uart_dma_edma.h:47
Definition: uart_dma_edma.h:44
Edma_IntrObject edmaIntrObjTx
Definition: uart_dma_edma.h:69