AM263Px MCU+ SDK  09.02.00
esmInfo_t Struct Reference

Detailed Description

Structure for accessing information register of ESM module.

Data Fields

uint32_t lastRstType
 
uint32_t plsGrpNum
 
uint32_t lvlGrpNum
 

Field Documentation

◆ lastRstType

uint32_t esmInfo_t::lastRstType

Last reset type 0 – Last reset was a Power On Reset 1 – Last reset was a Warm Reset

◆ plsGrpNum

uint32_t esmInfo_t::plsGrpNum

Number of event groups that are pulse

◆ lvlGrpNum

uint32_t esmInfo_t::lvlGrpNum

Number of event groups that are level