AM263Px MCU+ SDK  09.02.00
cb_rawsock_ovip_para_t Struct Reference

Detailed Description

parameters to open the over IP mode raw socket, the values are in host order

Data Fields

uint32_t laddr
 local IP address More...
 
uint16_t lport
 local IP port More...
 
uint32_t daddr
 destination IP address More...
 
uint16_t dport
 destination IP port More...
 

Field Documentation

◆ laddr

uint32_t cb_rawsock_ovip_para_t::laddr

local IP address

◆ lport

uint16_t cb_rawsock_ovip_para_t::lport

local IP port

◆ daddr

uint32_t cb_rawsock_ovip_para_t::daddr

destination IP address

◆ dport

uint16_t cb_rawsock_ovip_para_t::dport

destination IP port