AM263Px MCU+ SDK  09.02.00

Detailed Description

This is SWRev type which holds the information regarding Revision identifier and value corresponding to it .

Parameters
revValuestores software revision value retreived from sec manager.
revIdrevision identifier
rsvdreserved for future use.

Data Fields

uint32_t revValue
 
uint8_t revId
 
uint8_t rsvd [3]
 

Field Documentation

◆ revValue

uint32_t SWRev_t::revValue

Value for sw rev retreived from sec manager.

◆ revId

uint8_t SWRev_t::revId

revision identifier

◆ rsvd

uint8_t SWRev_t::rsvd[3]

Reserved