AM263Px MCU+ SDK  09.02.00
SDL_CCM_staticRegs Struct Reference

Detailed Description

CCM Static Register.

This is the structure that is used to return the static registers in the static registers readback function

Data Fields

volatile uint32_t CCMKEYR1
 
volatile uint32_t CCMKEYR2
 
volatile uint32_t CCMKEYR3
 
volatile uint32_t CCMPOLCNTRL
 

Field Documentation

◆ CCMKEYR1

volatile uint32_t SDL_CCM_staticRegs::CCMKEYR1

◆ CCMKEYR2

volatile uint32_t SDL_CCM_staticRegs::CCMKEYR2

◆ CCMKEYR3

volatile uint32_t SDL_CCM_staticRegs::CCMKEYR3

◆ CCMPOLCNTRL

volatile uint32_t SDL_CCM_staticRegs::CCMPOLCNTRL