AM263Px MCU+ SDK  09.02.00

Detailed Description

Structure holding the hs mmcsd controller command object.

Data Fields

MMCSD_cmd cmd
 
uint32_t cmdArg
 
uint32_t enableData
 
uint32_t numBlks
 
uint32_t enableDma
 

Field Documentation

◆ cmd

MMCSD_cmd MMCSD_cmdObj::cmd

Command to be passed to the controller/card.

◆ cmdArg

uint32_t MMCSD_cmdObj::cmdArg

Argument for the command.

◆ enableData

uint32_t MMCSD_cmdObj::enableData

This flag enables/disables data transfer. This can take following two values:

  • TRUE - Enable data transfer
  • FALSE - Disable data transfer.

◆ numBlks

uint32_t MMCSD_cmdObj::numBlks

Transfer data length in number of blocks (multiple of BLEN). This can take values in the following range: 1 <= numBlks <= 65535. Value of 0 means Stop count.

◆ enableDma

uint32_t MMCSD_cmdObj::enableDma

This flag enables/disables Dma. This can take following two values:

  • TRUE - Enable DMA.
  • FALSE - Disable DMA.