AM263Px MCU+ SDK  09.02.00
MCAN_RevisionId Struct Reference

Detailed Description

Structure for accessing Revision ID and Core Release Info. of MCAN module.

Data Fields

uint32_t scheme
 
uint32_t bu
 
uint32_t modId
 
uint32_t rtlRev
 
uint32_t major
 
uint32_t custom
 
uint32_t minor
 
uint32_t day
 
uint32_t mon
 
uint32_t year
 
uint32_t subStep
 
uint32_t step
 
uint32_t rel
 

Field Documentation

◆ scheme

uint32_t MCAN_RevisionId::scheme

Scheme

◆ bu

uint32_t MCAN_RevisionId::bu

Business Unit: 10 = Processors

◆ modId

uint32_t MCAN_RevisionId::modId

Module ID

◆ rtlRev

uint32_t MCAN_RevisionId::rtlRev

RTL revision

◆ major

uint32_t MCAN_RevisionId::major

Major revision

◆ custom

uint32_t MCAN_RevisionId::custom

Custom revision

◆ minor

uint32_t MCAN_RevisionId::minor

Minor revision

◆ day

uint32_t MCAN_RevisionId::day

Time Stamp Day. Two digits, BCD-coded.

◆ mon

uint32_t MCAN_RevisionId::mon

Time Stamp Month. Two digits, BCD-coded.

◆ year

uint32_t MCAN_RevisionId::year

Time Stamp Year. Single digit, BCD-coded.

◆ subStep

uint32_t MCAN_RevisionId::subStep

Sub-step of Core Release Single digit, BCD-coded.

◆ step

uint32_t MCAN_RevisionId::step

Step of Core Release.Two digits, BCD-coded Single digit, BCD-coded.

◆ rel

uint32_t MCAN_RevisionId::rel

Core Release. Single digit, BCD-coded.