AM263Px MCU+ SDK  09.02.00
ICSS_EMAC_FwStaticMmap Struct Reference

Detailed Description

ICSS EMAC Static Firmware Memory Map offsets. These are offsets for PRU0 and PRU1 DRAM memory.

Data Fields

uint32_t versionOffset
 
uint32_t version2Offset
 
uint32_t featureOffset
 
uint32_t futureFeatureOffset
 
uint32_t statisticsOffset
 
uint32_t statisticsSize
 
uint32_t stormPreventionOffsetBC
 
uint32_t phySpeedOffset
 
uint32_t portStatusOffset
 
uint32_t portControlAddr
 
uint32_t portMacAddr
 
uint32_t rxInterruptStatusOffset
 
uint32_t stormPreventionOffsetMC
 
uint32_t stormPreventionOffsetUC
 
uint32_t p0QueueDescOffset
 
uint32_t p0ColQueueDescOffset
 
uint32_t emacTtsConfigBaseOffset
 
uint32_t interfaceMacAddrOffset
 
uint32_t colStatusAddr
 
uint32_t promiscuousModeOffset
 
uint32_t specialUnicastMACAddrOffset
 
uint32_t specialUnicastMACAddressFeatureEnableOffset
 

Field Documentation

◆ versionOffset

uint32_t ICSS_EMAC_FwStaticMmap::versionOffset

Version offset for release 1

◆ version2Offset

uint32_t ICSS_EMAC_FwStaticMmap::version2Offset

Version offset for release 2

◆ featureOffset

uint32_t ICSS_EMAC_FwStaticMmap::featureOffset

Feature offset

◆ futureFeatureOffset

uint32_t ICSS_EMAC_FwStaticMmap::futureFeatureOffset

Offset reserved for enhance features, future use

◆ statisticsOffset

uint32_t ICSS_EMAC_FwStaticMmap::statisticsOffset

Statistics offset

◆ statisticsSize

uint32_t ICSS_EMAC_FwStaticMmap::statisticsSize

Statistics block size

◆ stormPreventionOffsetBC

uint32_t ICSS_EMAC_FwStaticMmap::stormPreventionOffsetBC

Storm prevention offset

◆ phySpeedOffset

uint32_t ICSS_EMAC_FwStaticMmap::phySpeedOffset

Phy Speed Offset

◆ portStatusOffset

uint32_t ICSS_EMAC_FwStaticMmap::portStatusOffset

Port Status Offset

◆ portControlAddr

uint32_t ICSS_EMAC_FwStaticMmap::portControlAddr

Port Control Addr offset

◆ portMacAddr

uint32_t ICSS_EMAC_FwStaticMmap::portMacAddr

Port Mac Addr offset

◆ rxInterruptStatusOffset

uint32_t ICSS_EMAC_FwStaticMmap::rxInterruptStatusOffset

RX Interrupt Status Offset

◆ stormPreventionOffsetMC

uint32_t ICSS_EMAC_FwStaticMmap::stormPreventionOffsetMC

Storm prevention offset (multicast)

◆ stormPreventionOffsetUC

uint32_t ICSS_EMAC_FwStaticMmap::stormPreventionOffsetUC

Storm prevention offset (unicast)

◆ p0QueueDescOffset

uint32_t ICSS_EMAC_FwStaticMmap::p0QueueDescOffset

Port 0 QueueDescOffset

◆ p0ColQueueDescOffset

uint32_t ICSS_EMAC_FwStaticMmap::p0ColQueueDescOffset

Port 0 Collision QueueDescOffset

◆ emacTtsConfigBaseOffset

uint32_t ICSS_EMAC_FwStaticMmap::emacTtsConfigBaseOffset

TTS Config Base Offset

◆ interfaceMacAddrOffset

uint32_t ICSS_EMAC_FwStaticMmap::interfaceMacAddrOffset

Interface Mac AddressrOffset

◆ colStatusAddr

uint32_t ICSS_EMAC_FwStaticMmap::colStatusAddr

Collision status address offset

◆ promiscuousModeOffset

uint32_t ICSS_EMAC_FwStaticMmap::promiscuousModeOffset

promiscuous mode feature control offset

◆ specialUnicastMACAddrOffset

uint32_t ICSS_EMAC_FwStaticMmap::specialUnicastMACAddrOffset

Special Unicast MAC address offset

◆ specialUnicastMACAddressFeatureEnableOffset

uint32_t ICSS_EMAC_FwStaticMmap::specialUnicastMACAddressFeatureEnableOffset

Special Unicast MAC address feature enable/disable offset