AM263Px MCU+ SDK  09.02.00
I2C_Memory_ExtendedParams Struct Reference

Detailed Description

Data Fields

I2C_ExtendedParams extendedParams
 
uint32_t memAddr
 
uint8_t memAddrSize
 

Field Documentation

◆ extendedParams

I2C_ExtendedParams I2C_Memory_ExtendedParams::extendedParams

[IN] Extended Parameters

◆ memAddr

uint32_t I2C_Memory_ExtendedParams::memAddr

[IN] Memory address to write to or read from

◆ memAddrSize

uint8_t I2C_Memory_ExtendedParams::memAddrSize

[IN] Memory address size I2CLLD_MemoryAddrSize