AM263Px MCU+ SDK  09.02.00
EventP_Object Struct Reference

Detailed Description

Opaque Event object used with the Event APIs.

Data Fields

uintptr_t rsv [EventP_OBJECT_SIZE_MAX/sizeof(uint32_t)]
 

Field Documentation

◆ rsv

uintptr_t EventP_Object::rsv[EventP_OBJECT_SIZE_MAX/sizeof(uint32_t)]

reserved, should NOT be modified by end users