AM263Px MCU+ SDK  09.02.00
EnetTas_ConfigStatus Struct Reference

Detailed Description

Config state machine variables. See IEEE Std 802.1Q-2018 8.6.8.4.

Data Fields

uint64_t configChangeTime
 
uint32_t configChangeErrorCounter
 
uint8_t configPending
 
uint8_t configChange
 

Field Documentation

◆ configChangeTime

uint64_t EnetTas_ConfigStatus::configChangeTime

New list is copied at this time.

◆ configChangeErrorCounter

uint32_t EnetTas_ConfigStatus::configChangeErrorCounter

Config change error counter, incremented if admin->baseTime < current time and TAS_enabled is true.

◆ configPending

uint8_t EnetTas_ConfigStatus::configPending

True if list update is pending.

◆ configChange

uint8_t EnetTas_ConfigStatus::configChange

Set to true when application trigger updating of admin list to active list, cleared when configChangeTime is updated.