AM263Px MCU+ SDK  09.02.00

Detailed Description

EEPROM device attributes, these are filled by SysCfg based on the device that is selected.

Data Fields

uint32_t size
 
uint32_t pageCount
 
uint32_t pageSize
 

Field Documentation

◆ size

uint32_t EEPROM_Attrs::size

Size of EEPROM in bytes

◆ pageCount

uint32_t EEPROM_Attrs::pageCount

Number of pages

◆ pageSize

uint32_t EEPROM_Attrs::pageSize

Size of each page, in bytes