AM263Px MCU+ SDK  09.02.00
DTHE_Attrs Struct Reference

Detailed Description

DTHE attributes.

Data Fields

uint32_t caBaseAddr
 
uint32_t aesBaseAddr
 
uint32_t shaBaseAddr
 
uint32_t isOpen
 
uint32_t faultStatus
 

Field Documentation

◆ caBaseAddr

uint32_t DTHE_Attrs::caBaseAddr

Crypto Accelerator Base Adders

◆ aesBaseAddr

uint32_t DTHE_Attrs::aesBaseAddr

Aes Base address

◆ shaBaseAddr

uint32_t DTHE_Attrs::shaBaseAddr

sha Base address

◆ isOpen

uint32_t DTHE_Attrs::isOpen

Flag to indicate whether the instance is opened already

◆ faultStatus

uint32_t DTHE_Attrs::faultStatus

Flag to ascertain whether the handle was opened successfully