Struct holds the Resolver Core Configurations Can be passed to RDC_coreParamsInit(Core_config_t* coreParams); Note : this is also called in the RDC_paramsInit(RDC_configParams* params);.
◆ BpfDc_bpfEnable
| bool Core_config_t::BpfDc_bpfEnable |
◆ BpfDc_offsetCorrectionEnable
| bool Core_config_t::BpfDc_offsetCorrectionEnable |
◆ BpfDc_dcOffCal1
| uint8_t Core_config_t::BpfDc_dcOffCal1 |
◆ BpfDc_dcOffCal2
| uint8_t Core_config_t::BpfDc_dcOffCal2 |
◆ BpfDc_manualSin
| int16_t Core_config_t::BpfDc_manualSin |
◆ BpfDc_manualCos
| int16_t Core_config_t::BpfDc_manualCos |
◆ IdealSample_overrideValue
| uint8_t Core_config_t::IdealSample_overrideValue |
◆ IdealSample_absThresholdValue
| uint16_t Core_config_t::IdealSample_absThresholdValue |
◆ IdealSample_sampleAdjustCount
| uint8_t Core_config_t::IdealSample_sampleAdjustCount |
◆ IdealSample_mode
| uint8_t Core_config_t::IdealSample_mode |
◆ IdealSample_bottomSampleEnable
| bool Core_config_t::IdealSample_bottomSampleEnable |
◆ Pg_estimationEnable
| bool Core_config_t::Pg_estimationEnable |
◆ Pg_estimationLimit
| uint8_t Core_config_t::Pg_estimationLimit |
◆ Pg_correctionEnable
| bool Core_config_t::Pg_correctionEnable |
◆ Pg_autoCorrectionEnable
| bool Core_config_t::Pg_autoCorrectionEnable |
◆ Pg_sinGainBypassValue
| int16_t Core_config_t::Pg_sinGainBypassValue |
◆ Pg_cosGainBypassValue
| int16_t Core_config_t::Pg_cosGainBypassValue |
◆ Pg_cosPhaseBypassValue
| int16_t Core_config_t::Pg_cosPhaseBypassValue |
◆ track2Constants