AM263Px MCU+ SDK  09.02.00
soc.h
Go to the documentation of this file.
1 /*
2  * Copyright (C) 2021-2023 Texas Instruments Incorporated
3  *
4  * Redistribution and use in source and binary forms, with or without
5  * modification, are permitted provided that the following conditions
6  * are met:
7  *
8  * Redistributions of source code must retain the above copyright
9  * notice, this list of conditions and the following disclaimer.
10  *
11  * Redistributions in binary form must reproduce the above copyright
12  * notice, this list of conditions and the following disclaimer in the
13  * documentation and/or other materials provided with the
14  * distribution.
15  *
16  * Neither the name of Texas Instruments Incorporated nor the names of
17  * its contributors may be used to endorse or promote products derived
18  * from this software without specific prior written permission.
19  *
20  * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
21  * "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
22  * LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
23  * A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT
24  * OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,
25  * SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT
26  * LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
27  * DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
28  * THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT
29  * (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
30  * OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
31  */
32 
33 #ifndef SOC_AM263PX_H_
34 #define SOC_AM263PX_H_
35 
36 #ifdef __cplusplus
37 extern "C"
38 {
39 #endif
40 
50 #include <kernel/dpl/SystemP.h>
51 #include <drivers/hw_include/cslr_soc.h>
52 #include "soc_xbar.h"
53 #include "soc_rcm.h"
54 
60 #define SOC_DOMAIN_ID_MAIN (0U)
61 
63 /*Control MMRs partition*/
64 #define MSS_CTRL_PARTITION0 (1)
65 #define TOP_CTRL_PARTITION0 (2)
66 #define CONTROLSS_CTRL_PARTITION0 (3)
67 
68 /*Clock and reset MMRs partition*/
69 #define MSS_RCM_PARTITION0 (4)
70 #define TOP_RCM_PARTITION0 (5)
71 
72 /*Pinmux MMR*/
73 //#define IOMUX_PARTITION0 (6)
74 
75 
76 /* define the unlock and lock values for MSS_CTRL, TOP_CTRL, MSS_RCM, TOP_RCM*/
77 #define KICK_LOCK_VAL (0x00000000U)
78 #define KICK0_UNLOCK_VAL (0x01234567U)
79 #define KICK1_UNLOCK_VAL (0x0FEDCBA8U)
80 
81 /* defines the Inputs to the SOC_selectAdcExtChXbarAPI for extChXbarIn param */
82 #define ADC0_EXTCHSEL_BIT0 (0U)
83 #define ADC0_EXTCHSEL_BIT1 (1U)
84 #define ADC1_EXTCHSEL_BIT0 (2U)
85 #define ADC1_EXTCHSEL_BIT1 (3U)
86 #define ADC2_EXTCHSEL_BIT0 (4U)
87 #define ADC2_EXTCHSEL_BIT1 (5U)
88 #define ADC3_EXTCHSEL_BIT0 (6U)
89 #define ADC3_EXTCHSEL_BIT1 (7U)
90 #define ADC4_EXTCHSEL_BIT0 (8U)
91 #define ADC4_EXTCHSEL_BIT1 (9U)
92 #define ADC_R0_EXTCHSEL_BIT0 (10U)
93 #define ADC_R0_EXTCHSEL_BIT1 (11U)
94 #define ADC_R1_EXTCHSEL_BIT0 (12U)
95 #define ADC_R2_EXTCHSEL_BIT1 (13U)
96 
97 
98 #define ADC_EXTCHSELCT_DELAY_3_CYCLES (0U)
99 #define ADC_EXTCHSELCT_DELAY_6_CYCLES (1U)
100 
102 static inline int32_t MCSPI_lld_isBaseAddrValid(uint32_t baseAddr)
103 {
104  int32_t status = (int32_t)-3;
105 
106  if ((baseAddr == CSL_MCSPI0_U_BASE) || \
107  (baseAddr == CSL_MCSPI1_U_BASE) || \
108  (baseAddr == CSL_MCSPI2_U_BASE) || \
109  (baseAddr == CSL_MCSPI3_U_BASE) || \
110  (baseAddr == CSL_MCSPI4_U_BASE) || \
111  (baseAddr == CSL_MCSPI5_U_BASE) || \
112  (baseAddr == CSL_MCSPI6_U_BASE) || \
113  (baseAddr == CSL_MCSPI7_U_BASE) )
114  {
115  status = 0;
116  }
117 
118  return status;
119 }
120 #define IS_I2C_BASE_ADDR_VALID(baseAddr) ((baseAddr == CSL_I2C0_U_BASE) || \
121  (baseAddr == CSL_I2C1_U_BASE) || \
122  (baseAddr == CSL_I2C2_U_BASE) || \
123  (baseAddr == CSL_I2C3_U_BASE))
124 
134 int32_t SOC_moduleClockEnable(uint32_t moduleId, uint32_t enable);
135 
146 int32_t SOC_moduleSetClockFrequency(uint32_t moduleId, uint32_t clkId, uint64_t clkRate);
147 
155 const char *SOC_getCoreName(uint16_t coreId);
156 
162 uint64_t SOC_getSelfCpuClk(void);
163 
170 void SOC_controlModuleLockMMR(uint32_t domainId, uint32_t partition);
171 
178 void SOC_controlModuleUnlockMMR(uint32_t domainId, uint32_t partition);
179 
186 void SOC_setEpwmTbClk(uint32_t epwmInstance, uint32_t enable);
187 
194 void SOC_setMultipleEpwmTbClk(uint32_t epwmMask, uint32_t enable);
195 
201 void SOC_enableAdcReference(uint32_t adcInstance);
209 void SOC_enableAdcOsdChannel(uint32_t adcInstance, uint32_t channel, uint32_t enable);
210 
238 void SOC_setAdcOsdConfig(uint32_t adcInstance, uint32_t config);
239 
246 void SOC_enableAdcGlobalForce(uint32_t adcInstance, uint32_t enable);
247 
254 void SOC_adcSocGlobalForce(uint32_t socNumber);
275 void SOC_selectAdcExtChXbar(uint32_t extChXbarOut, uint32_t extChXbarIn);
276 
285 void SOC_selextAdcExtChDelay(uint32_t delay);
286 
292 void SOC_enableAdcDacLoopback(uint32_t enable);
293 
300 void SOC_setEpwmGroup(uint32_t epwmInstance, uint32_t group);
301 
307 void SOC_selectSdfm1Clk0Source(uint8_t source);
308 
309 
320 void SOC_sdfmClkLoopBackConfig(uint32_t sdfmInstance, uint32_t clkInstance, uint32_t defaultValue);
321 
327 void SOC_gateEpwmClock(uint32_t epwmInstance);
328 
334 void SOC_gateFsitxClock(uint32_t fsitxInstance);
335 
341 void SOC_gateFsirxClock(uint32_t fsirxInstance);
342 
348 void SOC_gateCmpssaClock(uint32_t cmpssaInstance);
349 
355 void SOC_gateCmpssbClock(uint32_t cmpssbInstance);
356 
362 void SOC_gateEcapClock(uint32_t ecapInstance);
363 
369 void SOC_gateEqepClock(uint32_t eqepInstance);
370 
376 void SOC_gateSdfmClock(uint32_t sdfmInstance);
377 
381 void SOC_gateDacClock(void);
382 
388 void SOC_gateAdcClock(uint32_t adcInstance);
389 
395 void SOC_gateRdcClock(uint32_t rdcInstance);
396 
402 void SOC_gateOttoClock(uint32_t ottoInstance);
403 
409 void SOC_gateSdfmPllClock(uint32_t sdfmInstance);
410 
416 void SOC_gateFsiPllClock(uint32_t fsiInstance);
417 
423 void SOC_generateEpwmReset(uint32_t ePWMInstance);
424 
430 void SOC_generateFsiTxReset(uint32_t fsitxInstance);
431 
437 void SOC_generateFsiRxReset(uint32_t fsirxInstance);
438 
444 void SOC_generateCmpssaReset(uint32_t cmpssaInstance);
445 
451 void SOC_generateCmpssbReset(uint32_t cmpssbInstance);
452 
458 void SOC_generateEcapReset(uint32_t ecapInstance);
459 
465 void SOC_generateEqepReset(uint32_t eqepInstance);
466 
472 void SOC_generateSdfmReset(uint32_t sdfmInstance);
473 
478 
484 void SOC_generateAdcReset(uint32_t adcInstance);
485 
491 void SOC_generateRdcReset(uint32_t rdcInstance);
492 
499 void Soc_enableEPWMHalt (uint32_t epwmInstance);
500 
506 void SOC_generateOttoReset(uint32_t ottoInstance);
507 
514 void SOC_selectIcssGpiMux(uint8_t pru_instance, uint32_t mask);
515 
523 uint64_t SOC_virtToPhy(void *virtAddr);
524 
532 void *SOC_phyToVirt(uint64_t phyAddr);
533 
540 
542 static inline int32_t UART_IsBaseAddrValid(uint32_t baseAddr)
543 {
544  int32_t status = (int32_t)-3;
545 
546  if(((baseAddr == CSL_UART0_U_BASE) ||
547  (baseAddr == CSL_UART1_U_BASE) ||
548  (baseAddr == CSL_UART2_U_BASE) ||
549  (baseAddr == CSL_UART3_U_BASE) ||
550  (baseAddr == CSL_UART4_U_BASE) ||
551  (baseAddr == CSL_UART5_U_BASE)))
552  {
553  status = 0;
554  }
555 
556  return status;
557 }
558 
561 #ifdef __cplusplus
562 }
563 #endif
564 
565 #endif
SOC_gateFsitxClock
void SOC_gateFsitxClock(uint32_t fsitxInstance)
Gate the FSI-TX clock.
SOC_moduleSetClockFrequency
int32_t SOC_moduleSetClockFrequency(uint32_t moduleId, uint32_t clkId, uint64_t clkRate)
Set module clock to specified frequency.
SOC_generateEcapReset
void SOC_generateEcapReset(uint32_t ecapInstance)
Generate ECAP reset.
SOC_gateEcapClock
void SOC_gateEcapClock(uint32_t ecapInstance)
Gate the ECAP clock.
SOC_controlModuleUnlockMMR
void SOC_controlModuleUnlockMMR(uint32_t domainId, uint32_t partition)
Unlock control module partition to allow writes into control MMRs.
SOC_selectAdcExtChXbar
void SOC_selectAdcExtChXbar(uint32_t extChXbarOut, uint32_t extChXbarIn)
Selects the ADC External Channel Select bit for the output from each xbar out.
SOC_selectIcssGpiMux
void SOC_selectIcssGpiMux(uint8_t pru_instance, uint32_t mask)
Selection of ICSS GPI MUX.
SOC_virtToPhy
uint64_t SOC_virtToPhy(void *virtAddr)
SOC Virtual (CPU) to Physical address translation function.
SOC_gateFsirxClock
void SOC_gateFsirxClock(uint32_t fsirxInstance)
Gate the FSI-RX clock.
SOC_gateSdfmPllClock
void SOC_gateSdfmPllClock(uint32_t sdfmInstance)
Gate the SDFM PLL clock.
SOC_gateCmpssaClock
void SOC_gateCmpssaClock(uint32_t cmpssaInstance)
Gate the CMPSS-A clock.
SystemP.h
SOC_gateCmpssbClock
void SOC_gateCmpssbClock(uint32_t cmpssbInstance)
Gate the CMPSS-B clock.
SOC_getFlashDataBaseAddr
uint32_t SOC_getFlashDataBaseAddr(void)
This function gets the SOC mapped data base address of the flash.
SOC_generateCmpssbReset
void SOC_generateCmpssbReset(uint32_t cmpssbInstance)
Generate CMPSS-B reset.
SOC_generateDacReset
void SOC_generateDacReset(void)
Generate DAC reset.
SOC_enableAdcReference
void SOC_enableAdcReference(uint32_t adcInstance)
Enable ADC references by writing to Control MMR.
SOC_gateOttoClock
void SOC_gateOttoClock(uint32_t ottoInstance)
Gate the OTTO clock.
soc_rcm.h
SOC_setMultipleEpwmTbClk
void SOC_setMultipleEpwmTbClk(uint32_t epwmMask, uint32_t enable)
Enable or disable Multiple ePWM time base clock from Control MMR.
SOC_setAdcOsdConfig
void SOC_setAdcOsdConfig(uint32_t adcInstance, uint32_t config)
Sets the ADC OSD Configuration.
SOC_gateEqepClock
void SOC_gateEqepClock(uint32_t eqepInstance)
Gate the EQEP clock.
SOC_generateAdcReset
void SOC_generateAdcReset(uint32_t adcInstance)
Generate ADC reset.
SOC_generateEpwmReset
void SOC_generateEpwmReset(uint32_t ePWMInstance)
Generate ePWM reset.
SOC_phyToVirt
void * SOC_phyToVirt(uint64_t phyAddr)
Physical to Virtual (CPU) address translation function.
SOC_gateDacClock
void SOC_gateDacClock(void)
Gate the DAC clock.
SOC_getSelfCpuClk
uint64_t SOC_getSelfCpuClk(void)
Get the clock frequency in Hz of the CPU on which the driver is running.
SOC_enableAdcGlobalForce
void SOC_enableAdcGlobalForce(uint32_t adcInstance, uint32_t enable)
Enable or Disable the ADC instnace for Gloabl SW force.
SOC_enableAdcOsdChannel
void SOC_enableAdcOsdChannel(uint32_t adcInstance, uint32_t channel, uint32_t enable)
Enable or disable the OSD circuit over the ADC channels.
SOC_generateRdcReset
void SOC_generateRdcReset(uint32_t rdcInstance)
Generate RDC reset.
SOC_selectSdfm1Clk0Source
void SOC_selectSdfm1Clk0Source(uint8_t source)
Select the SDFM1 CLK0 source.
SOC_selextAdcExtChDelay
void SOC_selextAdcExtChDelay(uint32_t delay)
Mux select to choose delay for ADC Extchsel.
UART_IsBaseAddrValid
static int32_t UART_IsBaseAddrValid(uint32_t baseAddr)
API to validate UART base address.
Definition: soc.h:542
SOC_gateFsiPllClock
void SOC_gateFsiPllClock(uint32_t fsiInstance)
Gate the FSI-TX PLL clock.
SOC_gateAdcClock
void SOC_gateAdcClock(uint32_t adcInstance)
Gate the ADC clock.
MCSPI_lld_isBaseAddrValid
static int32_t MCSPI_lld_isBaseAddrValid(uint32_t baseAddr)
API to validate MCSPI base address.
Definition: soc.h:102
SOC_controlModuleLockMMR
void SOC_controlModuleLockMMR(uint32_t domainId, uint32_t partition)
Lock control module partition to prevent writes into control MMRs.
SOC_moduleClockEnable
int32_t SOC_moduleClockEnable(uint32_t moduleId, uint32_t enable)
Enable clock to specified module.
SOC_generateCmpssaReset
void SOC_generateCmpssaReset(uint32_t cmpssaInstance)
Generate CMPSS-A reset.
SOC_generateSdfmReset
void SOC_generateSdfmReset(uint32_t sdfmInstance)
Generate SDFM reset.
SOC_gateEpwmClock
void SOC_gateEpwmClock(uint32_t epwmInstance)
Gate the ePWM clock.
SOC_adcSocGlobalForce
void SOC_adcSocGlobalForce(uint32_t socNumber)
Triggers a global force for the SOC in enabled ADCs the ADCs may be enabled by using SOC_enableAdcGlo...
SOC_getCoreName
const char * SOC_getCoreName(uint16_t coreId)
Convert a core ID to a user readable name.
SOC_setEpwmTbClk
void SOC_setEpwmTbClk(uint32_t epwmInstance, uint32_t enable)
Enable or disable ePWM time base clock from Control MMR.
SOC_setEpwmGroup
void SOC_setEpwmGroup(uint32_t epwmInstance, uint32_t group)
Configure the ePWM group.
SOC_gateSdfmClock
void SOC_gateSdfmClock(uint32_t sdfmInstance)
Gate the SDFM clock.
SOC_generateFsiRxReset
void SOC_generateFsiRxReset(uint32_t fsirxInstance)
Generate FSI-RX reset.
Soc_enableEPWMHalt
void Soc_enableEPWMHalt(uint32_t epwmInstance)
Halt EPWM with corresponding cPU.
SOC_generateEqepReset
void SOC_generateEqepReset(uint32_t eqepInstance)
Generate EQEP reset.
soc_xbar.h
SOC_generateOttoReset
void SOC_generateOttoReset(uint32_t ottoInstance)
Generate OTTO reset.
SOC_sdfmClkLoopBackConfig
void SOC_sdfmClkLoopBackConfig(uint32_t sdfmInstance, uint32_t clkInstance, uint32_t defaultValue)
Sets the configuraion for the loopback control.
SOC_gateRdcClock
void SOC_gateRdcClock(uint32_t rdcInstance)
Gate the HW_RESOLVER clock.
SOC_generateFsiTxReset
void SOC_generateFsiTxReset(uint32_t fsitxInstance)
Generate FSI-TX reset.
SOC_enableAdcDacLoopback
void SOC_enableAdcDacLoopback(uint32_t enable)
Enable or Disable the ADC CAL Pin to loopback with DAC.