AM263Px MCU+ SDK  09.02.00
sdlr.h
Go to the documentation of this file.
1 /* ============================================================================
2  * Copyright (c) Texas Instruments Incorporated 2022
3  *
4  * Redistribution and use in source and binary forms, with or without
5  * modification, are permitted provided that the following conditions
6  * are met:
7  *
8  * Redistributions of source code must retain the above copyright
9  * notice, this list of conditions and the following disclaimer.
10  *
11  * Redistributions in binary form must reproduce the above copyright
12  * notice, this list of conditions and the following disclaimer in the
13  * documentation and/or other materials provided with the
14  * distribution.
15  *
16  * Neither the name of Texas Instruments Incorporated nor the names of
17  * its contributors may be used to endorse or promote products derived
18  * from this software without specific prior written permission.
19  *
20  * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
21  * "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
22  * LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
23  * A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT
24  * OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,
25  * SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT
26  * LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
27  * DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
28  * THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT
29  * (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
30  * OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
31  *
32 */
40 /* Register layer central -- contains field-manipulation macro definitions */
41 
42 #ifndef SDLR_H
43 #define SDLR_H
44 #include <stdint.h>
45 
46 /* the "expression" macros */
47 
48 /* the Field MaKe macro */
49 #define SDL_FMK(PER_REG_FIELD, val) \
50  (((val) << SDL_##PER_REG_FIELD##_SHIFT) & SDL_##PER_REG_FIELD##_MASK)
51 
52 /* the Field EXTract macro */
53 #define SDL_FEXT(reg, PER_REG_FIELD) \
54  (((reg) & SDL_##PER_REG_FIELD##_MASK) >> SDL_##PER_REG_FIELD##_SHIFT)
55 
56 /* the Field INSert macro */
57 #define SDL_FINS(reg, PER_REG_FIELD, val) \
58  ((reg) = ((reg) & ~SDL_##PER_REG_FIELD##_MASK) \
59  | (((val) << SDL_##PER_REG_FIELD##_SHIFT) & SDL_##PER_REG_FIELD##_MASK))
60 
61 
62 /* the "token" macros */
63 
64 /* the Field MaKe (Token) macro */
65 #define SDL_FMKT(PER_REG_FIELD, TOKEN) \
66  (((SDL_##PER_REG_FIELD##_##TOKEN) << SDL_##PER_REG_FIELD##_SHIFT) & SDL_##PER_REG_FIELD##_MASK)
67 
68 /* the Field INSert (Token) macro */
69 #define SDL_FINST(reg, PER_REG_FIELD, TOKEN) \
70  ((reg) = ((reg) & ~SDL_##PER_REG_FIELD##_MASK) \
71  | (((SDL_##PER_REG_FIELD##_##TOKEN) << SDL_##PER_REG_FIELD##_SHIFT) & SDL_##PER_REG_FIELD##_MASK))
72 
73 
74 /* the "raw" macros */
75 #define kw_val (1u) \
76 
77 /* the Field MaKe (Raw) macro */
78 #define SDL_FMKR(msb, lsb, val) \
79  (((val) & ((((uint32_t)1U) << ((msb) - (lsb) + ((uint32_t)1U))) - ((uint32_t)1U))) << (lsb))
80 
81 /* the Field EXTract (Raw) macro */
82 #define SDL_FEXTR(reg, msb, lsb) \
83  (((reg) >> (lsb)) & ((((uint32_t)1U) << ((msb) - (lsb) + ((uint32_t)1U))) - ((uint32_t)1U)))
84 
85 /* the Field INSert (Raw) macro */
86 #define SDL_FINSR(reg, msb, lsb, val) \
87  ((reg) = ((reg) & (~(((((uint32_t)1U) << ((msb) - (lsb) + ((uint32_t)1U))) - ((uint32_t)1U)) << (lsb)))) \
88  | SDL_FMKR((msb), (lsb), (val)))
89 
99 #define SDL_REG_RD(p) (*(p))
100 
108 #define SDL_REG_WR(p, v) (*(p) = (v))
109 
118 #define SDL_REG32_RD(p) (SDL_REG32_RD_RAW((volatile uint32_t *) (p)))
119 
127 #define SDL_REG32_WR(p, v) (SDL_REG32_WR_RAW( \
128  (volatile uint32_t *) (p), (uint32_t) (v)))
129 
138 #define SDL_REG16_RD(p) (SDL_REG16_RD_RAW((volatile uint16_t *) (p)))
139 
147 #define SDL_REG16_WR(p, v) (SDL_REG16_WR_RAW( \
148  (volatile uint16_t *) (p), (uint16_t) (v)))
149 
158 #define SDL_REG8_RD(p) (SDL_REG8_RD_RAW((volatile uint8_t *) (p)))
159 
167 #define SDL_REG8_WR(p, v) (SDL_REG8_WR_RAW( \
168  (volatile uint8_t *) (p), (uint8_t) (v)))
169 
179 #define SDL_REG32_RD_OFF(p, off) (SDL_REG32_RD_OFF_RAW( \
180  (volatile uint32_t *) (p), \
181  (uint32_t) (off)))
182 
192 #define SDL_REG32_WR_OFF(p, off, v) (SDL_REG32_WR_OFF_RAW( \
193  (volatile uint32_t *) (p), \
194  (uint32_t) (off), \
195  (uint32_t) (v)))
196 
207 #define SDL_REG32_FEXT(p, fld) (SDL_REG32_FEXT_RAW( \
208  ((volatile uint32_t *) (p)), \
209  ((uint32_t) SDL_##fld##_MASK), \
210  ((uint32_t) SDL_##fld##_SHIFT)))
211 
222 #define SDL_REG16_FEXT(p, fld) (SDL_REG16_FEXT_RAW( \
223  ((volatile uint16_t *) (p)), \
224  ((uint16_t) SDL_##fld##_MASK), \
225  ((uint32_t) SDL_##fld##_SHIFT)))
226 
237 #define SDL_REG8_FEXT(p, fld) (SDL_REG8_FEXT_RAW( \
238  ((volatile uint8_t *) (p)), \
239  ((uint8_t) SDL_##fld##_MASK), \
240  ((uint32_t) SDL_##fld##_SHIFT)))
241 
251 #define SDL_REG32_FINS(p, fld, v) (SDL_REG32_FINS_RAW( \
252  ((volatile uint32_t *) (p)), \
253  ((uint32_t) SDL_##fld##_MASK), \
254  ((uint32_t) SDL_##fld##_SHIFT), \
255  ((uint32_t) v)))
256 
266 #define SDL_REG16_FINS(p, fld, v) (SDL_REG16_FINS_RAW( \
267  ((volatile uint16_t *) (p)), \
268  ((uint16_t) SDL_##fld##_MASK), \
269  ((uint32_t) SDL_##fld##_SHIFT), \
270  ((uint16_t) v)))
271 
281 #define SDL_REG8_FINS(p, fld, v) (SDL_REG8_FINS_RAW( \
282  ((volatile uint8_t *) (p)), \
283  ((uint8_t) SDL_##fld##_MASK), \
284  ((uint32_t) SDL_##fld##_SHIFT), \
285  ((uint8_t) v)))
286 
287 /* ========================================================================== */
288 /* Function Declarations */
289 /* ========================================================================== */
290 
299 static inline uint32_t SDL_REG32_RD_RAW(volatile const uint32_t * const p);
300 static inline uint32_t SDL_REG32_RD_RAW(volatile const uint32_t * const p)
301 {
302  return (*p);
303 }
304 
312 static inline void SDL_REG32_WR_RAW(volatile uint32_t * const p, uint32_t v);
313 static inline void SDL_REG32_WR_RAW(volatile uint32_t * const p, uint32_t v)
314 {
315  *p = v;
316  return;
317 }
318 
327 static inline uint16_t SDL_REG16_RD_RAW(volatile const uint16_t * const p);
328 static inline uint16_t SDL_REG16_RD_RAW(volatile const uint16_t * const p)
329 {
330  return (*p);
331 }
332 
340 static inline void SDL_REG16_WR_RAW(volatile uint16_t * const p, uint16_t v);
341 static inline void SDL_REG16_WR_RAW(volatile uint16_t * const p, uint16_t v)
342 {
343  *p = v;
344  return;
345 }
346 
355 static inline uint8_t SDL_REG8_RD_RAW(volatile const uint8_t * const p);
356 static inline uint8_t SDL_REG8_RD_RAW(volatile const uint8_t * const p)
357 {
358  return (*p);
359 }
360 
368 static inline void SDL_REG8_WR_RAW(volatile uint8_t * const p, uint8_t v);
369 static inline void SDL_REG8_WR_RAW(volatile uint8_t * const p, uint8_t v)
370 {
371  *p = v;
372  return;
373 }
374 
384 static inline uint32_t SDL_REG32_RD_OFF_RAW(volatile const uint32_t *p, uint32_t off);
385 static inline uint32_t SDL_REG32_RD_OFF_RAW(volatile const uint32_t *p, uint32_t off)
386 {
387  uintptr_t pOff = ((uintptr_t) p) + off;
388  return (*(volatile const uint32_t *)(pOff));
389 }
390 
400 static inline void SDL_REG32_WR_OFF_RAW(volatile uint32_t *const p,
401  uint32_t off,
402  uint32_t v);
403 static inline void SDL_REG32_WR_OFF_RAW(volatile uint32_t *const p,
404  uint32_t off,
405  uint32_t v)
406 {
407  uintptr_t pOff = ((uintptr_t) p) + off;
408  (*(volatile uint32_t *)(pOff)) = (v);
409  return;
410 }
411 
422 static inline uint32_t SDL_REG32_FEXT_RAW(volatile const uint32_t * const p,
423  uint32_t mask,
424  uint32_t shift);
425 static inline uint32_t SDL_REG32_FEXT_RAW(volatile const uint32_t * const p,
426  uint32_t mask,
427  uint32_t shift)
428 {
429  uint32_t regVal = SDL_REG32_RD_RAW(p);
430  regVal = (regVal & mask) >> shift;
431  return (regVal);
432 }
433 
444 static inline uint16_t SDL_REG16_FEXT_RAW(volatile const uint16_t * const p,
445  uint16_t mask,
446  uint32_t shift);
447 static inline uint16_t SDL_REG16_FEXT_RAW(volatile const uint16_t * const p,
448  uint16_t mask,
449  uint32_t shift)
450 {
451  uint16_t regVal = SDL_REG16_RD_RAW(p);
452  regVal = (regVal & mask) >> shift;
453  return (regVal);
454 }
455 
466 static inline uint8_t SDL_REG8_FEXT_RAW(volatile const uint8_t * const p,
467  uint8_t mask,
468  uint32_t shift);
469 static inline uint8_t SDL_REG8_FEXT_RAW(volatile const uint8_t * const p,
470  uint8_t mask,
471  uint32_t shift)
472 {
473  uint8_t regVal = SDL_REG8_RD_RAW(p);
474  regVal = (regVal & mask) >> shift;
475  return (regVal);
476 }
477 
487 static inline void SDL_REG32_FINS_RAW(volatile uint32_t * const p,
488  uint32_t mask,
489  uint32_t shift,
490  uint32_t v);
491 static inline void SDL_REG32_FINS_RAW(volatile uint32_t * const p,
492  uint32_t mask,
493  uint32_t shift,
494  uint32_t v)
495 {
496  uint32_t regVal = SDL_REG32_RD_RAW(p);
497  regVal = (regVal & ~(mask));
498  regVal |= (v << shift) & mask;
499  SDL_REG32_WR_RAW(p, regVal);
500  return;
501 }
502 
512 static inline void SDL_REG16_FINS_RAW(volatile uint16_t * const p,
513  uint16_t mask,
514  uint32_t shift,
515  uint16_t v);
516 static inline void SDL_REG16_FINS_RAW(volatile uint16_t * const p,
517  uint16_t mask,
518  uint32_t shift,
519  uint16_t v)
520 {
521  uint16_t regVal = SDL_REG16_RD_RAW(p);
522  regVal = (regVal & ~(mask));
523  regVal |= (v << shift) & mask;
524  SDL_REG16_WR_RAW(p, regVal);
525  return;
526 }
527 
537 static inline void SDL_REG8_FINS_RAW(volatile uint8_t * const p,
538  uint8_t mask,
539  uint32_t shift,
540  uint8_t v);
541 static inline void SDL_REG8_FINS_RAW(volatile uint8_t * const p,
542  uint8_t mask,
543  uint32_t shift,
544  uint8_t v)
545 {
546  uint8_t regVal = SDL_REG8_RD_RAW(p);
547  regVal = (regVal & ~(mask));
548  regVal |= (v << shift) & mask;
549  SDL_REG8_WR_RAW(p, regVal);
550  return;
551 }
552 
553 #endif /* SDLR_H_ */
SDL_REG8_RD_RAW
static uint8_t SDL_REG8_RD_RAW(volatile const uint8_t *const p)
This function reads a 8-bit value from a hardware register and returns the value.
Definition: sdlr.h:356
SDL_REG32_WR_OFF_RAW
static void SDL_REG32_WR_OFF_RAW(volatile uint32_t *const p, uint32_t off, uint32_t v)
This function writes a 32-bit value to a hardware register with an offset.
Definition: sdlr.h:403
SDL_REG8_FINS_RAW
static void SDL_REG8_FINS_RAW(volatile uint8_t *const p, uint8_t mask, uint32_t shift, uint8_t v)
This function reads a 8 bit register, modifies specific set of bits and writes back to the register.
Definition: sdlr.h:541
SDL_REG32_RD_OFF_RAW
static uint32_t SDL_REG32_RD_OFF_RAW(volatile const uint32_t *p, uint32_t off)
This function reads a 32-bit value from a hardware register with an offset and returns the value.
Definition: sdlr.h:385
SDL_REG16_RD_RAW
static uint16_t SDL_REG16_RD_RAW(volatile const uint16_t *const p)
This function reads a 16-bit value from a hardware register and returns the value.
Definition: sdlr.h:328
SDL_REG16_FINS_RAW
static void SDL_REG16_FINS_RAW(volatile uint16_t *const p, uint16_t mask, uint32_t shift, uint16_t v)
This function reads a 16 bit register, modifies specific set of bits and writes back to the register.
Definition: sdlr.h:516
SDL_REG16_FEXT_RAW
static uint16_t SDL_REG16_FEXT_RAW(volatile const uint16_t *const p, uint16_t mask, uint32_t shift)
This function reads a 16 bit register, masks specific set of bits and returns the left shifted value.
Definition: sdlr.h:447
SDL_REG16_WR_RAW
static void SDL_REG16_WR_RAW(volatile uint16_t *const p, uint16_t v)
This function writes a 16-bit value to a hardware register.
Definition: sdlr.h:341
SDL_REG8_WR_RAW
static void SDL_REG8_WR_RAW(volatile uint8_t *const p, uint8_t v)
This function writes a 8-bit value to a hardware register.
Definition: sdlr.h:369
SDL_REG32_RD_RAW
static uint32_t SDL_REG32_RD_RAW(volatile const uint32_t *const p)
This function reads a 32-bit value from a hardware register and returns the value.
Definition: sdlr.h:300
SDL_REG32_FINS_RAW
static void SDL_REG32_FINS_RAW(volatile uint32_t *const p, uint32_t mask, uint32_t shift, uint32_t v)
This function reads a 32 bit register, modifies specific set of bits and writes back to the register.
Definition: sdlr.h:491
SDL_REG8_FEXT_RAW
static uint8_t SDL_REG8_FEXT_RAW(volatile const uint8_t *const p, uint8_t mask, uint32_t shift)
This function reads a 8 bit register, masks specific set of bits and returns the left shifted value.
Definition: sdlr.h:469
SDL_REG32_WR_RAW
static void SDL_REG32_WR_RAW(volatile uint32_t *const p, uint32_t v)
This function writes a 32-bit value to a hardware register.
Definition: sdlr.h:313
SDL_REG32_FEXT_RAW
static uint32_t SDL_REG32_FEXT_RAW(volatile const uint32_t *const p, uint32_t mask, uint32_t shift)
This function reads a 32 bit register, masks specific set of bits and returns the left shifted value.
Definition: sdlr.h:425