|
AM263Px MCU+ SDK
09.02.00
|
|
Go to the documentation of this file.
35 #ifndef SDL_SOC_TOG_H_
36 #define SDL_SOC_TOG_H_
39 #include <sdl/include/am263px/sdlr_soc_baseaddress.h>
63 #define SDL_TOG_INSTANCE_TIMEOUT0_CFG 0U
65 #define SDL_TOG_MAX_INSTANCE 1U
67 #define SDL_TOG_INSTANCE 0U
105 SDL_MCU_TIMEOUT0_CFG_BASE
int32_t SDL_TOG_getBaseaddr(SDL_TOG_Inst instance, uint32_t *baseAddr)
This API is used to get the base address of the instance.
static uint32_t SDL_TOG_baseAddress[SDL_TOG_MAX_INSTANCE]
Definition: sdl_soc_tog.h:103
void SDL_TOG_irqHandler(void)
This API is the interrupt handler for TOG.
int32_t SDL_TOG_registerInterrupt(void)
This API is used to get the base address of the instance.
#define SDL_TOG_MAX_INSTANCE
Definition: sdl_soc_tog.h:65
uint8_t SDL_TOG_Inst
Definition: sdl_soc_tog.h:61
This file contains the macro definations for Register layer.