AM263Px MCU+ SDK  09.02.00
General types and functions

Introduction

Files

file  unibase.h
 unibase general global header
 

Data Structures

struct  unibase_cb_set_t
 a set of callback functions to process platform specific tasks More...
 
struct  unibase_init_para_t
 initialization parameters More...
 

Functions

int unibase_init (unibase_init_para_t *ub_init_para)
 initialize unibase More...
 
void unibase_close (void)
 claose unibase More...
 
void ub_fatal (const char *mes1, const char *mes2)
 process a fatal error More...
 
bool ub_fatalerror (void)
 return the fatal error status More...
 
static bool ub_assert_fatal (bool cond, const char *mes1, const char *mes2)
 conditinal ub_fatal More...
 
uint64_t ub_rt_gettime64 (void)
 get 64-bit REALTIME clock value More...
 
uint64_t ub_mt_gettime64 (void)
 get 64-bit MONOTONIC clock value More...
 
uint64_t ub_gptp_gettime64 (void)
 get 64-bit PTP clock value More...
 

Typedefs

typedef int(* ub_console_out) (bool flush, const char *str)
 console output function More...
 
typedef int(* ub_debug_out) (bool flush, const char *str)
 debug output function More...
 
typedef void *(* ub_mutex_init) (void)
 mutex initialization function More...
 
typedef int(* ub_mutex_close) (void *mutex)
 mutex de-initialization function More...
 
typedef int(* ub_mutex_lock) (void *mutex)
 mutex lock function More...
 
typedef int(* ub_mutex_unlock) (void *mutex)
 mutex unlock function More...
 
typedef void(* ub_fatal_func) (void)
 function to process a fatal error event More...
 
typedef uint64_t(* ub_gettime64) (ub_clocktype_t ctype)
 64-bit timestamp function More...
 

Enumerations

enum  ub_clocktype_t { UB_CLOCK_DEFAULT =0, UB_CLOCK_REALTIME, UB_CLOCK_MONOTONIC, UB_CLOCK_GPTP }
 clock type which provides timestamp More...
 

Macros

#define CLOCK_MONOTONIC   CLOCK_REALTIME
 
#define UB_UNIBASE_LOGCAT   0
 

Macro Definition Documentation

◆ CLOCK_MONOTONIC

#define CLOCK_MONOTONIC   CLOCK_REALTIME

◆ UB_UNIBASE_LOGCAT

#define UB_UNIBASE_LOGCAT   0

Typedef Documentation

◆ ub_console_out

typedef int(* ub_console_out) (bool flush, const char *str)

console output function

◆ ub_debug_out

typedef int(* ub_debug_out) (bool flush, const char *str)

debug output function

◆ ub_mutex_init

typedef void*(* ub_mutex_init) (void)

mutex initialization function

◆ ub_mutex_close

typedef int(* ub_mutex_close) (void *mutex)

mutex de-initialization function

◆ ub_mutex_lock

typedef int(* ub_mutex_lock) (void *mutex)

mutex lock function

◆ ub_mutex_unlock

typedef int(* ub_mutex_unlock) (void *mutex)

mutex unlock function

◆ ub_fatal_func

typedef void(* ub_fatal_func) (void)

function to process a fatal error event

◆ ub_gettime64

typedef uint64_t(* ub_gettime64) (ub_clocktype_t ctype)

64-bit timestamp function

Enumeration Type Documentation

◆ ub_clocktype_t

clock type which provides timestamp

Enumerator
UB_CLOCK_DEFAULT 
UB_CLOCK_REALTIME 
UB_CLOCK_MONOTONIC 
UB_CLOCK_GPTP 

Function Documentation

◆ unibase_init()

int unibase_init ( unibase_init_para_t ub_init_para)

initialize unibase

Parameters
ub_init_paraa set of callback functions to support platfrom specific functions, and a string to initialize logging functions
Returns
0:succes, -1:error
Note
unibase_init MUST be called at the beginning. Calling unibase_init again after the first call are all ignored. If mutex_init=Null, it runs in a single thread mode.

◆ unibase_close()

void unibase_close ( void  )

claose unibase

◆ ub_fatal()

void ub_fatal ( const char *  mes1,
const char *  mes2 
)

process a fatal error

Parameters
mes1printing message 1
mes2printing message 2
Note
'fatal' callback is called if it is registered. after this call 'ub_fatalerror()' returns true;

◆ ub_fatalerror()

bool ub_fatalerror ( void  )

return the fatal error status

◆ ub_assert_fatal()

static bool ub_assert_fatal ( bool  cond,
const char *  mes1,
const char *  mes2 
)
inlinestatic

conditinal ub_fatal

◆ ub_rt_gettime64()

uint64_t ub_rt_gettime64 ( void  )

get 64-bit REALTIME clock value

Returns
clock value

◆ ub_mt_gettime64()

uint64_t ub_mt_gettime64 ( void  )

get 64-bit MONOTONIC clock value

Returns
clock value

◆ ub_gptp_gettime64()

uint64_t ub_gptp_gettime64 ( void  )

get 64-bit PTP clock value

Returns
clock value