AM263Px MCU+ SDK  09.02.00
Expand and Shrink Array

Introduction

Files

file  ub_esarray.h
 Allocated memory array which is expanded or shrinked automatically.
 

Functions

ub_esarray_cstd_tub_esarray_init (int esunit, int elesize, int maxeles)
 initialize ub_esarray object. More...
 
void ub_esarray_close (ub_esarray_cstd_t *eah)
 close ub_esarray More...
 
int ub_esarray_add_ele (ub_esarray_cstd_t *eah, ub_esarray_element_t *ed)
 add one element More...
 
int ub_esarray_pop_ele (ub_esarray_cstd_t *eah, ub_esarray_element_t *ed)
 pop in fifo mode(get from index=0, and delete index=0) More...
 
int ub_esarray_pop_last_ele (ub_esarray_cstd_t *eah, ub_esarray_element_t *ed)
 pop in stack mode(get from the last index, and delete it) More...
 
int ub_esarray_del_ele (ub_esarray_cstd_t *eah, ub_esarray_element_t *ed)
 delete one element *ed More...
 
int ub_esarray_data_lock (ub_esarray_cstd_t *eah)
 lock data to preserve checked out data by ub_esarray_get_newele or ub_esarray_get_ele More...
 
int ub_esarray_data_unlock (ub_esarray_cstd_t *eah)
 unlock data to return to the default status More...
 
int ub_esarray_ele_nums (ub_esarray_cstd_t *eah)
 returns the number of elements More...
 
ub_esarray_element_tub_esarray_get_newele (ub_esarray_cstd_t *eah)
 get a new element from the ub_esarray_array More...
 
ub_esarray_element_tub_esarray_get_ele (ub_esarray_cstd_t *eah, int index)
 get the indexed element from the ub_esarray_array More...
 
int ub_esarray_del_pointer (ub_esarray_cstd_t *eah, ub_esarray_element_t *ed)
 delete one element with element pointer More...
 
int ub_esarray_del_index (ub_esarray_cstd_t *eah, int index)
 delete one element with index More...
 

Typedefs

typedef struct ub_esarray_cstd ub_esarray_cstd_t
 the data handle of ub_esarray object, the inside of it is private More...
 
typedef void ub_esarray_element_t
 data type of the element More...
 

Typedef Documentation

◆ ub_esarray_cstd_t

typedef struct ub_esarray_cstd ub_esarray_cstd_t

the data handle of ub_esarray object, the inside of it is private

◆ ub_esarray_element_t

typedef void ub_esarray_element_t

data type of the element

Note
for actual element type, the caller needs to cast ub_esarray_element_t type value.

Function Documentation

◆ ub_esarray_init()

ub_esarray_cstd_t* ub_esarray_init ( int  esunit,
int  elesize,
int  maxeles 
)

initialize ub_esarray object.

Returns
the data handle of ub_esarray_array object
Parameters
esunitexpand and shrink unit
elesizeelement size
maxelesmax number of elements

◆ ub_esarray_close()

void ub_esarray_close ( ub_esarray_cstd_t eah)

close ub_esarray

Parameters
eahthe data handle of ub_esarray object

◆ ub_esarray_add_ele()

int ub_esarray_add_ele ( ub_esarray_cstd_t eah,
ub_esarray_element_t ed 
)

add one element

Returns
0 on success, -1 on error
Parameters
eahthe data handle of ub_esarray_array object
eda new element to add
Note
thread safe, data is copied, 'ed' can be freed after this call.

◆ ub_esarray_pop_ele()

int ub_esarray_pop_ele ( ub_esarray_cstd_t eah,
ub_esarray_element_t ed 
)

pop in fifo mode(get from index=0, and delete index=0)

Returns
0 on success, -1 on error
Parameters
eahthe data handle of ub_esarray_array object
edpopped element; the data is copied to ed, which must have elesize space
Note
thread safe, data is copied, 'ed' must be allocated by the caller.

◆ ub_esarray_pop_last_ele()

int ub_esarray_pop_last_ele ( ub_esarray_cstd_t eah,
ub_esarray_element_t ed 
)

pop in stack mode(get from the last index, and delete it)

Returns
0 on success, -1 on error
Parameters
eahthe data handle of ub_esarray_array object
edpoped element; the data is copied to ed, which must have elesize space
Note
thread safe, data is copied, 'ed' must be allocated by the caller.

◆ ub_esarray_del_ele()

int ub_esarray_del_ele ( ub_esarray_cstd_t eah,
ub_esarray_element_t ed 
)

delete one element *ed

Returns
0 on success, -1 if no such elemet exists
Parameters
eahthe data handle of ub_esarray_array object
edthe element which has the same contents as 'ed' should be deleted
Note
thread safe, the caller needs to bring 'ed' with the contents

◆ ub_esarray_data_lock()

int ub_esarray_data_lock ( ub_esarray_cstd_t eah)

lock data to preserve checked out data by ub_esarray_get_newele or ub_esarray_get_ele

Note
using the data pointers or the data index number is not thread safe, to be thread safe, call 'ub_esarray_data_lock' before the work, and call 'ub_esarray_data_unlock' after the work.

◆ ub_esarray_data_unlock()

int ub_esarray_data_unlock ( ub_esarray_cstd_t eah)

unlock data to return to the default status

◆ ub_esarray_ele_nums()

int ub_esarray_ele_nums ( ub_esarray_cstd_t eah)

returns the number of elements

Returns
the number of elements

◆ ub_esarray_get_newele()

ub_esarray_element_t* ub_esarray_get_newele ( ub_esarray_cstd_t eah)

get a new element from the ub_esarray_array

Returns
a new element which has area of elesize bytes
Parameters
eahthe data handle of ub_esarray_array object
Note
the contentes of the return is NOT THREAD-SAFE. the caller needs to make sure that no delete happens during the time to use the result pointer. the internal data is locked after this call.

◆ ub_esarray_get_ele()

ub_esarray_element_t* ub_esarray_get_ele ( ub_esarray_cstd_t eah,
int  index 
)

get the indexed element from the ub_esarray_array

Returns
the indexed element which has area of elesize bytes
Parameters
eahthe data handle of ub_esarray_array object
indexindex in the current ub_esarray_array
Note
the contentes of the return is NOT THREAD-SAFE. the caller needs to make sure that no delete happens during the time to use the result pointer. the internal data is locked after this call.

◆ ub_esarray_del_pointer()

int ub_esarray_del_pointer ( ub_esarray_cstd_t eah,
ub_esarray_element_t ed 
)

delete one element with element pointer

Returns
0 on success, -1 if no such element exists
Parameters
eahthe data handle of ub_esarray_array object
edthe element pointer which should be deleted
Note
NOT THREAD-SAFE; between ub_esarray_get_ele and ub_esarray_del_pointer, no other delete can happen.

◆ ub_esarray_del_index()

int ub_esarray_del_index ( ub_esarray_cstd_t eah,
int  index 
)

delete one element with index

Returns
0 on success, -1 if index >= number of elements
Parameters
eahthe data handle of ub_esarray_array object
indexthe index of the current ub_esarray_array, which should be deleted
Note
NOT THREAD-SAFE; index may not be right number, if other delete happens after getting index.