AM263Px MCU+ SDK  09.02.00
APIs for SDL MCRC

Introduction

This module contains APIs for using the MCRC module. The APIs can be used to configure the controller to calculate the signature for a set of data and then compare the calculated signature value against a predetermined good signature value.

Sub Modules

 MCRC API
 
 MCRC Low-Level API