The SDL CCM module provides API for CCM Diagnostics
◆ SDL_CCM_ESM_U_BASE
| #define SDL_CCM_ESM_U_BASE (SDL_ESM0_CCM_0_SELFTEST_ERR) |
◆ SDL_INTR_GROUP_NUM
| #define SDL_INTR_GROUP_NUM 1U |
◆ BASEADDRESS
| #define BASEADDRESS SDL_R5SS0_CCMR_U_BASE |
◆ ESM_INSTANCE
| #define ESM_INSTANCE SDL_ESM_INST_MAIN_ESM0 |
◆ SDL_R5SS0_CCM
◆ SDL_R5SS1_CCM
◆ SDL_CCM_MAX_INSTANCE
◆ SDL_CCM_Inst
◆ SDL_CCM_baseAddress
Initial value:=
{
SDL_R5SS0_CCMR_U_BASE,
SDL_R5SS1_CCMR_U_BASE,
}
This API is used to get the base address of the instance.