AM263Px MCU+ SDK  09.02.00
APIs for SOC Specific Functions

Introduction

For more details and example usage, see SOC

Sub Modules

 APIs for SOC Reset and Clock Functions
 
 APIs for SOC Xbars
 

Functions

static int32_t MCSPI_lld_isBaseAddrValid (uint32_t baseAddr)
 API to validate MCSPI base address. More...
 
int32_t SOC_moduleClockEnable (uint32_t moduleId, uint32_t enable)
 Enable clock to specified module. More...
 
int32_t SOC_moduleSetClockFrequency (uint32_t moduleId, uint32_t clkId, uint64_t clkRate)
 Set module clock to specified frequency. More...
 
const char * SOC_getCoreName (uint16_t coreId)
 Convert a core ID to a user readable name. More...
 
uint64_t SOC_getSelfCpuClk (void)
 Get the clock frequency in Hz of the CPU on which the driver is running. More...
 
void SOC_controlModuleLockMMR (uint32_t domainId, uint32_t partition)
 Lock control module partition to prevent writes into control MMRs. More...
 
void SOC_controlModuleUnlockMMR (uint32_t domainId, uint32_t partition)
 Unlock control module partition to allow writes into control MMRs. More...
 
void SOC_setEpwmTbClk (uint32_t epwmInstance, uint32_t enable)
 Enable or disable ePWM time base clock from Control MMR. More...
 
void SOC_setMultipleEpwmTbClk (uint32_t epwmMask, uint32_t enable)
 Enable or disable Multiple ePWM time base clock from Control MMR. More...
 
void SOC_enableAdcReference (uint32_t adcInstance)
 Enable ADC references by writing to Control MMR. More...
 
void SOC_enableAdcOsdChannel (uint32_t adcInstance, uint32_t channel, uint32_t enable)
 Enable or disable the OSD circuit over the ADC channels. More...
 
void SOC_setAdcOsdConfig (uint32_t adcInstance, uint32_t config)
 Sets the ADC OSD Configuration. More...
 
void SOC_enableAdcGlobalForce (uint32_t adcInstance, uint32_t enable)
 Enable or Disable the ADC instnace for Gloabl SW force. More...
 
void SOC_adcSocGlobalForce (uint32_t socNumber)
 Triggers a global force for the SOC in enabled ADCs the ADCs may be enabled by using SOC_enableAdcGlobalForce() API
More...
 
void SOC_selectAdcExtChXbar (uint32_t extChXbarOut, uint32_t extChXbarIn)
 Selects the ADC External Channel Select bit for the output from each xbar out. More...
 
void SOC_selextAdcExtChDelay (uint32_t delay)
 Mux select to choose delay for ADC Extchsel. More...
 
void SOC_enableAdcDacLoopback (uint32_t enable)
 Enable or Disable the ADC CAL Pin to loopback with DAC. More...
 
void SOC_setEpwmGroup (uint32_t epwmInstance, uint32_t group)
 Configure the ePWM group. More...
 
void SOC_selectSdfm1Clk0Source (uint8_t source)
 Select the SDFM1 CLK0 source. More...
 
void SOC_sdfmClkLoopBackConfig (uint32_t sdfmInstance, uint32_t clkInstance, uint32_t defaultValue)
 Sets the configuraion for the loopback control. More...
 
void SOC_gateEpwmClock (uint32_t epwmInstance)
 Gate the ePWM clock. More...
 
void SOC_gateFsitxClock (uint32_t fsitxInstance)
 Gate the FSI-TX clock. More...
 
void SOC_gateFsirxClock (uint32_t fsirxInstance)
 Gate the FSI-RX clock. More...
 
void SOC_gateCmpssaClock (uint32_t cmpssaInstance)
 Gate the CMPSS-A clock. More...
 
void SOC_gateCmpssbClock (uint32_t cmpssbInstance)
 Gate the CMPSS-B clock. More...
 
void SOC_gateEcapClock (uint32_t ecapInstance)
 Gate the ECAP clock. More...
 
void SOC_gateEqepClock (uint32_t eqepInstance)
 Gate the EQEP clock. More...
 
void SOC_gateSdfmClock (uint32_t sdfmInstance)
 Gate the SDFM clock. More...
 
void SOC_gateDacClock (void)
 Gate the DAC clock. More...
 
void SOC_gateAdcClock (uint32_t adcInstance)
 Gate the ADC clock. More...
 
void SOC_gateRdcClock (uint32_t rdcInstance)
 Gate the HW_RESOLVER clock. More...
 
void SOC_gateOttoClock (uint32_t ottoInstance)
 Gate the OTTO clock. More...
 
void SOC_gateSdfmPllClock (uint32_t sdfmInstance)
 Gate the SDFM PLL clock. More...
 
void SOC_gateFsiPllClock (uint32_t fsiInstance)
 Gate the FSI-TX PLL clock. More...
 
void SOC_generateEpwmReset (uint32_t ePWMInstance)
 Generate ePWM reset. More...
 
void SOC_generateFsiTxReset (uint32_t fsitxInstance)
 Generate FSI-TX reset. More...
 
void SOC_generateFsiRxReset (uint32_t fsirxInstance)
 Generate FSI-RX reset. More...
 
void SOC_generateCmpssaReset (uint32_t cmpssaInstance)
 Generate CMPSS-A reset. More...
 
void SOC_generateCmpssbReset (uint32_t cmpssbInstance)
 Generate CMPSS-B reset. More...
 
void SOC_generateEcapReset (uint32_t ecapInstance)
 Generate ECAP reset. More...
 
void SOC_generateEqepReset (uint32_t eqepInstance)
 Generate EQEP reset. More...
 
void SOC_generateSdfmReset (uint32_t sdfmInstance)
 Generate SDFM reset. More...
 
void SOC_generateDacReset (void)
 Generate DAC reset. More...
 
void SOC_generateAdcReset (uint32_t adcInstance)
 Generate ADC reset. More...
 
void SOC_generateRdcReset (uint32_t rdcInstance)
 Generate RDC reset. More...
 
void Soc_enableEPWMHalt (uint32_t epwmInstance)
 Halt EPWM with corresponding cPU. More...
 
void SOC_generateOttoReset (uint32_t ottoInstance)
 Generate OTTO reset. More...
 
void SOC_selectIcssGpiMux (uint8_t pru_instance, uint32_t mask)
 Selection of ICSS GPI MUX. More...
 
uint64_t SOC_virtToPhy (void *virtAddr)
 SOC Virtual (CPU) to Physical address translation function. More...
 
void * SOC_phyToVirt (uint64_t phyAddr)
 Physical to Virtual (CPU) address translation function. More...
 
uint32_t SOC_getFlashDataBaseAddr (void)
 This function gets the SOC mapped data base address of the flash. More...
 
static int32_t UART_IsBaseAddrValid (uint32_t baseAddr)
 API to validate UART base address. More...
 

Macros

#define MSS_CTRL_PARTITION0   (1)
 
#define TOP_CTRL_PARTITION0   (2)
 
#define CONTROLSS_CTRL_PARTITION0   (3)
 
#define MSS_RCM_PARTITION0   (4)
 
#define TOP_RCM_PARTITION0   (5)
 
#define KICK_LOCK_VAL   (0x00000000U)
 
#define KICK0_UNLOCK_VAL   (0x01234567U)
 
#define KICK1_UNLOCK_VAL   (0x0FEDCBA8U)
 
#define ADC0_EXTCHSEL_BIT0   (0U)
 
#define ADC0_EXTCHSEL_BIT1   (1U)
 
#define ADC1_EXTCHSEL_BIT0   (2U)
 
#define ADC1_EXTCHSEL_BIT1   (3U)
 
#define ADC2_EXTCHSEL_BIT0   (4U)
 
#define ADC2_EXTCHSEL_BIT1   (5U)
 
#define ADC3_EXTCHSEL_BIT0   (6U)
 
#define ADC3_EXTCHSEL_BIT1   (7U)
 
#define ADC4_EXTCHSEL_BIT0   (8U)
 
#define ADC4_EXTCHSEL_BIT1   (9U)
 
#define ADC_R0_EXTCHSEL_BIT0   (10U)
 
#define ADC_R0_EXTCHSEL_BIT1   (11U)
 
#define ADC_R1_EXTCHSEL_BIT0   (12U)
 
#define ADC_R2_EXTCHSEL_BIT1   (13U)
 
#define ADC_EXTCHSELCT_DELAY_3_CYCLES   (0U)
 
#define ADC_EXTCHSELCT_DELAY_6_CYCLES   (1U)
 
#define IS_I2C_BASE_ADDR_VALID(baseAddr)
 

SOC Domain ID

#define SOC_DOMAIN_ID_MAIN   (0U)
 

Macro Definition Documentation

◆ SOC_DOMAIN_ID_MAIN

#define SOC_DOMAIN_ID_MAIN   (0U)

◆ MSS_CTRL_PARTITION0

#define MSS_CTRL_PARTITION0   (1)

◆ TOP_CTRL_PARTITION0

#define TOP_CTRL_PARTITION0   (2)

◆ CONTROLSS_CTRL_PARTITION0

#define CONTROLSS_CTRL_PARTITION0   (3)

◆ MSS_RCM_PARTITION0

#define MSS_RCM_PARTITION0   (4)

◆ TOP_RCM_PARTITION0

#define TOP_RCM_PARTITION0   (5)

◆ KICK_LOCK_VAL

#define KICK_LOCK_VAL   (0x00000000U)

◆ KICK0_UNLOCK_VAL

#define KICK0_UNLOCK_VAL   (0x01234567U)

◆ KICK1_UNLOCK_VAL

#define KICK1_UNLOCK_VAL   (0x0FEDCBA8U)

◆ ADC0_EXTCHSEL_BIT0

#define ADC0_EXTCHSEL_BIT0   (0U)

◆ ADC0_EXTCHSEL_BIT1

#define ADC0_EXTCHSEL_BIT1   (1U)

◆ ADC1_EXTCHSEL_BIT0

#define ADC1_EXTCHSEL_BIT0   (2U)

◆ ADC1_EXTCHSEL_BIT1

#define ADC1_EXTCHSEL_BIT1   (3U)

◆ ADC2_EXTCHSEL_BIT0

#define ADC2_EXTCHSEL_BIT0   (4U)

◆ ADC2_EXTCHSEL_BIT1

#define ADC2_EXTCHSEL_BIT1   (5U)

◆ ADC3_EXTCHSEL_BIT0

#define ADC3_EXTCHSEL_BIT0   (6U)

◆ ADC3_EXTCHSEL_BIT1

#define ADC3_EXTCHSEL_BIT1   (7U)

◆ ADC4_EXTCHSEL_BIT0

#define ADC4_EXTCHSEL_BIT0   (8U)

◆ ADC4_EXTCHSEL_BIT1

#define ADC4_EXTCHSEL_BIT1   (9U)

◆ ADC_R0_EXTCHSEL_BIT0

#define ADC_R0_EXTCHSEL_BIT0   (10U)

◆ ADC_R0_EXTCHSEL_BIT1

#define ADC_R0_EXTCHSEL_BIT1   (11U)

◆ ADC_R1_EXTCHSEL_BIT0

#define ADC_R1_EXTCHSEL_BIT0   (12U)

◆ ADC_R2_EXTCHSEL_BIT1

#define ADC_R2_EXTCHSEL_BIT1   (13U)

◆ ADC_EXTCHSELCT_DELAY_3_CYCLES

#define ADC_EXTCHSELCT_DELAY_3_CYCLES   (0U)

◆ ADC_EXTCHSELCT_DELAY_6_CYCLES

#define ADC_EXTCHSELCT_DELAY_6_CYCLES   (1U)

◆ IS_I2C_BASE_ADDR_VALID

#define IS_I2C_BASE_ADDR_VALID (   baseAddr)
Value:
((baseAddr == CSL_I2C0_U_BASE) || \
(baseAddr == CSL_I2C1_U_BASE) || \
(baseAddr == CSL_I2C2_U_BASE) || \
(baseAddr == CSL_I2C3_U_BASE))

Function Documentation

◆ MCSPI_lld_isBaseAddrValid()

static int32_t MCSPI_lld_isBaseAddrValid ( uint32_t  baseAddr)
inlinestatic

API to validate MCSPI base address.

◆ SOC_moduleClockEnable()

int32_t SOC_moduleClockEnable ( uint32_t  moduleId,
uint32_t  enable 
)

Enable clock to specified module.

Parameters
moduleId[in] see SOC_RcmPeripheralId for list of module ID's
enable[in] 1: enable clock to the module, 0: disable clock to the module
Returns
SystemP_SUCCESS Module clock is enabled
SystemP_FAILURE Module clock could not be enabled

◆ SOC_moduleSetClockFrequency()

int32_t SOC_moduleSetClockFrequency ( uint32_t  moduleId,
uint32_t  clkId,
uint64_t  clkRate 
)

Set module clock to specified frequency.

Parameters
moduleId[in] see SOC_RcmPeripheralId for list of module ID's
clkId[in] see SOC_RcmPeripheralClockSource for list of clocks
clkRate[in] Frequency to set in Hz
Returns
SystemP_SUCCESS Module clock is enabled
SystemP_FAILURE Module clock could not be enabled

◆ SOC_getCoreName()

const char* SOC_getCoreName ( uint16_t  coreId)

Convert a core ID to a user readable name.

Parameters
coreId[in] see CSL_CoreID
Returns
name as a string

◆ SOC_getSelfCpuClk()

uint64_t SOC_getSelfCpuClk ( void  )

Get the clock frequency in Hz of the CPU on which the driver is running.

Returns
Clock frequency in Hz

◆ SOC_controlModuleLockMMR()

void SOC_controlModuleLockMMR ( uint32_t  domainId,
uint32_t  partition 
)

Lock control module partition to prevent writes into control MMRs.

Parameters
domainId[in] See SOC_DomainId_t
partition[in] Partition number to unlock

◆ SOC_controlModuleUnlockMMR()

void SOC_controlModuleUnlockMMR ( uint32_t  domainId,
uint32_t  partition 
)

Unlock control module partition to allow writes into control MMRs.

Parameters
domainId[in] See SOC_DomainId_t
partition[in] Partition number to unlock

◆ SOC_setEpwmTbClk()

void SOC_setEpwmTbClk ( uint32_t  epwmInstance,
uint32_t  enable 
)

Enable or disable ePWM time base clock from Control MMR.

Parameters
epwmInstance[in] ePWM instance number [0 - (CSL_EPWM_PER_CNT-1)]
enable[in] TRUE to enable and FALSE to disable

◆ SOC_setMultipleEpwmTbClk()

void SOC_setMultipleEpwmTbClk ( uint32_t  epwmMask,
uint32_t  enable 
)

Enable or disable Multiple ePWM time base clock from Control MMR.

Parameters
epwmMask[in] ePWM instance Mask [1 - CSL_CONTROLSS_CTRL_EPWM_CLKSYNC_BIT_MAX]
enable[in] TRUE to enable and FALSE to disable

◆ SOC_enableAdcReference()

void SOC_enableAdcReference ( uint32_t  adcInstance)

Enable ADC references by writing to Control MMR.

Parameters
adcInstance[in] ADC instance number [0 - (CSL_ADC_PER_CNT-1)]

◆ SOC_enableAdcOsdChannel()

void SOC_enableAdcOsdChannel ( uint32_t  adcInstance,
uint32_t  channel,
uint32_t  enable 
)

Enable or disable the OSD circuit over the ADC channels.

Parameters
adcInstance[in] ADC instance [0 - 4] ADC_R instance [5,6]
channel[in] Channel number for the ADC. [0 - 5]
enable[in] TRUE to enable and FALSE to disable the OSD circuit.

◆ SOC_setAdcOsdConfig()

void SOC_setAdcOsdConfig ( uint32_t  adcInstance,
uint32_t  config 
)

Sets the ADC OSD Configuration.

Parameters
adcInstance[in] ADC instance [0 - 4] ADC_R instance [5,6]
config[in] configuration to be enabled of the OSD circuit.

It is recommended to wait for atleast 1uS after configuration, before sampling

config function Impedance Voltage on 5K Voltage on 7K
0 Zero Scale 5K // 7K VSSA VSSA
------— ------------— --------— ------------— --------—
1 Zero Scale 5K VSSA OPEN
------— ------------— --------— ------------— --------—
2 Zero Scale 7K OPEN VSSA
------— ------------— --------— ------------— --------—
3 Full Scale 5K // 7K VDD VDD
------— ------------— --------— ------------— --------—
4 Full Scale 5K VDD OPEN
------— ------------— --------— ------------— --------—
5 Full Scale 7K OPEN VDD
------— ------------— --------— ------------— --------—
6 5/12 Scale 5K // 7K VSSA VDD
------— ------------— --------— ------------— --------—
7 5/12 Scale 5K // 7K VDD VSSA
------— ------------— --------— ------------— --------—

◆ SOC_enableAdcGlobalForce()

void SOC_enableAdcGlobalForce ( uint32_t  adcInstance,
uint32_t  enable 
)

Enable or Disable the ADC instnace for Gloabl SW force.

Parameters
adcInstance[in] ADC instances [0 - 4] ADC_R instance [ 5 - 6]
enable[in] TRUE to enable and FALSE to disable the GLobal Force Selection

◆ SOC_adcSocGlobalForce()

void SOC_adcSocGlobalForce ( uint32_t  socNumber)

Triggers a global force for the SOC in enabled ADCs the ADCs may be enabled by using SOC_enableAdcGlobalForce() API

Parameters
socNumber[in] SOC Number [0 - 15]

◆ SOC_selectAdcExtChXbar()

void SOC_selectAdcExtChXbar ( uint32_t  extChXbarOut,
uint32_t  extChXbarIn 
)

Selects the ADC External Channel Select bit for the output from each xbar out.

Parameters
extChXbarOut[in] selects the ADC_EXTCHSEL_XBAR_OUTx x in [0 - 9]
extChXbarIn[in] Valid Values are the following ADC0_EXTCHSEL_BIT0
ADC0_EXTCHSEL_BIT1
ADC1_EXTCHSEL_BIT0
ADC1_EXTCHSEL_BIT1
ADC2_EXTCHSEL_BIT0
ADC2_EXTCHSEL_BIT1
ADC3_EXTCHSEL_BIT0
ADC3_EXTCHSEL_BIT1
ADC4_EXTCHSEL_BIT0
ADC4_EXTCHSEL_BIT1
ADC_R0_EXTCHSEL_BIT0
ADC_R0_EXTCHSEL_BIT1
ADC_R1_EXTCHSEL_BIT0
ADC_R2_EXTCHSEL_BIT1

◆ SOC_selextAdcExtChDelay()

void SOC_selextAdcExtChDelay ( uint32_t  delay)

Mux select to choose delay for ADC Extchsel.

Parameters
delay[in] 3 Cycle Delay or 6 Cycle Delay Valid Values are ADC_EXTCHSELCT_DELAY_3_CYCLES ADC_EXTCHSELCT_DELAY_6_CYCLES

◆ SOC_enableAdcDacLoopback()

void SOC_enableAdcDacLoopback ( uint32_t  enable)

Enable or Disable the ADC CAL Pin to loopback with DAC.

Parameters
enable[in] TRUE to enable, FALSE to disable

◆ SOC_setEpwmGroup()

void SOC_setEpwmGroup ( uint32_t  epwmInstance,
uint32_t  group 
)

Configure the ePWM group.

Parameters
epwmInstance[in] ePWM instance number [0 - (CSL_EPWM_PER_CNT-1)]
group[in] The group for this ePWM instance [0 - 3]

◆ SOC_selectSdfm1Clk0Source()

void SOC_selectSdfm1Clk0Source ( uint8_t  source)

Select the SDFM1 CLK0 source.

Parameters
source[in] Source of SDFM1 CLK0. 0: source is SDFM1 CK0 from Pinmux. 1: source is SDFM0 CK0 from Pinmux

◆ SOC_sdfmClkLoopBackConfig()

void SOC_sdfmClkLoopBackConfig ( uint32_t  sdfmInstance,
uint32_t  clkInstance,
uint32_t  defaultValue 
)

Sets the configuraion for the loopback control.

Parameters
sdfmInstance[in] SDFM instance number [0,1]
clkInstance[in] SDFM Clock number [0 - 3]
defaultValue[in] TRUE to set the default Loopback control loopback FALSE to set alternate Loopback control
Note
this API doesn't configure the PinMux if the loopback clock is required to be routed to the pin, the pinMux should be configured with the Output override enabled.

◆ SOC_gateEpwmClock()

void SOC_gateEpwmClock ( uint32_t  epwmInstance)

Gate the ePWM clock.

Parameters
epwmInstance[in] ePWM instance number [0 - (CSL_EPWM_PER_CNT-1)]

◆ SOC_gateFsitxClock()

void SOC_gateFsitxClock ( uint32_t  fsitxInstance)

Gate the FSI-TX clock.

Parameters
fsitxInstance[in] FSITX instance number [0 - 3]

◆ SOC_gateFsirxClock()

void SOC_gateFsirxClock ( uint32_t  fsirxInstance)

Gate the FSI-RX clock.

Parameters
fsirxInstance[in] FSIRX instance number [0 - 3]

◆ SOC_gateCmpssaClock()

void SOC_gateCmpssaClock ( uint32_t  cmpssaInstance)

Gate the CMPSS-A clock.

Parameters
cmpssaInstance[in] CMPSS-A instance number [0 - 9]

◆ SOC_gateCmpssbClock()

void SOC_gateCmpssbClock ( uint32_t  cmpssbInstance)

Gate the CMPSS-B clock.

Parameters
cmpssbInstance[in] CMPSS-B instance number [0 - 9]

◆ SOC_gateEcapClock()

void SOC_gateEcapClock ( uint32_t  ecapInstance)

Gate the ECAP clock.

Parameters
ecapInstance[in] ECAP instance number [0 - 9]

◆ SOC_gateEqepClock()

void SOC_gateEqepClock ( uint32_t  eqepInstance)

Gate the EQEP clock.

Parameters
eqepInstance[in] EQEP instance number [0 - 2]

◆ SOC_gateSdfmClock()

void SOC_gateSdfmClock ( uint32_t  sdfmInstance)

Gate the SDFM clock.

Parameters
sdfmInstance[in] SDFM instance number [0 - 1]

◆ SOC_gateDacClock()

void SOC_gateDacClock ( void  )

Gate the DAC clock.

◆ SOC_gateAdcClock()

void SOC_gateAdcClock ( uint32_t  adcInstance)

Gate the ADC clock.

Parameters
adcInstance[in] ADC instance number [0 - 4] or ADC_R instance [0 - 1]

◆ SOC_gateRdcClock()

void SOC_gateRdcClock ( uint32_t  rdcInstance)

Gate the HW_RESOLVER clock.

Parameters
rdcInstance[in] HW_RESOLVER instance number [0]

◆ SOC_gateOttoClock()

void SOC_gateOttoClock ( uint32_t  ottoInstance)

Gate the OTTO clock.

Parameters
ottoInstance[in] OTTO instance number [0 - 3]

◆ SOC_gateSdfmPllClock()

void SOC_gateSdfmPllClock ( uint32_t  sdfmInstance)

Gate the SDFM PLL clock.

Parameters
sdfmInstance[in] SDFM instance number [0 - 1]

◆ SOC_gateFsiPllClock()

void SOC_gateFsiPllClock ( uint32_t  fsiInstance)

Gate the FSI-TX PLL clock.

Parameters
fsiInstance[in] FSI instance number [0 - 3]

◆ SOC_generateEpwmReset()

void SOC_generateEpwmReset ( uint32_t  ePWMInstance)

Generate ePWM reset.

Parameters
ePWMInstance[in] ePWM instance number [0 - 31]

◆ SOC_generateFsiTxReset()

void SOC_generateFsiTxReset ( uint32_t  fsitxInstance)

Generate FSI-TX reset.

Parameters
fsitxInstance[in] FSI instance number [0 - 3]

◆ SOC_generateFsiRxReset()

void SOC_generateFsiRxReset ( uint32_t  fsirxInstance)

Generate FSI-RX reset.

Parameters
fsirxInstance[in] FSI instance number [0 - 3]

◆ SOC_generateCmpssaReset()

void SOC_generateCmpssaReset ( uint32_t  cmpssaInstance)

Generate CMPSS-A reset.

Parameters
cmpssaInstance[in] CMPSS-A instance number [0 - 9]

◆ SOC_generateCmpssbReset()

void SOC_generateCmpssbReset ( uint32_t  cmpssbInstance)

Generate CMPSS-B reset.

Parameters
cmpssbInstance[in] CMPSS-B instance number [0 - 9]

◆ SOC_generateEcapReset()

void SOC_generateEcapReset ( uint32_t  ecapInstance)

Generate ECAP reset.

Parameters
ecapInstance[in] ECAP instance number [0 - 9]

◆ SOC_generateEqepReset()

void SOC_generateEqepReset ( uint32_t  eqepInstance)

Generate EQEP reset.

Parameters
eqepInstance[in] EQEP instance number [0 - 2]

◆ SOC_generateSdfmReset()

void SOC_generateSdfmReset ( uint32_t  sdfmInstance)

Generate SDFM reset.

Parameters
sdfmInstance[in] SDFM instance number [0 - 1]

◆ SOC_generateDacReset()

void SOC_generateDacReset ( void  )

Generate DAC reset.

◆ SOC_generateAdcReset()

void SOC_generateAdcReset ( uint32_t  adcInstance)

Generate ADC reset.

Parameters
adcInstance[in] ADC instance number [0 - 4]

◆ SOC_generateRdcReset()

void SOC_generateRdcReset ( uint32_t  rdcInstance)

Generate RDC reset.

Parameters
rdcInstance

◆ Soc_enableEPWMHalt()

void Soc_enableEPWMHalt ( uint32_t  epwmInstance)

Halt EPWM with corresponding cPU.

Parameters
epwmInstance[in] EPWM instance number [0 - 31]

◆ SOC_generateOttoReset()

void SOC_generateOttoReset ( uint32_t  ottoInstance)

Generate OTTO reset.

Parameters
ottoInstance[in] OTTO instance number [0 - 3]

◆ SOC_selectIcssGpiMux()

void SOC_selectIcssGpiMux ( uint8_t  pru_instance,
uint32_t  mask 
)

Selection of ICSS GPI MUX.

Parameters
pru_instance[in] PRU instance number [0 - 1]
mask[in] Bitwise selection of ICSSM GPI source. GPI or PWMXBar select for ICSSM port 0/1. 0-GPI, 1-PWMXBAR

◆ SOC_virtToPhy()

uint64_t SOC_virtToPhy ( void *  virtAddr)

SOC Virtual (CPU) to Physical address translation function.

Parameters
virtAddr[IN] Virtual/CPU address
Returns
Corresponding SOC physical address

◆ SOC_phyToVirt()

void* SOC_phyToVirt ( uint64_t  phyAddr)

Physical to Virtual (CPU) address translation function.

Parameters
phyAddr[IN] Physical address
Returns
Corresponding virtual/CPU address

◆ SOC_getFlashDataBaseAddr()

uint32_t SOC_getFlashDataBaseAddr ( void  )

This function gets the SOC mapped data base address of the flash.

Returns
Data BaseAddress of the flash

◆ UART_IsBaseAddrValid()

static int32_t UART_IsBaseAddrValid ( uint32_t  baseAddr)
inlinestatic

API to validate UART base address.