AM263Px MCU+ SDK  09.02.00

Introduction

See HSM client for more details.

Data Structures

union  HsmVer_t
 type for reading HSMRt version. More...
 
struct  HsmClient_t
 This is a HSMClient type which holds the information needed by hsm client to communicate with HSM . More...
 
struct  EfuseRead_t
 This is a EfuseRead type which holds the information of eFuse row index and row data corresponding to it . More...
 
struct  EfuseRowWrite_t
 This is a EfuseRowWrite type which holds the information regarding programming eFuse row. More...
 
struct  EfuseRowCount_t
 This is a EfuseRowCount type which holds the information regarding eFuse row count and size of each row in bits. More...
 
struct  EfuseRowProt_t
 This is a EfuseRowProt type which holds the information of eFuse row index and protection status corresponding to the row index. More...
 
struct  KeyWriterCertHeader_t
 This is a keywriter_cert_header type which holds the information of customer key certificate and debug responce. More...
 
struct  FirewallRegionReq_t
 This is a FirewallRegionReq type which holds the information of Firewall region configuration. More...
 
struct  FirewallReq_t
 This is a FirewallReq_t type which holds the information of Firewall configuration. More...
 
struct  FirewallIntrReq_t
 This is a FirewallIntrReq type which holds the information of MPU Firewall request for interrupt enable, interrupt enable clear, interrupt enable status clear and fault clear. More...
 
struct  SWRev_t
 This is SWRev type which holds the information regarding Revision identifier and value corresponding to it . More...
 
struct  DKEK_t
 This is DKEK type which holds the label and context for derivation. This also holds the 256 derived KEK value which is returned by TIFS. More...
 
struct  RNGReq_t
 This is RNG type which holds the resultPtr for derivation which is returned by TIFS. This also holds the resultLengthPtr and DRBG Mode along with seedValue and seedSize. More...
 
struct  HsmMsg_t_
 HSM client / server message format struct. More...
 

Functions

union HsmVer_t_ __attribute__ ((packed)) HsmVer_t
 type for reading HSMRt version. More...
 
int32_t HsmClient_init (SIPC_Params *params)
 Initialize the HSM client for current core. More...
 
void HsmClient_deInit (void)
 De initialize the HSM client for current core. More...
 
int32_t HsmClient_getVersion (HsmClient_t *HsmClient, HsmVer_t *verId, uint32_t timeToWaitInTick)
 populates the current HSMRT version Id by default the hsm flag is set to HSM_FLAG_AOP for this service More...
 
int32_t HsmClient_getUID (HsmClient_t *HsmClient, uint8_t *uid, uint32_t timeout)
 The service issued to HSM Server populates the Device UID by default the hsm flag is set to HSM_FLAG_AOP for this service. More...
 
int32_t HsmClient_openDbgFirewall (HsmClient_t *HsmClient, uint8_t *cert, uint32_t cert_size, uint32_t timeout)
 The service issued to HSM Server verifies the certificate and by default the hsm flag is set to HSM_FLAG_AOP for this service. More...
 
int32_t HsmClient_importKeyring (HsmClient_t *HsmClient, uint8_t *cert, uint32_t cert_size, uint32_t timeout)
 The service issued to HSM Server verifies the certificate and imports the keys from the certificate. More...
 
int32_t HsmClient_readOTPRow (HsmClient_t *HsmClient, EfuseRead_t *readRow)
 The service issued to HSM Server retrieves the data of GP OTP row based on row index provided as param. More...
 
int32_t HsmClient_writeOTPRow (HsmClient_t *HsmClient, EfuseRowWrite_t *writeRow)
 The service issued to HSM Server writes the data to extended OTP efuse row based on row index provided as param. More...
 
int32_t HsmClient_lockOTPRow (HsmClient_t *HsmClient, EfuseRowProt_t *rowProt)
 The service issued to HSM Server sets the protection status bit of the specified row to 1. More...
 
int32_t HsmClient_getOTPRowCount (HsmClient_t *HsmClient, EfuseRowCount_t *rowCount)
 The service issued to HSM Server retrieves the count of extended OTP rows. More...
 
int32_t HsmClient_getOTPRowProtection (HsmClient_t *HsmClient, EfuseRowProt_t *rowProt)
 The service issued to HSM Server retrieves the extended otp efuse row protection status. More...
 
int32_t HsmClient_procAuthBoot (HsmClient_t *HsmClient, uint8_t *cert, uint32_t cert_size, uint32_t timeout)
 The service issued to HSM Server helps with extended secure boot for applications. More...
 
int32_t HsmClient_setFirewall (HsmClient_t *HsmClient, FirewallReq_t *FirewallReqObj, uint32_t timeout)
 The service issued to HSM Server sets the firewall for the given firewall id and region. More...
 
int32_t HsmClient_FirewallIntr (HsmClient_t *HsmClient, FirewallIntrReq_t *FirewallIntrReqObj, uint32_t timeout)
 The service issued to HSM Server sets the firewall interrupt request for the given firewall id. More...
 
int32_t HsmClient_keyWriter (HsmClient_t *HsmClient, KeyWriterCertHeader_t *certHeader, uint32_t timeout)
 The service issued to HSM Server verifies the certificate and process the keywriter operations,. More...
 
int32_t HsmClient_readSWRev (HsmClient_t *HsmClient, SWRev_t *readSWRev)
 The service issued to HSM Server retrieves the SWRevision value based on identifier as param. More...
 
int32_t HsmClient_writeSWRev (HsmClient_t *HsmClient, SWRev_t *writeSWRev)
 The service issued to HSM Server writes the SWRevision value based on identifier as param. More...
 
int32_t HsmClient_getDKEK (HsmClient_t *HsmClient, DKEK_t *getDKEK, uint32_t timeout)
 The service issued to HSM Server retrieves the derived KEK based on identifier as param. More...
 
int32_t HsmClient_register (HsmClient_t *HsmClient, uint8_t clientId)
 register a client to a particular ClientId More...
 
void HsmClient_unregister (HsmClient_t *HsmClient, uint8_t clientId)
 unregister a client to a particular ClientId More...
 
int32_t HsmClient_waitForBootNotify (HsmClient_t *HsmClient, uint32_t timeToWaitInTicks)
 Current core will wait for bootnotify message from HSM core. More...
 
int32_t Hsmclient_loadHSMRtFirmware (HsmClient_t *gHSMClient, const uint8_t *pHSMRt_firmware)
 Loads the HSMRt firmware. This is typically called by SBL. More...
 
int32_t HsmClient_getRandomNum (HsmClient_t *HsmClient, RNGReq_t *getRandomNum)
 Returns the Random Number Generated. More...
 

Enumerations

enum  HSM_ClientIds_t {
  HSM_BOOT_NOTIFY_CLIENT_ID = 0, HSM_CLIENT_ID_1, HSM_CLIENT_ID_2, HSM_CLIENT_ID_3,
  HSM_CLIENT_ID_4
}
 

Macros

#define LABEL_AND_CONTEXT_LEN_MAX   48U
 
#define HSM_MSG_GET_VERSION   (0x0002)
 GetVersion service type ID. More...
 
#define HSM_MSG_BOOT_NOTIFY   (0x000A)
 Boot Notify service type ID. More...
 
#define HSM_MSG_GET_UID   (0x9021)
 Get UID service type ID. More...
 
#define HSM_MSG_OPEN_DBG_FIREWALLS   (0x900C)
 Open Debug Firewalls service type ID. More...
 
#define HSM_MSG_READ_OTP_ROW   (0x9022)
 Read Extended otp row type ID. More...
 
#define HSM_MSG_WRITE_OTP_ROW   (0x9023)
 Write Extended otp row type ID. More...
 
#define HSM_MSG_PROT_OTP_ROW   (0x9024)
 Protect Extended otp row type ID. More...
 
#define HSM_MSG_GET_OTP_ROW_PROT   (0x9026)
 Get Extended otp row protection type ID. More...
 
#define HSM_MSG_GET_OTP_ROW_COUNT   (0x9027)
 Get Extended otp row count service type ID. More...
 
#define HSM_MSG_PROC_AUTH_BOOT   (0xC120)
 Secure Boot service type ID. More...
 
#define HSM_MSG_SET_FIREWALL   (0x9000U)
 Set Firewall service type ID. More...
 
#define HSM_MSG_SET_FIREWALL_INTR   (0x9002)
 Set Firewall Interrupt service type ID. More...
 
#define HSM_KEYWRITER_SEND_CUST_KEY_CERT   (0x9028)
 send KeyWriter customer key certificate More...
 
#define HSM_MSG_READ_SWREV   (0x9033)
 Read Software Revision service type ID. More...
 
#define HSM_MSG_WRITE_SWREV   (0x9032)
 Write Software Revision service type ID. More...
 
#define HSM_MSG_GET_DKEK   (0x9029)
 Get DKEK service type ID. More...
 
#define HSM_MSG_GET_RAND   (0x9001)
 Get RNG service type ID. More...
 
#define HSM_MSG_KEYRING_IMPORT   (0x9039)
 Get KEYRING import service type ID. More...
 
#define HSM_FLAG_AOP   (0x11)
 HSM FLAG used by HSM client to indicate that it expects ACK messasge from HSM and will wait for a response message. More...
 
#define HSM_FLAG_NAOP   (0x22)
 HSM FLAG used by HSM client to indicate that it does not expects an ACK messasge from HSM and will not wait for a response message. More...
 
#define HSM_FLAG_ACK   (0xAA)
 HSM FLAG used by HSM server to indicate that the request has been processed. More...
 
#define HSM_FLAG_NACK   (0x55)
 HSM FLAG used by HSM server to indicate that the request has not been processed. More...
 
#define HSM_CLIENT_ID   (0x01)
 HSM server SIPC client Id. More...
 
#define HSM_UID_SIZE   (64U)
 UID or Unique ID is a device specific ID of 64 bytes. More...
 
#define HSM_DBG_CERT_SIZE   (4096U)
 Maximum Certificate Size allowed for Debug Open. More...
 
#define HSM_KEYRING_CERT_SIZE   (10280U)
 Maximum Certificate Size allowed for Keyring Import. More...
 

Macro Definition Documentation

◆ LABEL_AND_CONTEXT_LEN_MAX

#define LABEL_AND_CONTEXT_LEN_MAX   48U

◆ HSM_MSG_GET_VERSION

#define HSM_MSG_GET_VERSION   (0x0002)

GetVersion service type ID.

◆ HSM_MSG_BOOT_NOTIFY

#define HSM_MSG_BOOT_NOTIFY   (0x000A)

Boot Notify service type ID.

◆ HSM_MSG_GET_UID

#define HSM_MSG_GET_UID   (0x9021)

Get UID service type ID.

◆ HSM_MSG_OPEN_DBG_FIREWALLS

#define HSM_MSG_OPEN_DBG_FIREWALLS   (0x900C)

Open Debug Firewalls service type ID.

◆ HSM_MSG_READ_OTP_ROW

#define HSM_MSG_READ_OTP_ROW   (0x9022)

Read Extended otp row type ID.

◆ HSM_MSG_WRITE_OTP_ROW

#define HSM_MSG_WRITE_OTP_ROW   (0x9023)

Write Extended otp row type ID.

◆ HSM_MSG_PROT_OTP_ROW

#define HSM_MSG_PROT_OTP_ROW   (0x9024)

Protect Extended otp row type ID.

◆ HSM_MSG_GET_OTP_ROW_PROT

#define HSM_MSG_GET_OTP_ROW_PROT   (0x9026)

Get Extended otp row protection type ID.

◆ HSM_MSG_GET_OTP_ROW_COUNT

#define HSM_MSG_GET_OTP_ROW_COUNT   (0x9027)

Get Extended otp row count service type ID.

◆ HSM_MSG_PROC_AUTH_BOOT

#define HSM_MSG_PROC_AUTH_BOOT   (0xC120)

Secure Boot service type ID.

◆ HSM_MSG_SET_FIREWALL

#define HSM_MSG_SET_FIREWALL   (0x9000U)

Set Firewall service type ID.

◆ HSM_MSG_SET_FIREWALL_INTR

#define HSM_MSG_SET_FIREWALL_INTR   (0x9002)

Set Firewall Interrupt service type ID.

◆ HSM_KEYWRITER_SEND_CUST_KEY_CERT

#define HSM_KEYWRITER_SEND_CUST_KEY_CERT   (0x9028)

send KeyWriter customer key certificate

◆ HSM_MSG_READ_SWREV

#define HSM_MSG_READ_SWREV   (0x9033)

Read Software Revision service type ID.

◆ HSM_MSG_WRITE_SWREV

#define HSM_MSG_WRITE_SWREV   (0x9032)

Write Software Revision service type ID.

◆ HSM_MSG_GET_DKEK

#define HSM_MSG_GET_DKEK   (0x9029)

Get DKEK service type ID.

◆ HSM_MSG_GET_RAND

#define HSM_MSG_GET_RAND   (0x9001)

Get RNG service type ID.

◆ HSM_MSG_KEYRING_IMPORT

#define HSM_MSG_KEYRING_IMPORT   (0x9039)

Get KEYRING import service type ID.

◆ HSM_FLAG_AOP

#define HSM_FLAG_AOP   (0x11)

HSM FLAG used by HSM client to indicate that it expects ACK messasge from HSM and will wait for a response message.

◆ HSM_FLAG_NAOP

#define HSM_FLAG_NAOP   (0x22)

HSM FLAG used by HSM client to indicate that it does not expects an ACK messasge from HSM and will not wait for a response message.

◆ HSM_FLAG_ACK

#define HSM_FLAG_ACK   (0xAA)

HSM FLAG used by HSM server to indicate that the request has been processed.

◆ HSM_FLAG_NACK

#define HSM_FLAG_NACK   (0x55)

HSM FLAG used by HSM server to indicate that the request has not been processed.

◆ HSM_CLIENT_ID

#define HSM_CLIENT_ID   (0x01)

HSM server SIPC client Id.

◆ HSM_UID_SIZE

#define HSM_UID_SIZE   (64U)

UID or Unique ID is a device specific ID of 64 bytes.

◆ HSM_DBG_CERT_SIZE

#define HSM_DBG_CERT_SIZE   (4096U)

Maximum Certificate Size allowed for Debug Open.

◆ HSM_KEYRING_CERT_SIZE

#define HSM_KEYRING_CERT_SIZE   (10280U)

Maximum Certificate Size allowed for Keyring Import.

Enumeration Type Documentation

◆ HSM_ClientIds_t

Enumerator
HSM_BOOT_NOTIFY_CLIENT_ID 
HSM_CLIENT_ID_1 
HSM_CLIENT_ID_2 
HSM_CLIENT_ID_3 
HSM_CLIENT_ID_4 

Function Documentation

◆ __attribute__()

union HsmVer_t_ __attribute__ ( (packed)  )

type for reading HSMRt version.

HSM client / server message format struct.

◆ HsmClient_init()

int32_t HsmClient_init ( SIPC_Params params)

Initialize the HSM client for current core.

Parameters
params[IN] SIPC_notify params.
Returns
  1. SystemP_SUCCESS if init sequence successful.
  2. SystemP_FAILURE if init sequence fails.

◆ HsmClient_deInit()

void HsmClient_deInit ( void  )

De initialize the HSM client for current core.

◆ HsmClient_getVersion()

int32_t HsmClient_getVersion ( HsmClient_t HsmClient,
HsmVer_t *  verId,
uint32_t  timeToWaitInTick 
)

populates the current HSMRT version Id by default the hsm flag is set to HSM_FLAG_AOP for this service

Parameters
timeToWaitInTick[IN] amount of time to block waiting for semaphore to be available, in units of system ticks (see KERNEL_DPL_CLOCK_PAGE)
HsmClient[IN] Client object which is using this getversion API.
verId[OUT] populates HsmVer_t struct which describes current version. This object's memory address needs to be cache aligned.
Returns
  1. SystemP_SUCCESS if returns successfully
  2. SystemP_FAILURE if NACK message is received or client id not registered.
  3. SystemP_TIMEOUT if timeout exception occours.

◆ HsmClient_getUID()

int32_t HsmClient_getUID ( HsmClient_t HsmClient,
uint8_t *  uid,
uint32_t  timeout 
)

The service issued to HSM Server populates the Device UID by default the hsm flag is set to HSM_FLAG_AOP for this service.

Parameters
timeout[IN] amount of time to block waiting for semaphore to be available, in units of system ticks (see KERNEL_DPL_CLOCK_PAGE)
HsmClient[IN] Client object which is using this getUID API.
uid[OUT] populates UID value.
Returns
  1. SystemP_SUCCESS if returns successfully
  2. SystemP_FAILURE if NACK message is received or client id not registered.
  3. SystemP_TIMEOUT if timeout exception occours.

◆ HsmClient_openDbgFirewall()

int32_t HsmClient_openDbgFirewall ( HsmClient_t HsmClient,
uint8_t *  cert,
uint32_t  cert_size,
uint32_t  timeout 
)

The service issued to HSM Server verifies the certificate and by default the hsm flag is set to HSM_FLAG_AOP for this service.

Parameters
timeout[IN] amount of time to block waiting for semaphore to be available, in units of system ticks (see KERNEL_DPL_CLOCK_PAGE)
HsmClient[IN] Client object which is using this openDbgFirewalls API.
cert[IN] point to the location of certificate in the device memory.
cert_size[IN] size of certificate.
Returns
  1. SystemP_SUCCESS if returns successfully
  2. SystemP_FAILURE if NACK message is received or client id not registered.
  3. SystemP_TIMEOUT if timeout exception occours.

◆ HsmClient_importKeyring()

int32_t HsmClient_importKeyring ( HsmClient_t HsmClient,
uint8_t *  cert,
uint32_t  cert_size,
uint32_t  timeout 
)

The service issued to HSM Server verifies the certificate and imports the keys from the certificate.

Parameters
timeout[IN] amount of time to block waiting for semaphore to be available, in units of system ticks (see KERNEL_DPL_CLOCK_PAGE)
HsmClient[IN] Client object which is using this importKeyring API.
cert[IN] point to the location of certificate in the device memory.
cert_size[IN] size of certificate.
Returns
  1. SystemP_SUCCESS if returns successfully
  2. SystemP_FAILURE if NACK message is received or client id not registered.
  3. SystemP_TIMEOUT if timeout exception occours.

◆ HsmClient_readOTPRow()

int32_t HsmClient_readOTPRow ( HsmClient_t HsmClient,
EfuseRead_t readRow 
)

The service issued to HSM Server retrieves the data of GP OTP row based on row index provided as param.

Parameters
HsmClient[IN] HsmClient object.
readRow[IN] populates EfuseRead_t struct with rowData corresponding to rowIdx.
Returns
  1. SystemP_SUCCESS if returns successfully
  2. SystemP_FAILURE if NACK message is received or client id not registered.

◆ HsmClient_writeOTPRow()

int32_t HsmClient_writeOTPRow ( HsmClient_t HsmClient,
EfuseRowWrite_t writeRow 
)

The service issued to HSM Server writes the data to extended OTP efuse row based on row index provided as param.

Parameters
HsmClient[IN] HsmClient object.
writeRow[IN] populates EfuseRowWrite_t struct with rowData corresponding to rowIdx.
Returns
  1. SystemP_SUCCESS if returns successfully
  2. SystemP_FAILURE if NACK message is received or client id not registered.

◆ HsmClient_lockOTPRow()

int32_t HsmClient_lockOTPRow ( HsmClient_t HsmClient,
EfuseRowProt_t rowProt 
)

The service issued to HSM Server sets the protection status bit of the specified row to 1.

Parameters
HsmClient[IN] HsmClient object.
rowProt[IN] Pointer to EfuseRowProt_t struct which contains the row index and row protection status
Returns
  1. SystemP_SUCCESS if returns successfully
  2. SystemP_FAILURE if NACK message is received or client id not registered.

◆ HsmClient_getOTPRowCount()

int32_t HsmClient_getOTPRowCount ( HsmClient_t HsmClient,
EfuseRowCount_t rowCount 
)

The service issued to HSM Server retrieves the count of extended OTP rows.

Parameters
HsmClient[IN] HsmClient object.
rowCount[IN] Pointer to EfuseRowCount_t struct which is populated by HSM server with row count and row size
Returns
  1. SystemP_SUCCESS if returns successfully
  2. SystemP_FAILURE if NACK message is received or client id not registered.

◆ HsmClient_getOTPRowProtection()

int32_t HsmClient_getOTPRowProtection ( HsmClient_t HsmClient,
EfuseRowProt_t rowProt 
)

The service issued to HSM Server retrieves the extended otp efuse row protection status.

Parameters
HsmClient[IN] HsmClient object.
rowProt[IN] Pointer to EfuseRowProt_t struct which is populated by HSM server with row protection status
Returns
  1. SystemP_SUCCESS if returns successfully
  2. SystemP_FAILURE if NACK message is received or client id not registered.

◆ HsmClient_procAuthBoot()

int32_t HsmClient_procAuthBoot ( HsmClient_t HsmClient,
uint8_t *  cert,
uint32_t  cert_size,
uint32_t  timeout 
)

The service issued to HSM Server helps with extended secure boot for applications.

Parameters
timeout[IN] amount of time to block waiting for semaphore to be available, in units of system ticks (see KERNEL_DPL_CLOCK_PAGE)
HsmClient[IN] Client object which is using this openDbgFirewalls API.
cert[IN] point to the location of certificate in the device memory.
cert_size[IN] size of certificate.
Returns
  1. SystemP_SUCCESS if returns successfully
  2. SystemP_FAILURE if NACK message is received or client id not registered.
  3. SystemP_TIMEOUT if timeout exception occours.

◆ HsmClient_setFirewall()

int32_t HsmClient_setFirewall ( HsmClient_t HsmClient,
FirewallReq_t FirewallReqObj,
uint32_t  timeout 
)

The service issued to HSM Server sets the firewall for the given firewall id and region.

Parameters
timeout[IN] amount of time to block waiting for semaphore to be available, in units of system ticks (see KERNEL_DPL_CLOCK_PAGE)
HsmClient[IN] HsmClient object.
FirewallReqObj[IN] Pointer to FirewallReq_t struct which contains information required for HSM to process set firewall request.
Returns
  1. SystemP_SUCCESS if returns successfully
  2. SystemP_FAILURE if NACK message is received or client id not registered.
  3. SystemP_TIMEOUT if timeout exception occours.

◆ HsmClient_FirewallIntr()

int32_t HsmClient_FirewallIntr ( HsmClient_t HsmClient,
FirewallIntrReq_t FirewallIntrReqObj,
uint32_t  timeout 
)

The service issued to HSM Server sets the firewall interrupt request for the given firewall id.

Parameters
timeout[IN] amount of time to block waiting for semaphore to be available, in units of system ticks (see KERNEL_DPL_CLOCK_PAGE)
HsmClient[IN] HsmClient object.
FirewallIntrReqObj[IN] Pointer to FirewallIntrReq_t struct which contains information required for HSM to process firewall interrupt request.
Returns
  1. SystemP_SUCCESS if returns successfully
  2. SystemP_FAILURE if NACK message is received or client id not registered.
  3. SystemP_TIMEOUT if timeout exception occours.

◆ HsmClient_keyWriter()

int32_t HsmClient_keyWriter ( HsmClient_t HsmClient,
KeyWriterCertHeader_t certHeader,
uint32_t  timeout 
)

The service issued to HSM Server verifies the certificate and process the keywriter operations,.

Parameters
HsmClient[IN] Client object which is using this API.
certHeader[IN] point to the location of certificate in the device memory. This object's memory address needs to be cache aligned.
timeout[IN] amount of time to block waiting for semaphore to be available, in units of system ticks (see KERNEL_DPL_CLOCK_PAGE)
Returns
  1. SystemP_SUCCESS if returns successfully
  2. SystemP_FAILURE if NACK message is received or client id not registered.
  3. SystemP_TIMEOUT if timeout exception occours.

◆ HsmClient_readSWRev()

int32_t HsmClient_readSWRev ( HsmClient_t HsmClient,
SWRev_t readSWRev 
)

The service issued to HSM Server retrieves the SWRevision value based on identifier as param.

Parameters
HsmClient[IN] HsmClient object.
readSWRev[IN] populates SWRev_t struct with SWRev value corresponding to identifier.
Returns
  1. SystemP_SUCCESS if returns successfully
  2. SystemP_FAILURE if NACK message is received or client id not registered.

◆ HsmClient_writeSWRev()

int32_t HsmClient_writeSWRev ( HsmClient_t HsmClient,
SWRev_t writeSWRev 
)

The service issued to HSM Server writes the SWRevision value based on identifier as param.

Parameters
HsmClient[IN] HsmClient object.
writeSWRev[IN] updates the SWRev efuses with SWRev value corresponding to identifier.
Returns
  1. SystemP_SUCCESS if returns successfully
  2. SystemP_FAILURE if NACK message is received or client id not registered.

◆ HsmClient_getDKEK()

int32_t HsmClient_getDKEK ( HsmClient_t HsmClient,
DKEK_t getDKEK,
uint32_t  timeout 
)

The service issued to HSM Server retrieves the derived KEK based on identifier as param.

The service issued to HSM Server retrieves the derived KEK.

Parameters
timeout[IN] amount of time to block waiting for semaphore to be available, in units of system ticks (see KERNEL_DPL_CLOCK_PAGE)
HsmClient[IN] HsmClient object.
getDKEK[IN] Pointer to DKEK_t which contains the request structure for Derived KEK.
Returns
  1. SystemP_SUCCESS if returns successfully
  2. SystemP_FAILURE if NACK message is received or client id not registered.

◆ HsmClient_register()

int32_t HsmClient_register ( HsmClient_t HsmClient,
uint8_t  clientId 
)

register a client to a particular ClientId

Parameters
HsmClient[IN] HsmClient object.
clientId[IN] enable HSM <--> R5 communication for given clientID
Returns
  1. SystemP_SUCCESS if clientId is available
  2. SystemP_FAILURE if clientId is not available or already in use.

◆ HsmClient_unregister()

void HsmClient_unregister ( HsmClient_t HsmClient,
uint8_t  clientId 
)

unregister a client to a particular ClientId

Parameters
HsmClient[IN] HsmClient object
clientId[IN] disable HSM <--> R5 communication for given clientId

◆ HsmClient_waitForBootNotify()

int32_t HsmClient_waitForBootNotify ( HsmClient_t HsmClient,
uint32_t  timeToWaitInTicks 
)

Current core will wait for bootnotify message from HSM core.

Parameters
HsmClient[IN] HsmClient object
timeToWaitInTicks[IN] amount of time to block waiting for semaphore to be available, in units of SystemP_timeout if timeout exception occours.system ticks (see KERNEL_DPL_CLOCK_PAGE)
Returns
  1. SystemP_SUCCESS -: when BootNotify received
  2. SystemP_FAILURE -: if faulty msg received

◆ Hsmclient_loadHSMRtFirmware()

int32_t Hsmclient_loadHSMRtFirmware ( HsmClient_t gHSMClient,
const uint8_t *  pHSMRt_firmware 
)

Loads the HSMRt firmware. This is typically called by SBL.

Parameters
gHSMClient[IN] Pointer to registered HSM Client
pHSMRt_firmware[IN] Pointer to signed HSMRt binary
Returns
SystemP_SUCCESS on success, else SystemP_FAILURE

◆ HsmClient_getRandomNum()

int32_t HsmClient_getRandomNum ( HsmClient_t HsmClient,
RNGReq_t getRandomNum 
)

Returns the Random Number Generated.

Parameters
HsmClient[IN] HsmClient object
getRandomNum[IN] Pointer to RNGReq_t which contains the request structure for Random Number Generated.
Returns
  1. SystemP_SUCCESS if returns successfully
  2. SystemP_FAILURE if NACK message is received or client id not registered.