AM263Px MCU+ SDK  09.02.00
dac/v0/dac.h File Reference

Go to the source code of this file.

Macros

#define DAC_LOCK_CONTROL   (0x1U)
 Header Files. More...
 
#define DAC_LOCK_SHADOW   (0x2U)
 Lock the shadow value register. More...
 
#define DAC_LOCK_OUTPUT   (0x4U)
 Lock the output enable register. More...
 
#define DAC_REG_BYTE_MASK   (0xFFU)
 Register Byte Mask. More...
 
#define DAC_LOCK_KEY   (0xA000U)
 DAC Lock Key. More...
 

Enumerations

enum  DAC_ReferenceVoltage { DAC_REF_VREF = 0, DAC_REF_VDDA = 1 }
 
enum  DAC_LoadMode { DAC_LOAD_SYSCLK = 0, DAC_LOAD_PWMSYNC = 4 }
 Values that can be passed to DAC_setLoadMode() as the mode parameter. More...
 

Functions

static uint16_t DAC_getRevision (uint32_t base)
 
static void DAC_setReferenceVoltage (uint32_t base, DAC_ReferenceVoltage source)
 
static void DAC_setLoadMode (uint32_t base, DAC_LoadMode mode)
 
static void DAC_setPWMSyncSignal (uint32_t base, uint16_t signal)
 
static uint16_t DAC_getActiveValue (uint32_t base)
 
static void DAC_setShadowValue (uint32_t base, uint16_t value)
 
static uint16_t DAC_getShadowValue (uint32_t base)
 
static void DAC_enableOutput (uint32_t base)
 
static void DAC_disableOutput (uint32_t base)
 
static void DAC_setOffsetTrim (uint32_t base, int16_t offset)
 
static int16_t DAC_getOffsetTrim (uint32_t base)
 
static void DAC_lockRegister (uint32_t base, uint16_t reg)
 
static bool DAC_isRegisterLocked (uint32_t base, uint16_t reg)
 
void DAC_tuneOffsetTrim (uint32_t base, Float32 referenceVoltage)