AM263Px MCU+ SDK  09.02.00
PBIST

Built-in Self-test (BIST) is a feature that allows self testing of the memory areas and logic circuitry in an Integrated Circuit (IC) without any external test equipment. In an embedded system, these tests are typically used during boot time or shutdown of the system to check the health of an SoC.

PBIST is used to test the memory regions in the SoC and provides detection for permanent faults. The primary use case for PBIST is when it is invoked at start-up providing valuable information on any stuck-at bits in the memory.

There can be multiple instances of PBIST in the SoC, and each has a number of memory regions associated with it. SDL provides support for PBIST features such as execution of PBIST test-for-diagnostic to test the PBIST logic and execution of PBIST. The same API is used with different configuration parameters to execute each instance. Checking of the status of HW POST PBIST execution is also supported.

Some things to note:

  • PBIST is expected to be run at boot-time or once per drive cycle.
  • PBIST must be run from a different core than is being tested. This is because the test is destructive in nature. For this reason also, after BIST test it is necessary to reset the module.
  • If SW-initiated PBIST is executed after the IP under test is already in use in the system, it is the application's responsibility to perform any necessary context save/restore necessary for the core/IP.

Features Supported

The PBIST Module of the SDL supports execution of the software-initiated PBIST for the various supported instances. It provides the following services:

  • Execution of the PBIST test for a specified instance
  • Checking of the PBIST results
  • Restore core to system control (PBIST reset and release test mode)
  • Return the status of the test

SysConfig Features

  • None

Features NOT Supported

  • None

Important Usage Guidelines

  • Execution of the PBIST tests requires preparation of the IPs under test by bringing them to a certain power and reset state before executing the test. It will be required that the application bring the cores/IPs to the proper state before executing the PBIST. Additionally, there is an "exit sequence" that is required to bring the cores/IPs back to the system control after the PBIST test is executed. This will also be the responsibility of the application. The PBIST examples provided with SDL will give the necessary sequences, which can be used by the application for implementing the sequence.

Example Usage

The following shows an example of SDL PBIST API usage by the application to execute the PBIST test and test-for-diagnostic.

Include the below file to access the APIs

#include <sdl/sdl_pbist.h>

Before executing the following PBIST tests, the IP under test must be brought to a certain power and reset state. The included PBIST example shows the sequence needed for each of the PBIST instances.

Once the core(s) are brought to the required state, the following APIs can be run.

Run the PBIST test-for-diagnostic:

bool PBISTResult;
status = SDL_PBIST_selfTest(SDL_PBIST_INST_MPU, SDL_PBIST_NEG_TEST, timeoutVal, &PBISTResult);
if ((status != SDL_PASS) || (PBISTResult == false))
{
// test failed
}

Perform the PBIST test

bool PBISTResult;
status = SDL_PBIST_selfTest(SDL_PBIST_INST_MPU, SDL_PBIST_TEST, timeoutVal, &PBISTResult);
if ((status != SDL_PASS) || (PBISTResult == false))
{
// test failed
}

API

APIs for PBIST (Memory Built-In Self Test)

SDL_PBIST_selfTest
int32_t SDL_PBIST_selfTest(SDL_PBIST_inst instance, SDL_PBIST_testType testType, uint32_t timeout, bool *pResult)
PBIST self test.
sdl_pbist.h
This file contains the SDL PBIST API's.
SDL_PBIST_NEG_TEST
@ SDL_PBIST_NEG_TEST
Definition: sdl_pbist.h:81
SDL_PBIST_TEST
@ SDL_PBIST_TEST
Definition: sdl_pbist.h:75