AM263Px MCU+ SDK  09.02.00
SDL MCU VTM

Introduction

This example demonstrates the usage of the VTM to detect overtemperature events and signal the events through the interrupt/ESM. The example shows how to configure the VTM for the various alerts and listen for VTM events using the interrupts/ESM. It also shows forcing an error in order to demonstrate application notification of overtemperature events.

The example demonstrates:

  • Configuring the VTM thresholds
  • Early alert event detection
  • Critial threshold event detection
  • Follow-up event notification when temperature has dropped to a safe level

Use Cases

Use Case Description
UC-0 Configuration of VTM threshold to trigger Low and High Threshold Hot alert warning.
UC-1 Configuration of VTM threshold to trigger Hot alert warning, then return thresholds back to normal to simulate "cooling down".
UC-2 Configuration of VTM threshold to trigger ESM interrupt.

Supported Combinations

Parameter Value
CPU + OS r5fss0-0 nortos
Toolchain ti-arm-clang
Board am263px-cc
Example folder examples/sdl/vtm/

Steps to Run the Example

See Also

VTM

Sample Output

Shown below is a sample output when the application is run,

[Cortex_R5_0]
VTM Example Application
UC1 :
Device Temperature: 70000mc
Configured hot alert Temperature: 58000mc
Hot Alert Temperature breached and received Interrupt : 133
Device Temperature: 70000mc
Configured cold alert Temperature: 72000mc
Cold Alert Temperature breached and received Interrupt
Temperature is below Configured Low Temperature and received Interrupt : 133
UC2 :
Device Temperature: 70000mc
Configured Low threshold Temperature: 66000mc
Low Threshold Temperature breached and received Interrupt: 134
Device Temperature: 70000mc
Configured hot threshold Temperature: 66000mc
Exceeded Configured Temperature and received Interrupt : 133
UC3 :
ESM_Test_init: Init MSS ESM complete
ESM Call back function called : instType 0x2, intType 0x1, grpChannel 0x1, index 0xc, intSrc 0x2c
Device Temperature: 70000mc
Configured Low threshold Temperature: 74000mc
Configured hot threshold Temperature: 66000mc
ESM Interrupt Received
All tests Passed