AM263Px MCU+ SDK  09.02.00
SDL TMU ROM_CHECKSUM Example

Introduction

This example demonstrates usage of the SDL TMU ROM Checksum. This example is used to check the integrity of the TMU ROM data. Its work is to take a set of data associated with the memory regions of TMU ROM and perform checksum on that data and then compare that resultant data value against a pre-determined golden vector value.

Use Cases

Use Case Description
UC-1 Calculate TMU ROM CHECKSUM from R5F Core.

Supported Combinations

Parameter Value
CPU + OS r5fss0-0 nortos
Toolchain ti-arm-clang
Board am263px-cc
Example folder examples/sdl/tmu_rom_checksum/

Steps to Run the Example

See Also

TMU_ROM_CHECKSUM

Sample Output

[MAIN_Cortex_R5_0_0]
ROM Checksum Example Application
Compute ROM-Checksum Data integrity passed