AM263Px MCU+ SDK  09.02.00
SDFM Filter sync DMA read

Introduction

A SDFM example that reads filter data from CPU In this example, SDFM filter data is read by DMA by SDFM FIFO DATA READTY INT trigger. SDFM configuration is shown below:

  • SDFM used in this example - SDFM0
  • Input control mode selected - MODE0
  • Data filter settings
    • Filter 1 is enabled
    • Sinc3 filter selected
    • OSR = 256
    • Synchronized by using MFE (Main Filter enable bit)
    • Filter output represented in 16 bit format
    • In order to convert 26 bit Data filter into 16 bit format user needs to right shift by 10 bits for Sinc3 filter with OSR = 256
    • FIFO is enabled for 16 levels.
  • Interrupt module settings for SDFM filter
    • Filter 1 will generate interrupt when a new filter FIFO Threshold is crossed.

Example Block diagram

External Connections

  • Connect Sigma-Delta streams to SDFM0_CLK0, SDFM0_D0

Watch Variables

  • filter1Result - Output of filter 1

AM263X-CC or AM263PX-CC

When using AM263x-CC with TMDSHSECDOCK (HSEC180 controlCARD Baseboard Docking Station)

  • Connect Sigma-Delta streams to HSEC Pin 91, HSEC Pin 72

If required, use PWM waveforms as data and clock

  • Connect HSEC Pin 51 to HSEC Pin 91
  • Connect HSEC Pin 49 to HSEC Pin 72

AM263X-LP or AM263PX-LP

This example is not supported on AM263X-LP

Supported Combinations

Parameter Value
CPU + OS r5fss0-0 nortos
Toolchain ti-arm-clang
Board am263px-cc
Example folder examples/drivers/sdfm/sdfm_filter_sync_dmaread/

Steps to Run the Example

  • When using CCS projects to build, import the CCS project for the required combination and build it using the CCS project menu (see Using SDK with CCS Projects).
  • When using makefiles to build, note the required combination and build using make command (see Using SDK with Makefiles)
  • Establish connections as mentioned in External Connections section
  • Launch a CCS debug session and run the executable, see CCS Launch, Load and Run
  • View the UART console logs for results

See Also

SDFM

Sample Output

Shown below is a sample output when the application is run,

SDFM filter sync CPU read Test Started ...
gSdfmFifo1Base : 50268032
Some of the copied FIFO data...
Transfer number : 0 | Data : -2731 -13654 -16384 -16384 -16384 -16384 -16384 -16384 -16384 -16384 -16384 -16384 -1638
Transfer number : 12 | Data : -16384 -16384 -16384 -16384 -16384 -16384 -16384 -16384 -16384 -16384 -16384 -16384 -16
Transfer number : 24 | Data : -16384 -16384 -16384 -16384 -16384 -16384 -16384 -16384 -16384 -16384 -16384 -16384 -16
Transfer number : 36 | Data : -16384 -16384 -16384 -16384 -16384 -16384 -16384 -16384 -16384 -16384 -16384 -16384 -16
Transfer number : 48 | Data : -16384 -16384 -16384 -16384 -16384 -16384 -16384 -16384 -16384 -16384 -16384 -16384 -16
Transfer number : 60 | Data : -16384 -16384 -16384 -16384 -16384 -16384 -16384 -16384 -16384 -16384 -16384 -16384 -16
All tests have passed!!