Introduction
A SDFM example that reads filter data from CPU
In this example, SDFM filter data is read by CPU in SDFM ISR routine. The SDFM configuration is shown below:
- SDFM used in this example - SDFM0
- Input control mode selected - MODE0
- Comparator settings
- Sinc3 filter selected
- OSR = 32
- HLT = 0x7FFF (Higher threshold setting)
- LLT = 0x0000(Lower threshold setting)
- Data filter settings
- Single filter module enabled
- Sinc3 filter selected
- OSR = 128
- Single filter is synchronized by using MFE (Main Filter enable bit)
- Filter output represented in 16 bit format
- In order to convert 25 bit Data filter into 16 bit format user needs to right shift by 7 bits for Sinc3 filter with OSR = 128
- Interrupt module settings for SDFM filter
- Single higher threshold comparator interrupt disabled
- Single lower threshold comparator interrupt disabled
- Single modulator failure interrupt disabled
- Single filter will generate interrupt when a new filter data is available.
Watch Variables
- filterResult - Output of filter 2
External Connections
- Connect Sigma-Delta streams to SDFM0_CLK1, SDFM0_D1
AM263X-CC
When using AM263x-CC with TMDSHSECDOCK (HSEC180 controlCARD Baseboard Docking Station)
- Connect Sigma-Delta streams to HSEC Pin 99, HSEC Pin 101
If required, use PWM waveforms as SDFM data and clock
- Connect HSEC Pin 51 to HSEC Pin 99
- Connect HSEC Pin 49 to HSEC Pin 101
AM263X-LP
- Connect Sigma-Delta streams to Boosterpack header J6/J8 Pin 74, J6/J8 Pin 73
If required, use PWM waveforms as data and clock
- Connect Boosterpack header J2/J4 Pin 11 to J6/J8 Pin 73
- Connect Boosterpack header J6/J8 Pin 59 to J6/J8 Pin 74
Supported Combinations
| Parameter | Value |
| CPU + OS | r5fss0-0 nortos |
| Toolchain | ti-arm-clang |
| Boards | am263px-cc, am263px-lp |
| Example folder | examples/drivers/sdfm/sdfm_filter_sync_cpuread_single_channel.c/ |
Steps to Run the Example
- When using CCS projects to build, import the CCS project for the required combination and build it using the CCS project menu (see Using SDK with CCS Projects).
- When using makefiles to build, note the required combination and build using make command (see Using SDK with Makefiles)
- Establish connections as mentioned in External Connections section
- Launch a CCS debug session and run the executable, see CCS Launch, Load and Run
- View the UART console logs for results
See Also
SDFM
Sample Output
Shown below is a sample output when the application is run,
[Cortex_R5_0] SDFM filter sync CPU read Test Started ...
All tests have passed!!