AM263Px MCU+ SDK  09.02.00
MCSPI Loopback Multi Instances Multi channels LLD

Introduction

This example demonstrates the McSPI RX and TX operation configured in interrupt, polling and DMA mode of operation using LLD API's and each mode is using different channels.

This example sends a known data in the TX mode of length APP_MCSPI_MSGSIZE and then receives the same in RX mode. Internal pad level loopback mode is enabled to receive data. To enable internal pad level loopback mode, D0 pin is configured to both TX Enable as well as RX input pin in the SYSCFG.

When transfer is completed, TX and RX buffer data are compared. If data is matched, test result is passed otherwise failed.

Supported Combinations

Parameter Value
CPU + OS r5fss0-0 freertos
r5fss0-0 nortos
Toolchain ti-arm-clang
Boards am263px-cc, am263px-lp
Example folder examples/drivers/mcspi/mcspi_loopback_multi_instances_multi_channels_lld

Steps to Run the Example

See Also

MCSPI

Sample Output

Shown below is a sample output when the application is run,

[MCSPI] Loopback example started ...
All tests have passed!!