AM263Px MCU+ SDK  09.02.00
MCAN Loopback Polling

Introduction

This example demonstrates the CAN message transmission and reception in digital loop back mode with the following configuration.

  • Classic CAN Message Format.
  • Message ID Type is Extended, Msg Id 0xD0, 0xD1, 0xD2, 0xD3, 0xD4.
  • MCAN is configured in Polling Mode.
  • Arbitration Bit Rate 1Mbps.
  • Data Bit Rate 5Mbps.
  • FIFO mode is used for Tx and RX to store message in message RAM.

5 Messages are transmitted and received back internally using internal loopback mode. When all the 5 messages received with the id and the data matches with the transmitted one, then the example is completed.

Supported Combinations

Parameter Value
CPU + OS r5fss0-0 freertos
r5fss0-0 nortos
Toolchain ti-arm-clang
Board am263px-cc, am263px-lp
Example folder examples/drivers/mcan/mcan_loopback_polling

Steps to Run the Example

See Also

MCAN

Sample Output

Shown below is a sample output when the application is run,

[MCAN] Loopback Polling mode, application started ...
All tests have passed!!