Introduction
EPWM XCMP Multiple Edges
This example uses the ePWM module to generate multiple edges in a pwm cycle.
- Three instances of epwm have been used to demonstrate the use of XCMP feature.
- For EPWMx, XCMP feature is disabled and it generates waves with duty cycle of 37.5%
- For EPWMy, XCMP feature is enabled and the only the ACTIVE set registers are used, duty cycle is 1%.
- For EPWMz, XCMP feature is enabled and the ACTIVE as well as the three SHADOW set registers are used.
- Using shadow set 3, waves with duty cycle 50% is generated for 5 cycles for both output channels.
- Using shadow set 2, waves with duty cycle 0% is generated for 8 cycles for both output channels.
- Using shadow set 1, waves with duty cycle 20% for channel A and 40% for channel B is generated and this continues.
External Connections
- For AM263PX-CC or AM263PX-CC
- EPWM0_A and EPWM0_B pin can be connected to an oscilloscope to view the waveform.
- EPWM1_A and EPWM1_B pin can be connected to an oscilloscope to view the waveform.
- EPWM2_A and EPWM2_B pin can be connected to an oscilloscope to view the waveform.
- For AM263PX-LP or AM263PX-LP
- EPWM1_A and EPWM1_B pin can be connected to an oscilloscope to view the waveform.
- EPWM2_A and EPWM2_B pin can be connected to an oscilloscope to view the waveform.
- EPWM3_A and EPWM3_B pin can be connected to an oscilloscope to view the waveform.
AM263PX-CC or AM263PX-CC
When using AM263PX-CC or AM263PX-CC with TMDSHSECDOCK (HSEC180 controlCARD Baseboard Docking Station)
- Capture waveform on HSEC Pin 49 for epwm0_A
- Capture waveform on HSEC Pin 51 for epwm0_B
- Capture waveform on HSEC Pin 53 for epwm1_A
- Capture waveform on HSEC Pin 55 for epwm1_B
- Capture waveform on HSEC Pin 50 for epwm2_A
- Capture waveform on HSEC Pin 52 for epwm2_B
AM263PX-LP or AM263PX-LP
- Capture waveform on boosterpack header J2/J4 Pin 37 for epwm1_A
- Capture waveform on boosterpack header J2/J4 Pin 38 for epwm1_B
- Capture waveform on boosterpack header J2/J4 Pin 39 for epwm2_A
- Capture waveform on boosterpack header J2/J4 Pin 40 for epwm2_B
- Capture waveform on boosterpack header J6/J8 Pin 77 for epwm3_A
- Capture waveform on boosterpack header J6/J8 Pin 78 for epwm3_B
Supported Combinations
| Parameter | Value |
| CPU + OS | r5fss0-0 nortos |
| Toolchain | ti-arm-clang |
| Board | am263px-cc, am263px-lp |
| Example folder | examples/drivers/epwm/epwm_xcmp_multiple_edges |
Steps to Run the Example
- When using CCS projects to build, import the CCS project for the required combination and build it using the CCS project menu (see Using SDK with CCS Projects).
- When using makefiles to build, note the required combination and build using make command (see Using SDK with Makefiles)
- Establish connections as mentioned in External Connections section
- Launch a CCS debug session and run the executable, see CCS Launch, Load and Run
See Also
EPWM
Sample Output
Shown below is a sample output when the application is run,
EPWM XCMP multiple edges Test Started ...
EPWM XCMP multiple edges Test Passed!!
All tests have passed!!
EPWM XCMP multiple edges waveform