Introduction
This example demonstrates the Global SOC force feature. The ADCs that need to be forced globally are first selected in the Global Control using the API SOC_enableAdcGlobalForce with the instance number and the enable (TRUE/ FALSE) as arguments. then the API SOC_adcSocGlobalForce can be used to set a software trigger globally on the given SOC number at all the ADCs selected above.
Configurations
- ADCx SOC0 is configured for Software only trigger and generate interrupt at EOC0. x is 0,1,2,3,4.
External Connections
External connections are arbitrary for this feature demonstration. for instance, ADC0 SOC0 is configured for Channel 0. Feed Analog voltages on ADC0_AIN2
AM263Px-CC E2
- ADC0_AIN2, i.e., HSEC PIN 15
AM263Px-LP
- ADC0_AIN2, i.e., J5/7 PIN 66
Watch Variables
The below watch variables can be used to view ADC conversion results.
- gAdc0Results[] : Digital representation of the voltage converted by ADC0 when triggered by Global Software force
- gAdc1Results[] : Digital representation of the voltage converted by ADC1 when triggered by Global Software force
- gAdc2Results[] : Digital representation of the voltage converted by ADC2 when triggered by Global Software force
- gAdc3Results[] : Digital representation of the voltage converted by ADC3 when triggered by Global Software force
- gAdc4Results[] : Digital representation of the voltage converted by ADC4 when triggered by Global Software force
Supported Combinations
| Parameter | Value |
| CPU + OS | r5fss0-0 nortos |
| Toolchain | ti-arm-clang |
| Board | am263px-cc, am263px-lp |
| Example folder | examples/drivers/adc/adc_global_force/ |
Steps to Run the Example
- When using CCS projects to build, import the CCS project for the required combination and build it using the CCS project menu (see Using SDK with CCS Projects).
- When using makefiles to build, note the required combination and build using make command (see Using SDK with Makefiles)
- Establish connections as mentioned in External Connections section
- Launch a CCS debug session and run the executable, see CCS Launch, Load and Run
- Using watch variables, view the ADC conversion results.
- View the ADC conversion results in UART console logs
See Also
ADC
Sample Output
Shown below is a sample output when the application is run,
ADC Triggered by Global Software Force Test Started ...
ADC Triggered by Global Software Force Test Passed
All tests have passed!!