AM263Px MCU+ SDK  09.02.00
AES

Access Protection Scheme

AES and SHA IP in DTHE support two contexts, namely Public and Secure.

AES

  • The AES IP is an efficient implementation of the Rijndael cipher (the AES algorithm) and a 128-bit polynomial multiplication. Rijndael is a block cipher with each data block consisting of 128-bits.
  • AES encryption requires a specific number of rounds depending on the key length. Supported key lengths are 128-bit, 192-bit, and 256 bit, requiring 10, 12, and 14 rounds respectively; or 32, 38, and 44 clock cycles respectively because (# of clock cycles) = 2 + 3 x (# of rounds). The larger key lengths provide greater encryption strength at the expense of additional rounds and therefore reduced throughput.
    AES functional diagram

AES-ECB

AES ECB feedback mode
  • Above figure illustrates the basic Electronic Code Book (ECB) feedback mode of operation, where the input data is passed directly to the basic crypto core and the output of the crypto core is passed directly to the output buffer. For decryption the crypto core operates in reverse, thus, the decrypt datapath is used for the data processing, where encryption uses the encrypt datapath.

AES-CBC

AES CBC feedback mode
  • Above figure illustrates the Cipher Block Chaining (CBC) feedback mode of operation, where the input data is XOR-ed with the initialization vector (IV) before it is passed to the basic crypto core. The output of the crypto core passes directly to the output buffer and becomes the next IV. For decryption, the operation is reversed, resulting in an XOR at the output of the crypto core. The input cipher text of the current operation is the IV for the next operation.

AES-CTR

AES CTR mode
  • Above figure illustrates the Counter(CTR) mode of operation, where the operation encrypts the IV. The output of the crypto core (encrypted IV) is XOR-ed with the data, creating the output result. The IV is built out of two components, one fixed part and a counter part. The counter part is incremented with each block. The counter width is variable per context and can be 16, 32, 64, 96 or 128-bit wide. Note that in this mode, encryption and decryption use the same operation.

AES-CFB

AES CFB mode
  • Above figure illustrates the full block (128-bit) Cipher Feedback (CFB) mode of operation for both encryption and decryption. The input for the crypto core is the IV; the result is XOR-ed with the data. The result is fed back via the IV register, as the next input for the crypto core. The decrypt operation is reversed, but the crypto core is still performing an encryption.

AES-CMAC

AES CMAC mode
  • Above figure illustrates the One Key Mac mode of operation, where the input to the crypto core is XOR-ed with the IV. The crypto core output is then fed back as IV for the next block. The last data input block is XOR-ed with an additional input value stored in the Temporary Buffer; this can be any precalculated value and is dependent on the alignment of the last input block. For CMAC mode, the tweak value (in temporary buffer) is calculated via K1 and K2 which is dervied from Key value from software.

API Sequence for ECB, CBC, CTR, CMAC Algorithms (Single Shot Mechanism)

This sequence performs Encryption and decryption operations for AES-ECB/CBC/CTR algorithms. Supported key lengths are 128, 192, 256 bit.

API Sequence for ECB, CBC, CTR, CMAC Algorithms (Multi Shot Mechanism)

This sequence performs Encryption and decryption operations for AES-ECB/CBC/CTR algorithms. Supported key lengths are 128, 192, 256 bit.

  • DTHE_open(): Function to open DTHE instance, enable DTHE engine.
  • DTHE_AES_open(): Function to open DTHE AES instance using the handle returned from DTHE_open().
  • DTHE_AES_execute(): Function to execute the AES driver with specified parameters and streamstate as init.
  • DTHE_AES_execute(): Function to execute the AES driver with specified parameters and streamstate as update.
  • DTHE_AES_execute(): Function to execute the AES driver with specified parameters and streamstate as finish.
  • DTHE_AES_close(): Function to close DTHE AES driver.
  • DTHE_close(): Function to De-initialize the DTHE instance.

In order to cancel an existing stream, DTHE_AES_close should be called followed by DTHE_AES_open like this. This will discard the current stream data -

API