AM62Px MCU+ SDK  11.01.01
tisci_lpm_enc_dec.h File Reference

Go to the source code of this file.

Data Structures

struct  tisci_msg_enc_req
 This file contains: More...
 
struct  tisci_msg_enc_resp
 Response for TISCI_MSG_LPM_ENCRYPT. More...
 
struct  tisci_msg_dec_req
 Request for TISCI_MSG_LPM_DECRYPT. More...
 
struct  tisci_msg_dec_resp
 Response for TISCI_MSG_LPM_DECRYPT. More...
 

Functions

struct tisci_msg_enc_req __attribute__ ((__packed__))
 

Variables

struct tisci_header hdr
 
uint64_t unencrypted_addr
 
uint64_t encrypted_addr
 
uint32_t unencrypted_len
 
uint32_t max_encrypted_len
 

Variable Documentation

◆ hdr

struct tisci_header hdr

◆ unencrypted_addr

uint64_t unencrypted_addr

◆ encrypted_addr

uint64_t encrypted_addr

◆ unencrypted_len

uint32_t unencrypted_len

◆ max_encrypted_len

uint32_t max_encrypted_len