AM62Px MCU+ SDK  11.01.01

Detailed Description

Request for TISCI_MSG_SYNC_RESUME.

Parameters
hdrTISCI header to provide ACK/NAK flags to the host.

Generic synchronization message between cores to be used as a checkpoint when TIFS and DM are working in coordination.

Data Fields

struct tisci_header hdr
 

Field Documentation

◆ hdr

struct tisci_header tisci_msg_sync_resume_req::hdr