AM62Px MCU+ SDK  11.01.01

Detailed Description

This file contains:

    WARNING!!: Autogenerated file from SYSFW. DO NOT MODIFY!!

System Firmware

TISCI Data structures for setting boot mode

Request to set boot mode

Parameters
hdrCommon tisci header
boot_mode_efuse_idxThe boot mode efuse to program
resvReserved field of 3 bytes
write_valNumber containing the 25-bit value to be blown

Data Fields

struct tisci_header hdr
 
uint8_t boot_mode_efuse_idx
 
uint8_t resv [3]
 
uint32_t write_val
 

Field Documentation

◆ hdr

struct tisci_header tisci_msg_set_otp_boot_mode_req::hdr

◆ boot_mode_efuse_idx

uint8_t tisci_msg_set_otp_boot_mode_req::boot_mode_efuse_idx

◆ resv

uint8_t tisci_msg_set_otp_boot_mode_req::resv[3]

◆ write_val

uint32_t tisci_msg_set_otp_boot_mode_req::write_val