AM62Px MCU+ SDK  11.01.01

Detailed Description

This file contains:

    WARNING!!: Autogenerated file from SYSFW. DO NOT MODIFY!!

System Firmware TISCI RM Proxy Messaging

TISCI Protocol Definitions for proxy messages

Configures a Navigator Subsystem proxy

Configures the channelized firewalls of a Navigator Subsystem proxy. The firewalls are configured to all the header host access to the backing RAM and target data configuration registers. The proxy index must be assigned to the host defined in the TISCI header via the RM board configuration resource assignment range list.

Parameters
hdrStandard TISCI header
valid_paramsBitfield defining validity of proxy configuration parameters. This field is unused at the moment but exists if expansion of the API is needed in the future.
nav_idSoC device ID of Navigator Subsystem where proxy is located
indexProxy index.

Data Fields

struct tisci_header hdr
 
uint32_t valid_params
 
uint16_t nav_id
 
uint16_t index
 

Field Documentation

◆ hdr

struct tisci_header tisci_msg_rm_proxy_cfg_req::hdr

◆ valid_params

uint32_t tisci_msg_rm_proxy_cfg_req::valid_params

◆ nav_id

uint16_t tisci_msg_rm_proxy_cfg_req::nav_id

◆ index

uint16_t tisci_msg_rm_proxy_cfg_req::index