AM62Px MCU+ SDK  11.01.01

Detailed Description

Result of a query operation.

Parameters
hdrTISCI header
freq_hzThe frequency in Hz that the hardware would set for the given parameters.

Data Fields

struct tisci_header hdr
 
uint64_t freq_hz
 

Field Documentation

◆ hdr

struct tisci_header tisci_msg_query_freq_resp::hdr

◆ freq_hz

uint64_t tisci_msg_query_freq_resp::freq_hz